Attributes (Unit Enable Determination - ASC) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The following table describes the attributes used by this module.

Table 1. Unit Enable Determination ASC Attributes
Name Type 1 Description Default Value
Network Mode   Specifies whether to allow the unit to operate normally or shutdown.
  • 0=Shutdown
  • 1=Enable
Enable
Hardware Mode   Specifies whether to allow the unit to operate normally or shutdown.
  • 0=Shutdown
  • 1=Enable
Enable
Power Fail Restart Enable   When this value is set to true, a timer will hold the output at shutdown until the Power Fail Restart Time has elapsed. False
Power Fail Restart Time   Sets the time to delay start when the power fail restart logic is enabled. 60.0

Display Units = Seconds

Resolution Mode   Used to determine how the input commands should be resolved into a single output command.
  • 0=Either Can Shutdown
  • 1=Network Priority
  • 2=Hardware Priority
Either Can Shutdown
Restart Status V Indicates the status of restart for N2 compatibility. False
State G, V Current desired state for the unit.
  • 0=Shutdown
  • 1=Enable
Enable
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)