Unit Enable Determination ASC - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This module is responsible for generating a Unit Enable command. This command is generated from a logical combination of a Network and Hardware Mode and the parameters for controlling the restart after a power failure. This module is implemented as a standard Control Activity.

Figure 1. Unit Enable Determination ASC Module

Figure 2. Unit Enable Determination ASC Module Use in Application

Figure 3. Unit Enable Determination ASC Module Activity