Module Use in Applications - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This section indicates how the module is identified in the tool software. This section includes a table that lists the individual module instances used by that particular group of modules and the applications in which the module instance is used.

To see a module's connections and how modules interact with it, view the Connections table.