Execution Status - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Execution Status logic block provides information about the conditions of the current execution:

  • Power Up: First execution following controller power cycle

  • Restart: First execution following controller reboot without the power being lost

  • Re-Enabled: Neither of the above conditions are true and this is the first execution after being re-enabled

  • Normal: None of the above conditions are true

An example use of the Execution Status block is to execute alternate logic for the first execution following a power failure or controller restart by using the Present Value to set the State of a Hybrid Activity.

You can use this block to perform a different calculation for the first execution after a particular State of a Hybrid Activity is enabled (for example, Execution Status - Present Value connecting to a MUX within a Hybrid Activity State section).

The Reliability associated with the Execution Status block always reports as Reliable.

The following table describes the output of the Execution Status logic block.

Table 1. Execution Status Block Output

Name

Data Type

Exposed for Connection by Default

Description

Default Value

Outputs

Present Value 1

Enum

Yes

Indicates the enumeration value output that provides information about the execution status.

Normal Set Name: Execution Status Normal, Power Up, Restart, or Re-Enabled

1 This input or output is the Default Element of the block.