Binary to Multistate Enum Set Mapping Rules - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Use the following table to match output objects to Binary Input and Binary Output enum sets when you edit or customize a device. If you do not match the object correctly, the output object turns orange and appear as Inactive/Active.

Table 1. Binary to Multistate Enum Set Mapping Rules

Name

Binary Enum Set ID

Multistate Enum Set ID

Absent Present

Absent Present

Absent/Present

Active Inactive

Active Inactive

Active/Inactive

Alarm Normal

Alarm Normal

Alarm/Normal

Auto Manual

Auto Manual

Automatic Manual

Clean Dirty

Clean Dirty

Clean/Dirty

Close Open

Close Open

Close/Open

Closed Minimum

Closed Minimum

Closed/Minimum

Cold Hot

Cold Hot

Cold/Hot

Disable Enable

Disable Enable

Disable/Enable

False True

False True

False/True

Forward Reverse

Forward Reverse

Forward/Reverse

Heat Cool

Heat Cool

Heating/Cooling

Inactive Active

Inactive Active

Inactive/Active

Lag Lead

Lag Lead

Lag/Lead

Local Remote

Local Remote

Local/Remote

Low High

Low High

Low/High

Low Normal

Low Normal

Low/Normal

Mechanical Free

Mechanical Free

Mechanical/Free

No Yes

No Yes

No/Yes

NoFlow Flow

NoFlow Flow

NoFlow/Flow

Normal Alarm

Normal Alarm

Normal/Alarm

Normal EnergyHoldOff

Normal EnergyHoldOff

Normal/Energy Hold Off

Normal FanOnly

Normal FanOnly

Normal/FanOnly

Normal Low

Normal Low

Normal/Low

Normal LowLimit

Normal LowLimit

Normal/Low Limit

Normal Reverse

Normal Reverse

Polarity

Normal Trigger

Normal Trigger

Normal/Trigger

NotAvailable Available

NotAvailable Available

Not Available/Available

Occ Unocc

Occ Unocc

Occ Sensor

Off Auto

Off Auto

Off/Auto

Off On

Off On

Off/On

Off On w Hold

Off On

Off/On/Hold

Off Reset

Off Reset

Off/Reset

Offline Online

Offline Online

Offline/Online

Ok Fault

Ok Fault

Ok/Fault

On Off

On Off

On/Off

Open Close

Open Close

Open/Close

Shutdown Enable

Shutdown Enable

Shutdown/Enable

Standby Run

Standby Run

Standby/Run

Start Stop

Start Stop

Start/Stop

State0 State1

State0 State1

States (0-1)

Stop Run

Stop Run

Stop/Run

Stop Start

Stop Start

Stop/Start

Summer Winter

Summer Winter

Summer/Winter

True False

True False

True/False

Unlock Lock

Unlock Lock

Unlock/Lock

Yes No

Yes No

Yes/No