Input Modules - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Inputs module category lists the inputs defined for the system. An input defines an interface to the actual hardware in a system. An input can represent a physical sensor in the system, or an input associated with a sensor. Inputs get data directly from hardware input points of a device.

See the following sections for information:

See the Upgrading System Files section for a list and description of the module and System Selection changes that were made since the last release of the tool.