Position Feedback (HP) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Position Feedback selections provide analog and binary inputs for modulated damper outputs. These feedback inputs are for monitoring only purposes. If you want to generate an alarm or other functionality using the position feedback inputs, you must create custom coding to do so.

The selection options for Position Feedback are:

  • Modulated Damper Outputs

    • No Position Feedback

    • Analog Input per Output

    • Binary Input per Output