Reversing Valve Output(s) (HP) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Reversing Valve Output selections set the logic in the Staged Compressor Control (Heat Pump Staged Compressors v51) Output module to determine whether the Reversing Valve Outputs (REV1-C and REV2-C) should be commanded on when there is a call for heating or cooling.

The selection options for Reversing Valve Output(s) are:

  • On for Cooling

  • On for Heating