Heat Pump Applications - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Heat Pump selections allow you to configure the mechanical choices for either an Air to Air, or Water to Air, Heat Pump configuration that contains one or two compressors. System Selection also allows optional Economizer and Supplemental Heating that are sequenced with the compressor logic.

See the Heat Pump Core Logic section for a list and description of the module and System Selection changes that were made since the last release of the tool.