Getting Started - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This section provides information on how to get started using the software, including basic information about the application and an overview of common tasks you can perform using the tool. Before you begin, gather any information you need to complete these tasks.

About Tool Information provides basic tool application information.

The tasks are categorized as follows:

  • Configuration and Simulation Tasks—Configuration and simulation tasks include how to create and configure your system, simulate your system, and define its associated hardware.

  • Commissioning and Servicing Tasks—Commissioning and servicing tasks include transfer of a Controller Application File (CAF) to a device, transfer of a device's CAF to a computer, and commissioning devices by viewing live data through the controller tool software.

For information on upgrading your system to the next release, see the Upgrading System Files section.