Discharge Air Temperature (FC) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This option is used primarily as a commissioning check-out feature to verify that the Discharge Air Temperature responds to commands to the heating and/or cooling devices.