Optional Equipment (FC) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
  • Filter Switch: This option creates a Filter Status Input and is typically mapped to the Supervisory system to create a Change Filter Alarm.

  • Lighting: This option creates an output to interface a Lighting Relay. When selected, the Always Occupied selection in the Occupancy (FC) section is not available. Only the Occupancy Mode Determination Mode logic interfaces with the Lighting Output. The default output configuration is a single, maintained binary output.