Condensate Alarm (FC) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This option provides a Binary Input to indicate the condensate drain is clogged. The cooling is disabled when the Condensate Alarm is active. The Shutdown on Alarm option shuts down the fan coil when the condensate alarm is active.