Common Heating-Cooling (FC) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

These selections provide the logic to control a Common Heating-Cooling (also known as 2-pipe) coil. If you select either one of the Cooling or Heating Coil options, this option is not available.