Cycle During Occupied (FC) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This option configures the Fan Determination State Generator module’s input for Fan Cycle to a Yes value, allowing the fan to turn off during Occupied if heating and cooling are both inactive. Otherwise, the Fan runs continuously during Occupied Mode. This selection is not available if the Fan Controlled By Other selection has been made.