Default Controller Tab - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04
Table 1. Hardware Definition - Default Controller Tab

Field

Description

System Type

Specifies the system type.

Default Controller

Indicates the default device used when users select the system type in the System Selection wizard.
Note: If you do not have any field controllers on your instance of the Tool, then you must select Artificial Field Device or Artificial IO Device appears as the default controller. The Artificial Field Device allows you to work with an application if you do not have the required hardware packages.

Close

Closes the dialog box.

Opens the Help system.