Field Device Selection Dialog Box - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

See the Defining Hardware section.

Note: If a warning message appears after selecting a field device, see Troubleshooting.
Table 1. Field Device Selection Dialog Box

Field

Description

Selections

Includes information for the following:

  • Name: Displays the names of the available selections.
  • Description: Description of the available selections.
  • Device Type: Type of controller.
  • Region: Displays the region of the controller.
  • Universal Inputs: Number of universal inputs.
  • Analog Inputs: Number of analog inputs.
  • Binary Inputs: Number of binary inputs.
  • Universal Outputs: Number of universal outputs.
  • Analog Outputs: Number of analog outputs.
  • Binary Outputs: Number of binary outputs.
  • Relay Outputs: Number of relay outputs.

OK

Applies the changes and closes the dialog box.

Cancel

Closes the dialog box without applying the changes.

Opens the Help system.