Reviewing Available Packages - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

About this task

In the Define Hardware dialog box, click the Packages tab to review all available package files.

The tool automatically checks for new or updated firmware package files at system start-up in the Packages Directory: C:\ProgramData\Johnson Controls\MetasysIII\Field Controller Packages.

Note: To import field controller packages, perform one of the following actions:
  • Click Import in Define Hardware > Packages. See Importing Package Files.
  • Double-click the package file or use the Package Importer, located in the Start menu. Restart the tool to view the newly imported package file.