Defining Hardware - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04
You can define hardware by using the Define Hardware dialog box. You can complete the following tasks:
  • define the hardware, map points, and define network settings for the system.
  • review the device packages that are installed in the tool.
  • define the default devices for each system type.
  • create, remove, modify, and view application point mapping for a Serial N2 Slave object in a controller.