Modules (Custom/Monitoring Zone Items) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Zone Items selections load the following modules in this Control View column:

Inputs

  • ZNX-T (Zone X Temperature Sensor AI, where X is 1-6): This Input is loaded when the Zone Temperature Sensor (AI) node is selected. Specific Inputs are loaded per sensor.

  • ZNX-H (Zone X Humidity AI, where X is 1-6): This Input is loaded when the Zone Humidity Sensor (AI) node is selected. Specific Inputs are loaded per sensor.

  • ZNX-Q (Zone X Species AI, where X is 1-6): This Input is loaded when the Zone CO2 Sensor (AI) node is selected. Specific Inputs are loaded per sensor.

See the Input Modules section.