Modules (Custom/Monitoring Sand Filter Items) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Sand Filter Items selections load the following modules in these Control View columns:

Inputs

  • SANDFILT-S (Sand Filter Backwash Status BI): This Input is loaded when the Backwash Status (BI) node is selected.

See the Input Modules section.

Outputs

  • SANDFILT-C (Sand Filter Command BO): This Output is loaded when the Command (BO) node is selected.

See the Output Modules section.