Pipe Mounted Items (Custom/Monitoring) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The selection options for Pipe Mounted Items are:

  • Temperature Sensor (AI): This option measures the temperature in a piping system for up to six locations.

    • 1 Sensor (1 AI)

    • 2 Sensors (2 AIs)

    • 3 Sensors (3 AIs)

    • 4 Sensors (4 AIs)

    • 5 Sensors (5 AIs)

    • 6 Sensors (6 AIs)

  • Water Flow Status Switch (BI): This option indicates when flow is present in a piping system for up to six locations.

    • 1 Switch (1 BI)

    • 2 Switches (2 BIs)

    • 3 Switches (3 BIs)

    • 4 Switches (4 BIs)

    • 5 Switches (5 BIs)

    • 6 Switches (6 BIs)

  • Water Flow Sensor (AI): This option measures the volume of water flowing through a piping system for up to six locations.

    • 1 Sensor (1 AI)

    • 2 Sensors (2 AIs)

    • 3 Sensors (3 AIs)

    • 4 Sensors (4 AIs)

    • 5 Sensors (5 AIs)

    • 6 Sensors (6 AIs)

  • Steam Pressure (AI): This option measures the pressure of the steam in a piping system.

  • Water Pressure (AI): This option measures the water pressure in a piping system for up to six locations.

    • 1 Sensor (1 AI)

    • 2 Sensors (2 AIs)

    • 3 Sensors (3 AIs)

    • 4 Sensors (4 AIs)

    • 5 Sensors (5 AIs)

    • 6 Sensors (6 AIs)

  • BTU Meter (AI): This option measures the heat energy in a hydrinic loop by measuring the supply and return media temperature and the volume of fluid flow for up to six locations.

    • 1 Sensor (1 AI)

    • 2 Sensors (2 AIs)

    • 3 Sensors (3 AIs)

    • 4 Sensors (4 AIs)

    • 5 Sensors (5 AIs)

    • 6 Sensors (6 AIs)