Misc Temps (Custom/Monitoring) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The selection options for Misc Temps are:

  • Cooler Temperature Sensor (AI): This option measures the temperature in up to four cooler systems.

    • 1 Sensor (1 AI)

    • 2 Sensors (2 AIs)

    • 3 Sensors (3 AIs)

    • 4 Sensors (4 AIs)

  • Freezer Temperature Sensor (AI): This option measures the temperature in up to four freezer systems.

    • 1 Sensor (1 AI)

    • 2 Sensors (2 AIs)

    • 3 Sensors (3 AIs)

    • 4 Sensors (4 AIs)

  • Pool Temperature Sensor (AI): This option measures the temperature in a pool.