Modules (Custom/Monitoring Misc Temps) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Misc Temps selections load the following modules in this Control View column:

Inputs

  • CLRX-T (Cooler X Temperature AI, where X is 1-4): This Input is loaded when the Cooler Temperature Sensor (AI) node is selected. Specific Inputs are loaded per sensor.

  • FZRX-T (Freezer X Temperature AI, where X is 1-4): This Input is loaded when the Freezer Temperature Sensor (AI) node is selected. Specific Inputs are loaded per sensor.

  • POOL-T (Pool Temperature AI): This Input is loaded when the Pool Temperature Sensor (AI) node is selected.

See the Input Modules section.