Modules (Custom/Monitoring Misc Alarm Monitoring) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Misc Alarm Monitoring selections load the following modules in this Control View column:

Inputs

  • CHEM-A (Chemical Treatment Alarm BI): This Input is loaded when the Monitor Chemical Treatment Alarm (BI) node is selected.

  • COMP-A (Compressor Alarm BI): This Input is loaded when the Monitor Compressed Air Low Pressure Switch (BI) node is selected.

  • EMGSDX-A (Emergency Shutoff X Alarm BI, where X is 1-6): This Input is loaded when the Monitor Emergency Shuttoff (BI) node is selected. Specific Inputs are loaded per shutoff valve.

  • EQUAKE-A (Earthquake Alarm BI): This Input is loaded when the Monitor Earthquake Detector (BI) node is selected.

  • FCP-A (Fire Panel Alarm BI): This Input is loaded when the Monitor Panel Alarm (BI) node is selected.

  • FCP-TBL (Fire Panel Trouble BI): This Input is loaded when the Monitor Panel Trouble (BI) node is selected.

  • GAS-A (Gas Detection Alarm BI): This Input is loaded when the Monitor Gas Detection (BI) node is selected.

  • HALON-A (Halon Alarm BI): This Input is loaded when the Monitor Halon Alarm (BI) node is selected.

  • HALON-TBL (Halon Trouble BI): This Input is loaded when the Monitor Halon Trouble (BI) node is selected.

  • MOISTX-A (Moisture Detector X Alarm BI, where X is 1-6): This Input is loaded when the Moisture Detector (BI) node is selected. Specific Inputs are loaded per detector.

  • PANICX-A (Panic Button X Alarm BI, where X is 1-6): This Input is loaded when the Panic Button (BI) node is selected. Specific Inputs are loaded per panic button.

  • REFRIG-A (Refrigerant Alarm BI): This Input is loaded when the Monitor Refrigerant Alarm (BI) node is selected.

  • SEWGX-A (Sewage Pump X Alarm BI, where X is 1-6): This Input is loaded when the Monitor Sewage Pump Alarm (BI) node is selected. Specific Inputs are loaded per pump.

  • SPX-A (Sump Pump X Alarm BI, where X is 1-6): This Input is loaded when the Monitor Sewage Pump Alarm (BI) node is selected. Specific Inputs are loaded per pump.

  • TANK-L (Tank Level AI): This Input is loaded when the Water Tank Level Sensor (AI) node is selected.

  • TANKHI-A (Tank High Level Alarm BI): This Input is loaded when the Water Tank High Level Alarm (BI) node is selected.

  • TANKLO-A (Tank High Level Alarm BI): This Input is loaded when the Water Tank Low Level Alarm (BI) node is selected.

See the Input Modules section.