Modules (Custom/Monitoring Light Items) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Light Items selections load the following modules in this Control View column:

Inputs

  • LIGHT-L (Light Level AI): This Input is loaded when the Light Level Sensor (AI) node is selected.

  • LIGHT-S (Light Level BI): This Input is loaded when the Photocell Light Sensor (BI) node is selected.

See the Input Modules section.