Modules (Custom/Monitoring Electrical Power Items) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Electrical Power Items selections load the following modules in this Control View column:

Inputs

  • ELEC-A (Electric Fault BI): This Input is loaded when the Monitor Fault (BI) node is selected.

  • ELEC-KW (Electric KW AI): This Input is loaded when the Monitor KW (AI) node is selected.

  • ELEC-KWH (Electric KWH AI): This Input is loaded when the Monitor KWH (AI) node is selected.

  • ELEC-S (Electric Status BI): This Input is loaded when the Monitor Status (BI) node is selected.

  • PHA-AMPS (Phase A Current AI), PHB-AMPS (Phase B Current AI), and PHC-AMPS (Phase C Current AI): These three Inputs are loaded when the Monitor Current (3 AI) node is selected.

  • PHA-PF (Phase A Power Factor AI), PHB-PF (Phase B Power Factor AI), and PHC-PF (Phase C Power Factor AI): These three Inputs are loaded when the Monitor Power Factor (3 AI) node is selected.

  • PHA-VOLTS (Phase A Voltage AI), PHB-VOLTS (Phase B Voltage AI), and PHC-VOLTS (Phase C Voltage AI): These three Inputs are loaded when the Monitor Voltage (3 AI) node is selected.

  • PHASE-FAIL (Electric Phase Failure BI): This Input is loaded when the Monitor Phase Failure (BI) node is selected.

See the Input Modules section.