Duct Items (Custom/Monitoring) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The selection options for Duct Items are:

  • Duct Temperature Sensor (AI): This option measures the temperature in the ductwork for up to six locations.

    • 1 Sensor (1 AI)

    • 2 Sensors (2 AIs)

    • 3 Sensors (3 AIs)

    • 4 Sensors (4 AIs)

    • 5 Sensors (5 AIs)

    • 6 Sensors (6 AIs)

  • Duct Pressure Sensor (AI): This option measures the static pressure in the ductwork.

  • High Duct Pressure Switch (BI): This option indicates when the duct static pressure exceeds the switch setting.

  • Low Duct Pressure Switch (BI): This option indicates when the duct static pressure falls below the switch setting.

  • High Duct Temperature Alarm (BI): This option indicates when the duct temperature exceeds the switch setting.

  • Low Duct Temperature Alarm (BI): This option indicates when the duct temperature falls below the switch setting.

  • Filter Status Diff Pressure Switch (BI): This option indicates when the static pressure difference across a filter exceeds the switch setting for up to six filters.

    • 1 Switch (1 BI)

    • 2 Switches (2 BIs)

    • 3 Switches (3 BIs)

    • 4 Switches (4 BIs)

    • 5 Switches (5 BIs)

    • 6 Switches (6 BIs)