Domestic Water Items (Custom/Monitoring) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The selection options for Domestic Water Items are:

  • Domestic HW Temp Sensor (AI): This option measures the temperature of the domestic hot water system.

  • Monitor Domestic HW Alarm (BI): This option indicates whether the domestic hot water system is in an alarm condition.

  • Monitor Domestic Hot Water Pump (BI): This option monitors the domestic hot water pump.

  • Monitor Domestic Water Pump (BI): This option monitors the domestic water pump.