Modules (Custom/Monitoring Domestic Water Items) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Domestic Water Items selections load the following modules in this Control View column:

Inputs

  • DHW-A (Domestic HW Temp Alarm BI): This Input is loaded when the Monitor Domestic HW Alarm (BI) node is selected.

  • DHW-T (Domestic HW Temp AI): This Input is loaded when the Domestic HW Temp Sensor (AI) node is selected.

  • DHWP-S (Domestic HW Pump Status BI): This Input is loaded when the Monitor Domestic HW Pump (BI) node is selected.

  • DWP-S (Domestic Water Pump Status BI): This Input is loaded when the Monitor Domestic Water Pump (BI) node is selected.

See the Input Modules section.