Modules (Custom/Monitoring Voltage Output) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Voltage Output selections load the following modules in this Control View column:

Outputs

  • VOLTX-O (Voltage Out X AO, where X is 1-6): This Output is loaded when the Voltage Output (AO) node is selected. Specific Outputs are loaded per sensor.

See the Output Modules section.