Command Motor (Custom/Monitoring) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The selection options for Command Motor are:

  • Command Motor (BO): This option indicates the command to the motor.

    • Status (BI): This option indicates whether the motor is running based on the motor command for up to six motors.

    • Quantity

      • One

      • Two

      • Three

      • Four

      • Five

      • Six