Command General Equipment or Lighting (Custom/Monitoring) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The selection options for Command General Equipment or Lighting are:

  • Command General Equipment or Lighting (BO): This option indicates the command to the equipment or lighting.

    • Status (BI): This option indicates whether the equipment/lighting is running/on based on the command for up to six systems.

    • Quantity

      • One

      • Two

      • Three

      • Four

      • Five

      • Six