Selecting Points for Read-Only Display - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

About this task

Selected check boxes indicate that the point is read-only. Read-only items can be viewed but not commanded on the display. The read-only option can only be edited from the Display Pages tree.

Procedure

  1. Start the tool and open the controller application.
  2. Select the Display widget.
  3. Click Edit.
  4. In the Display Pages tree, select the check box next to any point you desire to be read-only.
  5. Click Apply. The display configuration is saved. This change becomes effective after you transfer the application to the controller. See Transferring the Application of the Display Device.