Importing and Exporting Display Configuration Files - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Procedure

  1. Start the tool and open the controller application.
  2. Select the Display widget.
  3. Click Edit.
  4. Locate the Display Pages panel.
  5. Select the Export button () in the Import/Export area.
    1. Create a name and select a location for your file.
    2. Select Save. Your configuration is saved for future use.
  6. Select the Import button () in the Import/Export area..
    1. Browse to your file location and select a file.
    2. Select Open. The Display Pages tree updates based on the configuration in the file.
    Note: You will see an error message if the selected file is invalid or contains points that are not present in the current application.