Renaming a Module - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Procedure

  1. Right-click the module to rename and select Rename. The Rename dialog box appears. See the Rename (Module/Block) screen section.
    Note: You also can select a module and press the F2 key to perform this function.
  2. Type a name for the module in the User Name field.
  3. Click OK.