Viewing and Printing Application Logic - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

About this task

You can view and print application logic only in Configuration mode (Control View Connections). See the Control View Connections Option in Logic View section.

Procedure

  1. Click the Logic tab.
    Note: The Control View Connections option appears second in the list, just below the Activities folder in the Activities tree.
  2. Use the Logic View’s select, pan, and zoom options to view the application logic. See the Panning and Zooming sections for details.
  3. Use the Logic View’s Print Preview and Print options to print the logic of the entire application. See the Printing the Logic Diagram section for details.