Renaming a Block - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

About this task

We typically do not recommend renaming logic blocks because their names identify their function. You may wish to rename a Container logic block (Activity or Hybrid Activity) to identify the logic it contains.

To rename a block in the Logic View:

Procedure

  1. Right-click the block to rename and select Rename. The Rename dialog box appears. See the Rename (Module/Block) screen section.
    Note: You also can select a block and press the F2 key to perform this function.
  2. Type a name for the block in the User Name field.
  3. Click OK.