Disabling Peer-to-Peer Communication - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

About this task

To disable peer-to-peer communication:

Procedure

  1. View the details of the Network Input or Network Output.
  2. Click Edit.
  3. In the Peer Reference section, select the Peer to Peer Disabled option in the Object Identifier drop-down menu.
  4. Click Apply, and then click Close.