Changing a Column Label - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Procedure

  1. Click the State Tables tab. The State Tables tab appears with the system’s state selection data populated within tables in the right pane, and the states in the left pane of the tab. The panes allow you to scroll both vertically and horizontally, keeping the first column visible. See the State Selection (State Tables Tab) screen section.
  2. Click Edit.
  3. Right-click the column header and select Change Column Label. The Rename/Name dialog box appears.
    Note: We recommend leaving the label field empty so that dynamic naming may be used.
  4. Type a name in the Name field.
  5. Click OK.
  6. Click Apply.