Adding a Table to the State Selection Tables - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Procedure

  1. Click the State Tables tab. The State Tables tab appears with the system’s state selection data populated within tables in the right pane, and the states in the left pane of the tab. The panes allow you to scroll both vertically and horizontally, keeping the first column visible. See the State Selection (State Tables Tab) screen section.
  2. Click Edit.
  3. Right-click the module name (table heading: yellow = connected or orange = not connected) and select Create State Selection Table. The Create State Selection Table dialog box appears.
  4. Type a name in the Name field.
    Note: We recommend leaving this field empty so that dynamic naming may be used.
  5. Select a priority for the table.
    Note: Selecting 0 places the table at the top of the list, thus giving it the highest priority in the list.
  6. Select the type of data for the table (Enumeration or Boolean).
  7. Click OK.
  8. Click Apply.