Custom Modification Example - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

About this task

For example, you may want to add lighting control to a Mixed Air Single Duct Air Handling Unit application where the lights turn on/off when the AHU turns on/off.

To add lighting control to a Mixed Air Single Duct Air Handling Unit application:

Procedure

  1. With your MASD application open, add the Output Control Lighting module and the LIGHT-C Output module (Figure 1).
    Figure 1. MASD Application with Lighting Module and LIGHT-C Output

  2. Select the Lighting Output Control module and click the Connections tab.
  3. Right-click the Present Value output and select Make Connection. The Select Reference dialog box appears (Figure 2).
  4. In the Filter box, type Light and select LIGHT-C. On the right pane, select I1 (Figure 2).
    Figure 2. Viewing and Making Connections (Lighting/LIGHT-C)

  5. Click OK. The connection appears in the Destination section (Figure 3).
    Figure 3. Lighting/LIGHT-C Connection Complete

  6. Click State Tables and add a Lighting column.
    1. Click Edit.
    2. Right-click State Tables and select Create State Selection Column. The Create State Selection Column dialog box appears (Figure 4).
    3. In the Name box, type Lighting and click OK.
    Figure 4. Adding Lighting Column to the State Tables

  7. In the Start Stop Sequencing DA-T table, click Edit and set the Lighting to Off when the State is Off and On when the State is On.
    Figure 5. Start Stop Sequencing DA-T and Lighting State Table Configuration

  8. Click Apply.
  9. Click Connections and Show All. In the State Selection Output column, right-click Lighting [undefined] and click Make Connection. In the Select Reference dialog box that appears, select Lighting, and then select Input in the right pane to connect the Lighting output to the Output Control Lighting module.
    Figure 6. Viewing and Making Connections (State Selection/Lighting)

    Figure 7. State Selection/Lighting Connection Complete