This topic explains how to implement the Output Override Monitoring feature.
Effective Command inputs monitor the current command and the priority of the current command to an output object and make these values available for use within the application. These values are currently used by the Override Monitoring feature that prevents PID logic blocks from winding up and tuning incorrectly when the actual control outputs are overridden.
Scenarios where you might want to add an Effective Command input for an output include:
-
when a system has more stages than are currently supported by the application. An example of this scenario is a unit with more than eight stages of cooling. This configuration requires that you manually add extra binary outputs for the additional stages. Then, you must replace the MSC 08 module with the appropriate MSC for the actual number of stages present in your application (up to 12 stages). To add override monitoring for the additional stages, you must add Effective Command inputs to match the new binary outputs you just added.
-
when you need to add a custom control loop. We recommended you select a Sideloop for a custom control loop. Even if the logic within the sideloop is not complete enough to meet the specification for your application, the override monitoring feature for the outputs is automatically added. Then, you can modify the logic that enables the control loop to meet the specification.
If a loop requires that you manually add an analog output, and you want to use the override monitoring feature, you must add an associated Effective Command input to the Miscellaneous Inputs column of the Control View to provide this feature.
To add an effective command input for an output:
- Add the output module. For detailed instructions on how to add an output to your application, see Adding an Output or Miscellaneous Output.
- Select and add the appropriate effective command miscellaneous input module using Table 1. For detailed instructions on how to add an input to your application, see Adding an Input or Miscellaneous Input.
On the left side of the table, identify the output you added in Step 1. The right side of the table indicates the criteria to use when adding the associated effective command miscellaneous input module. The table includes the following columns to help configure the input/output pair:
- Standard Name - Indicates the standard name of the module visible via the Rename dialog box.
- Name - Indicates the name of the module visible in the Output and Miscellaneous Input columns of the Control View after the module is added to the application. A value of N/A in this column indicates that there is no available input/output pair.
- Application - Indicates the Application filter to select in the Input Selection and Output Selection dialog boxes.
-
Function - Indicates the Function filter to select in the Input Selection and Output Selection dialog boxes.
To add more than one input/output pair, the output must have a unique standard name within the application (visible via the Rename dialog box).
- Verify that the Object Identifier of the miscellaneous input module matches that of the associated output module by viewing the Object Identifier attribute in the Details dialog box for both modules.
|
Output Configuration |
Miscellaneous Input Configuration |
||||||
|---|---|---|---|---|---|---|---|
| Standard Name | Name | Application | Function | Standard Name | Name | Application | Function |
| 2 Pipe Circulation Pump 1 BO | HCP1-C | 2 Pipe Circulation Pump 1 | Command | ||||
| 2 Pipe Circulation Pump 2 BO | HCP2-C | 3 Pipe Circulation Pump 2 | Command | ||||
|
Blr1 AO |
BLR1-O |
Boiler1 |
Output |
Eff Blr1 Cmd |
BLR1-% |
Blr1 |
Effective Command |
|
Blr1 BO |
BLR1-C |
Boiler1 |
Command |
N/A |
|||
|
Blr1 Pump AO |
BP1-O |
Boiler1 Circ Pmp |
Output |
Eff Blr1 Pump Cmd |
BP1-% |
Boiler1 Circ Pmp |
Effective Command |
|
Blr1 Pump BO |
BP1-C |
Boiler1 Circ Pmp |
Command |
N/A |
|||
|
Blr1 BO |
BLR1-EN |
Boiler1 Ena |
Command |
N/A |
|||
|
Blr1 Iso Valve BO |
BLR1ISOV-C |
Boiler1 Iso Valve |
Command |
N/A |
|||
|
Boiler 1 SP AO |
BLR1SP-O |
Boiler1 SP |
Output |
N/A |
|||
|
Blr2 AO |
BLR2-O |
Boiler2 |
Output |
Eff Blr2 Cmd |
BLR2-% |
Blr2 |
Effective Command |
|
Blr2 BO |
BLR2-C |
Boiler2 |
Command |
N/A |
|||
|
Blr2 Pump AO |
BP2-O |
Boiler2 Circ Pmp |
Output |
Eff Blr2 Pump Cmd |
BP2-% |
Boiler2 Circ Pmp |
Effective Command |
|
Blr2 Pump BO |
BP2-C |
Boiler2 Circ Pmp |
Command |
N/A |
|||
|
Blr2 BO |
BLR2-EN |
Boiler2 Ena |
Command |
N/A |
|||
|
Blr2 Iso Valve BO |
BLR2ISOV-C |
Boiler2 Iso Valve |
Command |
N/A |
|||
|
Boiler 2 SP AO |
BLR2SP-O |
Boiler2 SP |
Output |
N/A |
|||
|
Blr3 AO |
BLR3-O |
Boiler3 |
Output |
Eff Blr3 Cmd |
BLR3-% |
Blr3 |
Effective Command |
|
Blr3 BO |
BLR3-C |
Boiler3 |
Command |
N/A |
|||
|
Blr3 Pump AO |
BP3-O |
Boiler3 Circ Pmp |
Output |
Eff Blr3 Pump Cmd |
BP3-% |
Boiler3 Circ Pmp |
Effective Command |
|
Blr3 Pump BO |
BP3-C |
Boiler3 Circ Pmp |
Command |
N/A |
|||
|
Blr3 BO |
BLR3-EN |
Boiler3 Ena |
Command |
N/A |
|||
|
Blr3 Iso Valve BO |
BLR3ISOV-C |
Boiler3 Iso Valve |
Command |
N/A |
|||
|
Boiler 3 SP AO |
BLR3SP-O |
Boiler3 SP |
Output |
N/A |
|||
|
Blr4 AO |
BLR4-O |
Boiler4 |
Output |
Eff Blr4 Cmd |
BLR4-% |
Blr4 |
Effective Command |
|
Blr4 BO |
BLR4-C |
Boiler4 |
Command |
N/A |
|||
|
Blr4 Pump AO |
BP4-O |
Boiler4 Circ Pmp |
Output |
Eff Blr4 Pump Cmd |
BP4-% |
Boiler4 Circ Pmp |
Effective Command |
|
Blr4 Pump BO |
BP4-C |
Boiler4 Circ Pmp |
Command |
N/A |
|||
|
Blr4 BO |
BLR4-EN |
Boiler4 Ena |
Command |
N/A |
|||
|
Blr4 Iso Valve BO |
BLR4ISOV-C |
Boiler4 Iso Valve |
Command |
N/A |
|||
|
Boiler 4 SP AO |
BLR4SP-O |
Boiler4 SP |
Output |
N/A |
|||
|
Blr5 AO |
BLR5-O |
Boiler5 |
Output |
Eff Blr5 Cmd |
BLR5-% |
Blr5 |
Effective Command |
|
Blr5 BO |
BLR5-C |
Boiler5 |
Command |
N/A |
|||
|
Blr5 Pump AO |
BP5-O |
Boiler5 Circ Pmp |
Output |
Eff Blr5 Pump Cmd |
BP5-% |
Boiler5 Circ Pmp |
Effective Command |
|
Blr5 Pump BO |
BP5-C |
Boiler5 Circ Pmp |
Command |
N/A |
|||
|
Blr5 BO |
BLR5-EN |
Boiler5 Ena |
Command |
N/A |
|||
|
Blr5 Iso Valve BO |
BLR5ISOV-C |
Boiler5 Iso Valve |
Command |
N/A |
|||
|
Boiler 5 SP AO |
BLR5SP-O |
Boiler5 SP |
Output |
N/A |
|||
|
Blr6 AO |
BLR6-O |
Boiler6 |
Output |
Eff Blr6 Cmd |
BLR6-% |
Blr6 |
Effective Command |
|
Blr6 BO |
BLR6-C |
Boiler6 |
Command |
N/A |
|||
|
Blr6 Pump AO |
BP6-O |
Boiler6 Circ Pmp |
Output |
Eff Blr6 Pump Cmd |
BP6-% |
Boiler6 Circ Pmp |
Effective Command |
|
Blr6 Pump BO |
BP6-C |
Boiler6 Circ Pmp |
Command |
N/A |
|||
|
Blr6 BO |
BLR6-EN |
Boiler6 Ena |
Command |
N/A |
|||
|
Blr6 Iso Valve BO |
BLR6ISOV-C |
Boiler6 Iso Valve |
Command |
N/A |
|||
|
Boiler 6 SP AO |
BLR6SP-O |
Boiler6 SP |
Output |
N/A |
|||
|
Blr7 AO |
BLR7-O |
Boiler7 |
Output |
Eff Blr7 Cmd |
BLR7-% |
Blr7 |
Effective Command |
|
Blr7 BO |
BLR7-C |
Boiler7 |
Command |
N/A |
|||
|
Blr7 Pump AO |
BP7-O |
Boiler7 Circ Pmp |
Output |
Eff Blr7 Pump Cmd |
BP7-% |
Boiler7 Circ Pmp |
Effective Command |
|
Blr7 Pump BO |
BP7-C |
Boiler7 Circ Pmp |
Command |
N/A |
|||
|
Blr7 BO |
BLR7-EN |
Boiler7 Ena |
Command |
N/A |
|||
|
Blr7 Iso Valve BO |
BLR7ISOV-C |
Boiler7 Iso Valve |
Command |
N/A |
|||
|
Boiler 7 SP AO |
BLR7SP-O |
Boiler7 SP |
Output |
N/A |
|||
|
Blr8 AO |
BLR8-O |
Boiler8 |
Output |
Eff Blr8 Cmd |
BLR8-% |
Blr8 |
Effective Command |
|
Blr8 BO |
BLR8-C |
Boiler8 |
Command |
N/A |
|||
|
Blr8 Pump AO |
BP8-O |
Boiler8 Circ Pmp |
Output |
Eff Blr8 Pump Cmd |
BP8-% |
Boiler8 Circ Pmp |
Effective Command |
|
Blr8 Pump BO |
BP8-C |
Boiler8 Circ Pmp |
Command |
N/A |
|||
|
Blr8 BO |
BLR8-EN |
Boiler8 Ena |
Command |
N/A |
|||
|
Blr8 Iso Valve BO |
BLR8ISOV-C |
Boiler8 Iso Valve |
Command |
N/A |
|||
|
Boiler 8 SP AO |
BLR8SP-O |
Boiler8 SP |
Output |
N/A |
|||
|
Box Heating 2 Position BO |
HTG-C |
Box Heating |
Command |
Eff Box Heating 2 Position Binary Cmd |
HTG-EC |
Box Heating 2 Position |
Effective Vlv Command |
|
Box Heating Stage 1 BO |
HTG1-C |
Box Heating |
Stage 1 Command |
Eff Box Heating Stage 1 Binary Cmd |
HTG1-EC |
Box Heating Stage 1 |
Effective Stg Command |
|
Box Heating Stage 2 BO |
HTG2-C |
Box Heating |
Stage 2 Command |
Eff Box Heating Stage 2 Binary Cmd |
HTG2-EC |
Box Heating Stage 2 |
Effective Stg Command |
|
Box Heating Stage 3 BO |
HTG3-C |
Box Heating |
Stage 3 Command |
Eff Box Heating Stage 3 Binary Cmd |
HTG3-EC |
Box Heating Stage 3 |
Effective Stg Command |
|
Box Heating Valve AO |
HTG-O |
Box Heating |
Output |
Eff Box Heating Valve Cmd |
HTG-% |
Box Heating |
Effective Command |
|
Box Heating Valve PAO |
HTG-O |
Box Heating |
Output_PAO |
Eff Box Heating Valve Cmd |
HTG-% |
Box Heating |
Effective Command |
|
Box Heating Enable BO |
HTG-EN |
Box Heating Enable |
Command |
N/A |
|||
|
HW Bypass Valve AO |
BYPV-O |
Bypass Loop |
Output |
Eff HW Bypass Valve Cmd |
BYPV-% |
HW Bypass Valve |
Effective Command |
|
Calibration Solenoid BO |
ACSOL-C |
Calibration |
Command |
N/A |
|||
|
Chiller 1 CHW Iso Valve BO |
CH1CHWISOV -C |
Chiller 1 CHW Iso Valve |
Command |
N/A |
|||
|
Chiller 1 CW Iso Valve BO |
CH1CWISOV-C |
Chiller 1 CW Iso Valve |
Command |
N/A |
|||
|
Chiller 2 CHW Iso Valve BO |
CH2CHWISOV-C |
Chiller 2 CHW Iso Valve |
Command |
N/A |
|||
|
Chiller 2 CW Iso Valve BO |
CH2CWISOV-C |
Chiller 2 CW Iso Valve |
Command |
N/A |
|||
|
Chiller 3 CHW Iso Valve BO |
CH3CHWISOV-C |
Chiller 3 CHW Iso Valve |
Command |
N/A |
|||
|
Chiller 3 CW Iso Valve BO |
CH3CWISOV-C |
Chiller 3 CW Iso Valve |
Command |
N/A |
|||
|
Chiller 4 CHW Iso Valve BO |
CH4CHWISOV-C |
Chiller 4 CHW Iso Valve |
Command |
N/A |
|||
|
Chiller 4 CW Iso Valve BO |
CH4CWISOV-C |
Chiller 4 CW Iso Valve |
Command |
N/A |
|||
|
Chiller 5 CHW Iso Valve BO |
CH5CHWISOV-C |
Chiller 5 CHW Iso Valve |
Command |
N/A |
|||
|
Chiller 5 CW Iso Valve BO |
CH5CWISOV-C |
Chiller 5 CW Iso Valve |
Command |
N/A |
|||
|
Chiller 6 CHW Iso Valve BO |
CH6CHWISOV-C |
Chiller 6 CHW Iso Valve |
Command |
N/A |
|||
|
Chiller 6 CW Iso Valve BO |
CH6CWISOV-C |
Chiller 6 CW Iso Valve |
Command |
N/A |
|||
|
Chiller 7 CHW Iso Valve BO |
CH7CHWISOV-C |
Chiller 7 CHW Iso Valve |
Command |
N/A |
|||
|
Chiller 7 CW Iso Valve BO |
CH7CWISOV-C |
Chiller 7 CW Iso Valve |
Command |
N/A |
|||
|
Chiller 8 CHW Iso Valve BO |
CH8CHWISOV-C |
Chiller 8 CHW Iso Valve |
Command |
N/A |
|||
|
Chiller 8 CW Iso Valve BO |
CH8CWISOV-C |
Chiller 8 CW Iso Valve |
Command |
N/A |
|||
|
Chlr1 BO |
CH1-EN |
Chiller1 |
Command |
N/A |
|||
|
Chlr1 CHW ISO Valve AO |
CH1CHWISOV-O |
Chiller1 CHW Iso Valve |
Output |
N/A |
|||
|
Chlr1 CHW Iso Valve BO |
CH1CHWISOV-C |
Chiller1 CHW Iso Valve |
Command |
N/A |
|||
|
Chlr1 Curr Limit AO |
CH1CL-O |
Chiller1 CurrLim |
Output |
Eff Chlr1 Curr Limit Cmd |
CH1CL-% |
Chlr1 Curr Limit |
Effective Command |
|
Chlr1 CW ISO Valve AO |
CH1CWISOV-O |
Chiller1 CW Iso Valve |
Output |
N/A |
|||
|
Chlr1 CW Iso Valve BO |
CH1CWISOV-C |
Chiller1 CW Iso Valve |
Command |
N/A |
|||
|
Chlr1 Setpoint AO |
CH1SP-O |
Chiller1 Setpoint |
Output |
Eff Chlr1 Setpoint Cmd |
CH1SP-% |
Chlr1 Setpoint |
Effective Command |
|
Chlr2 BO |
CH2-EN |
Chiller2 |
Command |
N/A |
|||
|
Chlr2 CHW ISO Valve AO |
CH2CHWISOV-O |
Chiller2 CHW Iso Valve |
Output |
N/A |
|||
|
Chlr2 CHW Iso Valve BO |
CH2CHWISOV-C |
Chiller2 CHW Iso Valve |
Command |
N/A |
|||
|
Chlr2 Curr Limit AO |
CH2CL-O |
Chiller2 CurrLim |
Output |
Eff Chlr2 Curr Limit Cmd |
CH2CL-% |
Chlr2 Curr Limit |
Effective Command |
|
Chlr2 CW ISO Valve AO |
CH2CWISOV-O |
Chiller2 CW Iso Valve |
Output |
N/A |
|||
|
Chlr2 CW Iso Valve BO |
CH2CWISOV-C |
Chiller2 CW Iso Valve |
Command |
N/A |
|||
|
Chlr2 Setpoint AO |
CH2SP-O |
Chiller2 Setpoint |
Output |
Eff Chlr2 Setpoint Cmd |
CH2SP-% |
Chlr2 Setpoint |
Effective Command |
|
Chlr3 BO |
CH3-EN |
Chiller3 |
Command |
N/A |
|||
|
Chlr3 CHW ISO Valve AO |
CH3CHWISOV-O |
Chiller3 CHW Iso Valve |
Output |
N/A |
|||
|
Chlr3 CHW Iso Valve BO |
CH3CHWISOV-C |
Chiller3 CHW Iso Valve |
Command |
N/A |
|||
|
Chlr3 Curr Limit AO |
CH3CL-O |
Chiller3 CurrLim |
Output |
Eff Chlr3 Curr Limit Cmd |
CH3CL-% |
Chlr3 Curr Limit |
Effective Command |
|
Chlr3 CW ISO Valve AO |
CH3CWISOV-O |
Chiller3 CW Iso Valve |
Output |
N/A |
|||
|
Chlr3 CW Iso Valve BO |
CH3CWISOV-C |
Chiller3 CW Iso Valve |
Command |
N/A |
|||
|
Chlr3 Setpoint AO |
CH3SP-O |
Chiller3 Setpoint |
Output |
Eff Chlr3 Setpoint Cmd |
CH3SP-% |
Chlr3 Setpoint |
Effective Command |
|
Chlr4 BO |
CH4-EN |
Chiller4 |
Command |
N/A |
|||
|
Chlr4 CHW ISO Valve AO |
CH4CHWISOV-O |
Chiller4 CHW Iso Valve |
Output |
N/A |
|||
|
Chlr4 CHW Iso Valve BO |
CH4CHWISOV-C |
Chiller4 CHW Iso Valve |
Command |
N/A |
|||
|
Chlr4 Curr Limit AO |
CH4CL-O |
Chiller4 CurrLim |
Output |
Eff Chlr4 Curr Limit Cmd |
CH4CL-% |
Chlr4 Curr Limit |
Effective Command |
|
Chlr4 CW ISO Valve AO |
CH4CWISOV-O |
Chiller4 CW Iso Valve |
Output |
N/A |
|||
|
Chlr4 CW Iso Valve BO |
CH4CWISOV-C |
Chiller4 CW Iso Valve |
Command |
N/A |
|||
|
Chlr4 Setpoint AO |
CH4SP-O |
Chiller4 Setpoint |
Output |
Eff Chlr4 Setpoint Cmd |
CH4SP-% |
Chlr4 Setpoint |
Effective Command |
|
Chlr5 BO |
CH5-EN |
Chiller5 |
Command |
N/A |
|||
|
Chlr5 CHW ISO Valve AO |
CH5CHWISOV-O |
Chiller5 CHW Iso Valve |
Output |
N/A |
|||
|
Chlr5 CHW Iso Valve BO |
CH5CHWISOV-C |
Chiller5 CHW Iso Valve |
Command |
N/A |
|||
|
Chlr5 Curr Limit AO |
CH5CL-O |
Chiller5 CurrLim |
Output |
Eff Chlr5 Curr Limit Cmd |
CH5CL-% |
Chlr5 Curr Limit |
Effective Command |
|
Chlr5 CW ISO Valve AO |
CH5CWISOV-O |
Chiller5 CW Iso Valve |
Output |
N/A |
|||
|
Chlr5 CW Iso Valve BO |
CH5CWISOV-C |
Chiller5 CW Iso Valve |
Command |
N/A |
|||
|
Chlr5 Setpoint AO |
CH5SP-O |
Chiller5 Setpoint |
Output |
Eff Chlr5 Setpoint Cmd |
CH5SP-% |
Chlr5 Setpoint |
Effective Command |
|
Chlr6 BO |
CH6-EN |
Chiller6 |
Command |
N/A |
|||
|
Chlr6 CHW ISO Valve AO |
CH6CHWISOV-O |
Chiller6 CHW Iso Valve |
Output |
N/A |
|||
|
Chlr6 CHW Iso Valve BO |
CH6CHWISOV-C |
Chiller6 CHW Iso Valve |
Command |
N/A |
|||
|
Chlr6 Curr Limit AO |
CH6CL-O |
Chiller6 CurrLim |
Output |
Eff Chlr6 Curr Limit Cmd |
CH6CL-% |
Chlr6 Curr Limit |
Effective Command |
|
Chlr6 CW ISO Valve AO |
CH6CWISOV-O |
Chiller6 CW Iso Valve |
Output |
N/A |
|||
|
Chlr6 CW Iso Valve BO |
CH6CWISOV-C |
Chiller6 CW Iso Valve |
Command |
N/A |
|||
|
Chlr6 Setpoint AO |
CH6SP-O |
Chiller6 Setpoint |
Output |
Eff Chlr6 Setpoint Cmd |
CH6SP-% |
Chlr6 Setpoint |
Effective Command |
|
Chlr7 BO |
CH7-EN |
Chiller7 |
Command |
N/A |
|||
|
Chlr7 CHW ISO Valve AO |
CH7CHWISOV-O |
Chiller7 CHW Iso Valve |
Output |
N/A |
|||
|
Chlr7 CHW Iso Valve BO |
CH7CHWISOV-C |
Chiller7 CHW Iso Valve |
Command |
N/A |
|||
|
Chlr7 Curr Limit AO |
CH7CL-O |
Chiller7 CurrLim |
Output |
Eff Chlr7 Curr Limit Cmd |
CH7CL-% |
Chlr7 Curr Limit |
Effective Command |
|
Chlr7 CW ISO Valve AO |
CH7CWISOV-O |
Chiller7 CW Iso Valve |
Output |
N/A |
|||
|
Chlr7 CW Iso Valve BO |
CH7CWISOV-C |
Chiller7 CW Iso Valve |
Command |
N/A |
|||
|
Chlr7 Setpoint AO |
CH7SP-O |
Chiller7 Setpoint |
Output |
Eff Chlr7 Setpoint Cmd |
CH7SP-% |
Chlr7 Setpoint |
Effective Command |
|
Chlr8 BO |
CH8-EN |
Chiller8 |
Command |
N/A |
|||
|
Chlr8 CHW ISO Valve AO |
CH8CHWISOV-O |
Chiller8 CHW Iso Valve |
Output |
N/A |
|||
|
Chlr8 CHW Iso Valve BO |
CH8CHWISOV-C |
Chiller8 CHW Iso Valve |
Command |
N/A |
|||
|
Chlr8 Curr Limit AO |
CH8CL-O |
Chiller8 CurrLim |
Output |
Eff Chlr8 Curr Limit Cmd |
CH8CL-% |
Chlr8 Curr Limit |
Effective Command |
|
Chlr8 CW ISO Valve AO |
CH8CWISOV-O |
Chiller8 CW Iso Valve |
Output |
N/A |
|||
|
Chlr8 CW Iso Valve BO |
CH8CWISOV-C |
Chiller8 CW Iso Valve |
Command |
N/A |
|||
|
Chlr8 Setpoint AO |
CH8SP-O |
Chiller8 Setpoint |
Output |
Eff Chlr8 Setpoint Cmd |
CH8SP-% |
Chlr8 Setpoint |
Effective Command |
|
CHW Bypass Valve AO |
CHWBYPV-O |
CHW Bypass Loop |
Output |
Eff CHW Bypass Valve Cmd |
CHWBYPV-% |
CHW Bypass Valve |
Effective Command |
|
CD PAO Stroke Time |
PARAM-CD-ST |
Cold Deck Damper |
StrokeTime |
N/A |
|||
|
Cold Deck Damper AO |
CD-O |
Cold Deck Damper |
Output |
Eff Cold Deck Damper Cmd |
CD-% |
Cold Deck Damper |
Effective Command |
|
Cold Deck Damper PAO |
CD-O |
Cold Deck Damper |
Output_ PAO |
Eff Cold Deck Damper Cmd |
CD-% |
Cold Deck Damper |
Effective Command |
|
Cold Deck Damper PAO |
CD-O |
Cold Deck Damper |
Output_PAO_ Integrated |
Eff Cold Deck Damper Cmd |
CD-% |
Cold Deck Damper |
Effective Command |
|
Cold Deck PAO - Minimum Pulse Width |
PARAM-CD-MINP |
Cold Deck Damper |
MinPulse |
N/A |
|||
|
Combustion Damper BO |
COMBDPR-C |
Combustion Damper |
Command |
N/A |
|||
|
Compressor Stage 1 BO |
COMP1-C |
Compressor |
Stage 1 Command |
Eff Compressor Stage 1 Binary Cmd |
COMP1-EC |
Compressor Stage 1 |
Effective Stg Command |
|
Compressor Stage 2 BO |
COMP2-C |
Compressor |
Stage 2 Command |
Eff Compressor Stage 2 Binary Cmd |
COMP2-EC |
Compressor Stage 2 |
Effective Stg Command |
|
Cooling Circulation Pump 1 BO |
CP1-C |
2 Pipe Circulation Pump 1 |
Command |
||||
|
Cooling Circulation Pump 2 BO |
CP2-C |
2 Pipe Circulation Pump 2 |
Command |
||||
|
CWP1 AO |
CWP1-O |
Cond Water Pump1 |
Output |
N/A |
|||
|
CWP1 BO |
CWP1-C |
Cond Water Pump1 |
Command |
N/A |
|||
|
CWP2 AO |
CWP2-O |
Cond Water Pump2 |
Output |
N/A |
|||
|
CWP2 BO |
CWP2-C |
Cond Water Pump2 |
Command |
N/A |
|||
|
CWP3 AO |
CWP3-O |
Cond Water Pump3 |
Output |
N/A |
|||
|
CWP3 BO |
CWP3-C |
Cond Water Pump3 |
Command |
N/A |
|||
|
CWP4 AO |
CWP4-O |
Cond Water Pump4 |
Output |
N/A |
|||
|
CWP4 BO |
CWP4-C |
Cond Water Pump4 |
Command |
N/A |
|||
|
CWP5 AO |
CWP5-O |
Cond Water Pump5 |
Output |
N/A |
|||
|
CWP5 BO |
CWP5-C |
Cond Water Pump5 |
Command |
N/A |
|||
|
CWP6 AO |
CWP6-O |
Cond Water Pump6 |
Output |
N/A |
|||
|
CWP6 BO |
CWP6-C |
Cond Water Pump6 |
Command |
N/A |
|||
|
CWP7 AO |
CWP7-O |
Cond Water Pump7 |
Output |
N/A |
|||
|
CWP7 BO |
CWP7-C |
Cond Water Pump7 |
Command |
N/A |
|||
|
CWP8 AO |
CWP8-O |
Cond Water Pump8 |
Output |
N/A |
|||
|
CWP8 BO |
CWP8-C |
Cond Water Pump8 |
Command |
N/A |
|||
|
Cooling Valve AO |
CLG-O |
Cooling |
Output |
Eff Cooling Valve Cmd |
CLG-% |
Cooling Valve |
Effective Command |
|
Cooling Valve BO |
CLG-C |
Cooling |
Command |
Eff Cooling Valve Binary Cmd |
CLG-EC |
Cooling Valve |
Effective Vlv Command |
|
Cooling Valve PAO |
CLG-O |
Cooling |
Output_PAO |
Eff Cooling Valve Cmd |
CLG-% |
Cooling Valve |
Effective Command |
|
Cooling Damper AO |
CLGFBD-O |
Cooling Face & Bypass Damper |
Output |
Eff Cooling Damper Cmd |
CLGFBD-% |
Cooling Damper |
Effective Command |
|
Cooling Damper PAO |
CLGFBD-O |
Cooling Face & Bypass Damper |
Output_PAO |
Eff Cooling Damper Cmd |
CLGFBD-% |
Cooling Damper |
Effective Command |
|
Cooling Circulation Pump BO |
CP-C |
Cooling Pump |
Command |
N/A |
|||
|
Cooling Stage 1 BO |
CLG1-C |
Cooling Stage |
Stage 1 Command |
Eff Cooling Stage 1 Binary Cmd |
CLG1-EC |
Cooling Stage 1 |
Effective Stg Command |
|
Cooling Stage 2 BO |
CLG2-C |
Cooling Stage |
Stage 2 Command |
Eff Cooling Stage 2 Binary Cmd |
CLG2-EC |
Cooling Stage 2 |
Effective Stg Command |
|
Cooling Stage 3 BO |
CLG3-C |
Cooling Stage |
Stage 3 Command |
Eff Cooling Stage 3 Binary Cmd |
CLG3-EC |
Cooling Stage 3 |
Effective Stg Command |
|
Cooling Stage 4 BO |
CLG4-C |
Cooling Stage |
Stage 4 Command |
Eff Cooling Stage 4 Binary Cmd |
CLG4-EC |
Cooling Stage 4 |
Effective Stg Command |
|
Cooling Stage 5 BO |
CLG5-C |
Cooling Stage |
Stage 5 Command |
Eff Cooling Stage 5 Binary Cmd |
CLG5-EC |
Cooling Stage 5 |
Effective Stg Command |
|
Cooling Stage 6 BO |
CLG6-C |
Cooling Stage |
Stage 6 Command |
Eff Cooling Stage 6 Binary Cmd |
CLG6-EC |
Cooling Stage 6 |
Effective Stg Command |
|
Cooling Stage 7 BO |
CLG7-C |
Cooling Stage |
Stage 7 Command |
Eff Cooling Stage 7 Binary Cmd |
CLG7-EC |
Cooling Stage 7 |
Effective Stg Command |
|
Cooling Stage 8 BO |
CLG8-C |
Cooling Stage |
Stage 8 Command |
Eff Cooling Stage 8 Binary Cmd |
CLG8-EC |
Cooling Stage 8 |
Effective Stg Command |
|
Cooling Valve Command BO |
CLG-C |
Cooling Valve |
Command |
Eff Cooling Valve Binary Cmd |
CLG-EC |
Cooling Valve |
Effective Vlv Command |
|
Current Out 1 AO |
CURRENT1-O |
Current 1 |
Output |
N/A |
|||
|
Current Out 2 AO |
CURRENT2-O |
Current 2 |
Output |
N/A |
|||
|
Current Out 3 AO |
CURRENT3-O |
Current 3 |
Output |
N/A |
|||
|
Current Out 4 AO |
CURRENT4-O |
Current 4 |
Output |
N/A |
|||
|
Current Out 5 AO |
CURRENT5-O |
Current 5 |
Output |
N/A |
|||
|
Current Out 6 AO |
CURRENT6-O |
Current 6 |
Output |
N/A |
|||
|
Domestic HW Valve AO |
DHWV-O |
Domestic HW Valve |
Output |
Eff Domestic HW Valve Cmd |
DHWV-% |
Domestic HW Valve |
Effective Command |
|
Economizer Enable BO |
ECON-C |
Economizer Enable |
Command |
N/A |
|||
|
Exhaust Air Damper AO |
EAD-O |
Exhaust Air Damper |
Output |
Eff Exhaust Air Damper Cmd |
EAD-% |
Exhaust Air Damper |
Effective Command |
|
Exhaust Air Damper BO |
EAD-C |
Exhaust Air Damper |
Command |
N/A |
|||
|
Exhaust Air Damper PAO |
EAD-O |
Exhaust Air Damper |
Output_PAO |
Eff Exhaust Air Damper Cmd |
EAD-% |
Exhaust Air Damper |
Effective Command |
|
Exhaust Air Damper PAO - Minimum Pulse Width |
PARAM-EAD-MINP |
Exhaust Air Damper |
MinPulse |
N/A |
|||
|
Exhaust Damper PAO Stroke Time |
PARAM-EAD-ST |
Exhaust Air Damper |
StrokeTime |
N/A |
|||
| Exhaust Air Damper2 BO | EAD2-C | Exhaust Air Damper2 | Command | ||||
|
Exhaust Fan BO |
EF-C |
Exhaust Fan |
Command |
N/A |
|||
|
Exhaust Fan BO |
EF-C |
Exhaust Fan |
Run/Stop |
N/A |
|||
|
Exhaust Fan Speed AO |
EF-O |
Exhaust Fan |
Output |
Eff Exhaust Fan Speed Cmd |
EF-% |
Exhaust Fan Speed |
Effective Command |
|
VSD Bypass Drive BV |
EF-BYPASS |
Exhaust Fan |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
EF-RESET |
Exhaust Fan |
Reset Drive Fault |
N/A |
|||
|
Exhaust Fan2 BO |
EF2-C |
Exhaust Fan2 |
Command |
N/A |
|||
|
Exhaust Fan2 BO |
EF2-C |
Exhaust Fan2 |
Run/Stop |
N/A |
|||
|
Exhaust Fan2 Speed AO |
EF2-O |
Exhaust Fan2 |
Output |
Eff Exhaust Fan2 Speed Cmd |
EF2-% |
Exhaust Fan2 Speed |
Effective Command |
|
FBP Damper AO |
FBD-O |
Face & Bypass Damper |
Output |
Eff FBP Damper Cmd |
FBD-% |
FBP Damper |
Effective Command |
|
FBP Damper PAO |
FBD-O |
Face & Bypass Damper |
Output_PAO |
Eff FBP Damper Cmd |
FBD-% |
FBP Damper |
Effective Command |
|
Fan BO |
SF-C |
Fan |
Command |
N/A |
|||
|
Fan Speed 1 BO |
SFL-C |
Fan |
Command LO |
N/A |
|||
|
Fan Speed 2 BO |
SFM-C |
Fan |
Command MED |
N/A |
|||
|
Fan Speed 3 BO |
SFH-C |
Fan |
Command HI |
N/A |
|||
|
Fan Speed AO |
SF-O |
Fan |
Output |
N/A |
|||
|
GEF BO |
GEF-C |
GEF |
Command |
N/A |
|||
|
Heat Recovery Valve AO |
HR-O |
Heat Recovery |
Output |
Eff Heat Recovery Valve Cmd |
HR-% |
Heat Recovery Valve |
Effective Command |
|
Heat Recovery Valve BO |
HR-C |
Heat Recovery |
Command |
N/A |
|||
|
Heat Recovery Valve PAO |
HR-O |
Heat Recovery |
Output_PAO |
Eff Heat Recovery Valve Cmd |
HR-% |
Heat Recovery Valve |
Effective Command |
|
Heat Recovery Exhaust FBD AO |
HREAFBD-O |
Heat Recovery EA FBD AO |
Output |
N/A |
|||
|
Heat Recovery Exhaust FBD BO |
HREAFBD-C |
Heat Recovery EA FBD BO |
Command |
N/A |
|||
|
Heat Recovery OA FBD AO |
HROAFBD-O |
Heat Recovery OA FBD AO |
Output |
N/A |
|||
|
Heat Recovery OA FBD BO |
HROAFBD-C |
Heat Recovery OA FBD BO |
Command |
N/A |
|||
|
Heat Recovery Pump BO |
HRP-C |
Heat Recovery Pump |
Command |
N/A |
|||
|
Heat Recovery Wheel AO |
HRW-O |
Heat Recovery Wheel |
Output |
Eff Heat Recovery Wheel Cmd |
HR-% |
Heat Recovery Wheel |
Effective Command |
|
Heat Recovery Wheel BO |
HRW-C |
Heat Recovery Wheel |
Command |
N/A |
|||
|
Heat Tape 1 Command BO |
HTAPE1-C |
Heat Tape 1 |
Command |
N/A |
|||
|
Heat Tape 2 Command BO |
HTAPE2-C |
Heat Tape 2 |
Command |
N/A |
|||
|
Heat Tape 3 Command BO |
HTAPE3-C |
Heat Tape 3 |
Command |
N/A |
|||
|
Heat Tape 4 Command BO |
HTAPE4-C |
Heat Tape 4 |
Command |
N/A |
|||
|
Heat Tape 5 Command BO |
HTAPE5-C |
Heat Tape 5 |
Command |
N/A |
|||
|
Heat Tape 6 Command BO |
HTAPE6-C |
Heat Tape 6 |
Command |
N/A |
|||
|
Heating Stage 1 BO |
HTG1-C |
Heating |
Stage 1 Command |
Eff Heating Stage 1 Binary Cmd |
HTG1-EC |
Heating Stage 1 |
Effective Stg Command |
|
Heating Stage 2 BO |
HTG2-C |
Heating |
Stage 2 Command |
Eff Heating Stage 2 Binary Cmd |
HTG2-EC |
Heating Stage 2 |
Effective Stg Command |
|
Heating Stage 3 BO |
HTG3-C |
Heating |
Stage 3 Command |
Eff Heating Stage 3 Binary Cmd |
HTG3-EC |
Heating Stage 3 |
Effective Stg Command |
|
Heating Valve AO |
HTG-O |
Heating |
Output |
Eff Heating Valve Cmd |
HTG-% |
Heating Valve |
Effective Command |
|
Heating Valve BO |
HTG-C |
Heating |
Command |
Eff Heating Valve Binary Cmd |
HTG-EC |
Heating Valve |
Effective Vlv Command |
|
Heating Valve PAO |
HTG-O |
Heating |
Output_PAO |
Eff Heating Valve Cmd |
HTG-% |
Heating Valve |
Effective Command |
|
Reheat Valve 1 AO |
HTG1-O |
Heating 1 |
Output |
Eff Reheat Valve 1 Cmd |
HTG1-% |
Reheat Valve 1 |
Effective Command |
|
Reheat Valve 2 AO |
HTG2-O |
Heating 2 |
Output |
Eff Reheat Valve 2 Cmd |
HTG2-% |
Reheat Valve 2 |
Effective Command |
|
Reheat Stage 1 BO |
HTG1-C |
Heating Stage |
Stage 1 Command |
Eff Reheat Stage 1 Binary Cmd |
HTG1-EC |
Reheat Stage 1 |
Effective Stg Command |
|
Reheat Stage 2 BO |
HTG2-C |
Heating Stage |
Stage 2 Command |
Eff Reheat Stage 2 Binary Cmd |
HTG2-EC |
Reheat Stage 2 |
Effective Stg Command |
|
Reheat Stage 3 BO |
HTG3-C |
Heating Stage |
Stage 3 Command |
Eff Reheat Stage 3 Binary Cmd |
HTG3-EC |
Reheat Stage 3 |
Effective Stg Command |
|
Reheat Stage 4 BO |
HTG4-C |
Heating Stage |
Stage 4 Command |
Eff Reheat Stage 4 Binary Cmd |
HTG4-EC |
Reheat Stage 4 |
Effective Stg Command |
|
Reheat Stage 5 BO |
HTG5-C |
Heating Stage |
Stage 5 Command |
Eff Reheat Stage 5 Binary Cmd |
HTG5-EC |
Reheat Stage 5 |
Effective Stg Command |
|
Reheat Stage 6 BO |
HTG6-C |
Heating Stage |
Stage 6 Command |
Eff Reheat Stage 6 Binary Cmd |
HTG6-EC |
Reheat Stage 6 |
Effective Stg Command |
|
Reheat Stage 7 BO |
HTG7-C |
Heating Stage |
Stage 7 Command |
Eff Reheat Stage 7 Binary Cmd |
HTG7-EC |
Reheat Stage 7 |
Effective Stg Command |
|
Reheat Stage 8 BO |
HTG8-C |
Heating Stage |
Stage 8 Command |
Eff Reheat Stage 8 Binary Cmd |
HTG8-EC |
Reheat Stage 8 |
Effective Stg Command |
|
Heating Valve Command BO |
HTG-C |
Heating Valve |
Command |
Eff Heating Valve Binary Cmd |
HTG-EC |
Heating Valve |
Effective Vlv Command |
|
2 Pipe Valve AO |
HC-O |
Heating/Cooling |
Output |
Eff 2 Pipe Valve Cmd |
HC-% |
2 Pipe Valve |
Effective Command |
|
2 Pipe Valve BO |
HC-C |
Heating/Cooling |
Command |
Eff 2 Pipe Valve Binary Cmd |
HC-EC |
2 Pipe Valve |
Effective Vlv Command |
|
2 Pipe Valve PAO |
HC-O |
Heating/Cooling |
Output_PAO |
Eff 2 Pipe Valve Cmd |
HC-% |
2 Pipe Valve |
Effective Command |
|
2 Pipe Damper AO |
HCFBD-O |
Heating/Cooling Face & Bypass Damper |
Output |
Eff 2 Pipe Damper Cmd |
HCFBD-% |
2 Pipe Damper |
Effective Command |
|
2 Pipe Damper PAO |
HCFBD-O |
Heating/Cooling Face & Bypass Damper |
Output_PAO |
Eff 2 Pipe Damper Cmd |
HCFBD-% |
2 Pipe Damper |
Effective Command |
|
2 Pipe Circulation Pump BO |
HCP-C |
Heating/Cooling Pump |
Command |
N/A |
|||
|
2 Pipe Valve Command BO |
HC-C |
Heating/Cooling Valve |
Command |
Eff 2 Pipe Valve Binary Cmd |
HC-EC |
2 Pipe Valve |
Effective Vlv Command |
|
HD PAO Stroke Time |
PARAM-HD-ST |
Hot Deck Damper |
StrokeTime |
N/A |
|||
|
Hot Deck Damper AO |
HD-O |
Hot Deck Damper |
Output |
Eff Hot Deck Damper Cmd |
HD-% |
Hot Deck Damper |
Effective Command |
|
Hot Deck Damper PAO |
HD-O |
Hot Deck Damper |
Output_PAO |
Eff Hot Deck Damper Cmd |
HD-% |
Hot Deck Damper |
Effective Command |
|
Hot Deck Damper PAO |
HD-O |
Hot Deck Damper |
Output_PAO _Integrated |
Eff Hot Deck Damper Cmd |
HD-% |
Hot Deck Damper |
Effective Command |
|
Hot Deck PAO - Minimum Pulse Width |
PARAM-HD-MINP |
Hot Deck Damper |
MinPulse |
N/A |
|||
|
Hot Gas Bypass Valve BO |
HGBPV-C |
Hot Gas Bypass Valve |
Command |
N/A |
|||
|
Iso Valve BO |
ISOVLV-C |
HP Iso Valve |
Command |
N/A |
|||
|
Humidification AO |
HUM-O |
Humidifier |
Output |
Eff Humidification Cmd |
HUM-% |
Humidification |
Effective Command |
|
Humidifier Enable BO |
HUM-C |
Humidifier Enable |
Command |
N/A |
|||
|
Humidification Stage 1 BO |
HUM1-C |
Humidifier Stage |
Stage 1 Command |
Eff Humidification Stage 1 Binary Cmd |
HUM1-EC |
Humidification Stage 1 |
Effective Stg Command |
|
Humidification Stage 2 BO |
HUM2-C |
Humidifier Stage |
Stage 2 Command |
Eff Humidification Stage 2 Binary Cmd |
HUM2-EC |
Humidification Stage 2 |
Effective Stg Command |
|
Humidification Stage 3 BO |
HUM3-C |
Humidifier Stage |
Stage 3 Command |
Eff Humidification Stage 3 Binary Cmd |
HUM3-EC |
Humidification Stage 3 |
Effective Stg Command |
|
Humidification Stage 4 BO |
HUM4-C |
Humidifier Stage |
Stage 4 Command |
Eff Humidification Stage 4 Binary Cmd |
HUM4-EC |
Humidification Stage 4 |
Effective Stg Command |
|
HW Mixing Valve AO |
HXMV-O |
HX Mixing Valve |
Output |
Eff HW Mixing Valve Cmd |
MIX-% |
HW Mixing Valve |
Effective Command |
|
HX1 Iso Valve BO |
HX1ISOV-C |
HX1 Iso Valve |
Command |
N/A |
|||
|
HX1 AO1 |
HX1V1-O |
HX1 Valve 1 |
Output |
Eff HX1 Valve 1 Cmd |
HX1V1-% |
HX1 Valve 1 |
Effective Command |
|
HX1 AO2 |
HX1V2-O |
HX1 Valve 2 |
Output |
Eff HX1 Valve 2 Cmd |
HX1V2-% |
HX1 Valve 2 |
Effective Command |
|
HX2 Iso Valve BO |
HX2ISOV-C |
HX2 Iso Valve |
Command |
N/A |
|||
|
HX2 AO1 |
HX2V1-O |
HX2 Valve 1 |
Output |
Eff HX2 Valve 1 Cmd |
HX2V1-% |
HX2 Valve 1 |
Effective Command |
|
HX2 AO2 |
HX2V2-O |
HX2 Valve 2 |
Output |
Eff HX2 Valve 2 Cmd |
HX2V2-% |
HX2 Valve 2 |
Effective Command |
|
Lighting BO |
LIGHT-C |
Lighting |
Command |
N/A |
|||
|
Minimum OA Damper AO |
MOAD-O |
Min Outdoor Air Damper |
Output |
Eff Minimum OA Damper Cmd |
MOAD-% |
Minimum OA Damper |
Effective Command |
|
Minimum OA Damper BO |
MOAD-C |
Min Outdoor Air Damper |
Command |
N/A |
|||
|
Minimum OA Fan AO |
MOAF-O |
Min Outdoor Air Fan |
Output |
Eff Minimum OA Fan Cmd |
MOAF-% |
Minimum OA Fan |
Effective Command |
|
Minimum OA Fan BO |
MOAF-C |
Min Outdoor Air Fan |
Command |
N/A |
|||
|
Minimum OA Fan BO |
MOAF-C |
Min Outdoor Air Fan |
Run/Stop |
N/A |
|||
|
VSD Bypass Drive BV |
MOAF-BYPASS |
Min Outdoor Air Fan |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
MOAF-RESET |
Min Outdoor Air Fan |
Reset Drive Fault |
N/A |
|||
|
Misc 1 Command BO |
MISC1-C |
Misc 1 |
Command |
N/A |
|||
|
Misc 2 Command BO |
MISC2-C |
Misc 2 |
Command |
N/A |
|||
|
Misc 3 Command BO |
MISC3-C |
Misc 3 |
Command |
N/A |
|||
|
Misc 4 Command BO |
MISC4-C |
Misc 4 |
Command |
N/A |
|||
|
Misc 5 Command BO |
MISC5-C |
Misc 5 |
Command |
N/A |
|||
|
Misc 6 Command BO |
MISC6-C |
Misc 6 |
Command |
N/A |
|||
|
Cooling Valve PAO |
MISC-O |
Miscellaneous |
Output_PAO |
N/A |
|||
|
Mixed Air Damper AO |
MISC-O |
Miscellaneous |
Output |
Eff Mixed Air Damper Cmd |
MAD-% |
Mixed Air Damper |
Effective Command |
|
Reheat Stage 1 BO |
MISC1-C |
Miscellaneous |
Stage 1 Command |
Eff Reheat Stage 1 Binary Cmd |
MISC1-EC |
Miscellaneous |
Effective Stg Command |
|
Reheat Stage 2 BO |
MISC2-C |
Miscellaneous |
Stage 2 Command |
Eff Reheat Stage 2 Binary Cmd |
MISC2-EC |
Miscellaneous |
Effective Stg Command |
|
Reheat Stage 3 BO |
MISC3-C |
Miscellaneous |
Stage 3 Command |
Eff Reheat Stage 3 Binary Cmd |
MISC3-EC |
Miscellaneous |
Effective Stg Command |
|
Reheat Stage 4 BO |
MISC4-C |
Miscellaneous |
Stage 4 Command |
Eff Reheat Stage 4 Binary Cmd |
MISC4-EC |
Miscellaneous |
Effective Stg Command |
|
Reheat Stage 5 BO |
MISC5-C |
Miscellaneous |
Stage 5 Command |
Eff Reheat Stage 5 Binary Cmd |
MISC5-EC |
Miscellaneous |
Effective Stg Command |
|
Reheat Stage 6 BO |
MISC6-C |
Miscellaneous |
Stage 6 Command |
Eff Reheat Stage 6 Binary Cmd |
MISC6-EC |
Miscellaneous |
Effective Stg Command |
|
Reheat Stage 7 BO |
MISC7-C |
Miscellaneous |
Stage 7 Command |
Eff Reheat Stage 7 Binary Cmd |
MISC7-EC |
Miscellaneous |
Effective Stg Command |
|
Reheat Stage 8 BO |
MISC8-C |
Miscellaneous |
Stage 8 Command |
Eff Reheat Stage 8 Binary Cmd |
MISC8-EC |
Miscellaneous |
Effective Stg Command |
|
Supply Fan BO |
MISC-C |
Miscellaneous |
Command |
N/A |
|||
|
Mixed Air Damper AO |
MAD-O |
Mixed Air Damper |
Output |
Eff Mixed Air Damper Cmd |
MAD-% |
Mixed Air Damper |
Effective Command |
|
HW Mixing Valve AO |
MIX-O |
Mixing Valve |
Output |
Eff Mixing Valve Cmd |
MIX-% |
Mixing Valve |
Effective Command |
|
Motor 1 Command BO |
MOTOR1-C |
Motor 1 |
Command |
N/A |
|||
|
Motor 2 Command BO |
MOTOR2-C |
Motor 2 |
Command |
N/A |
|||
|
Motor 3 Command BO |
MOTOR3-C |
Motor 3 |
Command |
N/A |
|||
|
Motor 4 Command BO |
MOTOR4-C |
Motor 4 |
Command |
N/A |
|||
|
Motor 5 Command BO |
MOTOR5-C |
Motor 5 |
Command |
N/A |
|||
|
Motor 6 Command BO |
MOTOR6-C |
Motor 6 |
Command |
N/A |
|||
|
OA Damper AO |
OAD-O |
Outdoor Air Damper |
Output |
Eff OA Damper Cmd |
OAD-% |
OA Damper |
Effective Command |
|
OA Damper BO |
OAD-C |
Outdoor Air Damper |
Command |
N/A |
|||
|
OA Damper2 BO |
OAD2-C |
OA Damper2 |
Command |
N/A |
|||
|
Fan BO |
SF-C |
Parallel Supply Fan |
Command |
N/A |
|||
|
PCHWP 1 AO |
PCHWP1-O |
PCHWP1 |
Output |
Eff PCHWP 1 Cmd |
PCHWP1-% |
PCHWP 1 |
Effective Command |
|
PCHWP1 BO |
PCHWP1-C |
PCHWP1 |
Command |
N/A |
|||
|
PCHWP 2 AO |
PCHWP2-O |
PCHWP2 |
Output |
Eff PCHWP 2 Cmd |
PCHWP2-% |
PCHWP 2 |
Effective Command |
|
PCHWP2 BO |
PCHWP2-C |
PCHWP2 |
Command |
N/A |
|||
|
PCHWP 3 AO |
PCHWP3-O |
PCHWP3 |
Output |
Eff PCHWP 3 Cmd |
PCHWP3-% |
PCHWP 3 |
Effective Command |
|
PCHWP3 BO |
PCHWP3-C |
PCHWP3 |
Command |
N/A |
|||
|
PCHWP 4 AO |
PCHWP4-O |
PCHWP4 |
Output |
Eff PCHWP 4 Cmd |
PCHWP4-% |
PCHWP 4 |
Effective Command |
|
PCHWP4 BO |
PCHWP4-C |
PCHWP4 |
Command |
N/A |
|||
|
PCHWP 5 AO |
PCHWP5-O |
PCHWP5 |
Output |
Eff PCHWP 5 Cmd |
PCHWP5-% |
PCHWP 5 |
Effective Command |
|
PCHWP5 BO |
PCHWP5-C |
PCHWP5 |
Command |
N/A |
|||
|
PCHWP 6 AO |
PCHWP6-O |
PCHWP6 |
Output |
Eff PCHWP 6 Cmd |
PCHWP6-% |
PCHWP 6 |
Effective Command |
|
PCHWP6 BO |
PCHWP6-C |
PCHWP6 |
Command |
N/A |
|||
|
PCHWP 7 AO |
PCHWP7-O |
PCHWP7 |
Output |
Eff PCHWP 7 Cmd |
PCHWP7-% |
PCHWP 7 |
Effective Command |
|
PCHWP7 BO |
PCHWP7-C |
PCHWP7 |
Command |
N/A |
|||
|
PCHWP 8 AO |
PCHWP8-O |
PCHWP8 |
Output |
Eff PCHWP 8 Cmd |
PCHWP8-% |
PCHWP 8 |
Effective Command |
|
PCHWP8 BO |
PCHWP8-C |
PCHWP8 |
Command |
N/A |
|||
|
PHWP1 AO |
PHWP1-O |
PHWP1 |
Output |
Eff PHWP1 Cmd |
PHWP1-% |
PHWP1 |
Effective Command |
|
PHWP1 BO |
PHWP1-C |
PHWP1 |
Command |
N/A |
|||
|
PHWP2 AO |
PHWP2-O |
PHWP2 |
Output |
Eff PHWP2 Cmd |
PHWP2-% |
PHWP2 |
Effective Command |
|
PHWP2 BO |
PHWP2-C |
PHWP2 |
Command |
N/A |
|||
|
PHWP3 AO |
PHWP3-O |
PHWP3 |
Output |
Eff PHWP3 Cmd |
PHWP3-% |
PHWP3 |
Effective Command |
|
PHWP3 BO |
PHWP3-C |
PHWP3 |
Command |
N/A |
|||
|
PHWP4 AO |
PHWP4-O |
PHWP4 |
Output |
Eff PHWP4 Cmd |
PHWP4-% |
PHWP4 |
Effective Command |
|
PHWP4 BO |
PHWP4-C |
PHWP4 |
Command |
N/A |
|||
|
PHWP5 AO |
PHWP5-O |
PHWP5 |
Output |
Eff PHWP5 Cmd |
PHWP5-% |
PHWP5 |
Effective Command |
|
PHWP5 BO |
PHWP5-C |
PHWP5 |
Command |
N/A |
|||
|
PHWP6 AO |
PHWP6-O |
PHWP6 |
Output |
Eff PHWP6 Cmd |
PHWP6-% |
PHWP6 |
Effective Command |
|
PHWP6 BO |
PHWP6-C |
PHWP6 |
Command |
N/A |
|||
|
PHWP7 AO |
PHWP7-O |
PHWP7 |
Output |
Eff PHWP7 Cmd |
PHWP7-% |
PHWP7 |
Effective Command |
|
PHWP7 BO |
PHWP7-C |
PHWP7 |
Command |
N/A |
|||
|
PHWP8 AO |
PHWP8-O |
PHWP8 |
Output |
Eff PHWP8 Cmd |
PHWP8-% |
PHWP8 |
Effective Command |
|
PHWP8 BO |
PHWP8-C |
PHWP8 |
Command |
N/A |
|||
|
Preheat Valve AO |
PH-O |
Preheat |
Output |
Eff Preheat Valve Cmd |
PH-% |
Preheat Valve |
Effective Command |
|
Preheat Valve BO |
PH-C |
Preheat |
Command |
Eff Preheat Valve Binary Cmd |
PH-EC |
Preheat Valve |
Effective Vlv Command |
|
Preheat Valve PAO |
PH-O |
Preheat |
Output_PAO |
Eff Preheat Valve Cmd |
PH-% |
Preheat Valve |
Effective Command |
|
Preheat Valve 1 AO |
PH1-O |
Preheat 1 |
Output |
Eff Preheat Valve 1 Cmd |
PH1-% |
Preheat Valve 1 |
Effective Command |
|
Preheat Valve 2 AO |
PH2-O |
Preheat 2 |
Output |
Eff Preheat Valve 2 Cmd |
PH2-% |
Preheat Valve 2 |
Effective Command |
|
Preheat Enable BO |
PH-EN |
Preheat Enable |
Command |
N/A |
|||
|
Preheat Damper AO |
PHFBD-O |
Preheat Face & Bypass Damper |
Output |
Eff Preheat Damper Cmd |
PHFBD-% |
Preheat Damper |
Effective Command |
|
Preheat Damper PAO |
PHFBD-O |
Preheat Face & Bypass Damper |
Output_PAO |
Eff Preheat Damper Cmd |
PHFBD-% |
Preheat Damper |
Effective Command |
|
Preheat Circulation Pump BO |
PHP-C |
Preheat Pump |
Command |
N/A |
|||
|
Preheat Circulation Pump 1 BO |
PHP1-C |
Preheat Circulation Pump 1 |
Command |
N/A |
|||
|
Preheat Circulation Pump 2 BO |
PHP2-C |
Preheat Circulation Pump 2 |
Command |
N/A |
|||
|
Preheat Stage 1 BO |
PH1-C |
Preheat Stage |
Stage 1 Command |
Eff Preheat Stage 1 Binary Cmd |
PH1-EC |
Preheat Stage 1 |
Effective Stg Command |
|
Preheat Stage 2 BO |
PH2-C |
Preheat Stage |
Stage 2 Command |
Eff Preheat Stage 2 Binary Cmd |
PH2-EC |
Preheat Stage 2 |
Effective Stg Command |
|
Preheat Stage 3 BO |
PH3-C |
Preheat Stage |
Stage 3 Command |
Eff Preheat Stage 3 Binary Cmd |
PH3-EC |
Preheat Stage 3 |
Effective Stg Command |
|
Preheat Stage 4 BO |
PH4-C |
Preheat Stage |
Stage 4 Command |
Eff Preheat Stage 4 Binary Cmd |
PH4-EC |
Preheat Stage 4 |
Effective Stg Command |
|
Preheat Stage 5 BO |
PH5-C |
Preheat Stage |
Stage 5 Command |
Eff Preheat Stage 5 Binary Cmd |
PH5-EC |
Preheat Stage 5 |
Effective Stg Command |
|
Preheat Stage 6 BO |
PH6-C |
Preheat Stage |
Stage 6 Command |
Eff Preheat Stage 6 Binary Cmd |
PH6-EC |
Preheat Stage 6 |
Effective Stg Command |
|
Preheat Stage 7 BO |
PH7-C |
Preheat Stage |
Stage 7 Command |
Eff Preheat Stage 7 Binary Cmd |
PH7-EC |
Preheat Stage 7 |
Effective Stg Command |
|
Preheat Stage 8 BO |
PH8-C |
Preheat Stage |
Stage 8 Command |
Eff Preheat Stage 8 Binary Cmd |
PH8-EC |
Preheat Stage 8 |
Effective Stg Command |
|
Reheat Valve AO |
RH-O |
Reheat |
Output |
Eff Reheat Valve Cmd |
RH-% |
Reheat Valve |
Effective Command |
|
Reheat Valve PAO |
RH-O |
Reheat |
Output_PAO |
Eff Reheat Valve Cmd |
RH-% |
Reheat Valve |
Effective Command |
|
Reheat Enable BO |
RF-EN |
Reheat Enable |
Command |
N/A |
|||
|
Reheat Circulation Pump BO |
RHP-C |
Reheat Pump |
Command |
N/A |
|||
|
Reheat Circulation Pump 1 BO |
RHP1-C |
Reheat Circulation Pump 1 |
Command |
N/A |
|||
|
Reheat Circulation Pump 2 BO |
RHP2-C |
Reheat Circulation Pump 2 |
Command |
N/A |
|||
|
Relief Fan BO |
RLF-C |
Relief Fan |
Command |
N/A |
|||
|
Relief Fan BO |
RLF-C |
Relief Fan |
Run/Stop |
N/A |
|||
|
Relief Fan Speed AO |
RLF-O |
Relief Fan |
Output |
Eff Relief Fan Speed Cmd |
RLF-% |
Relief Fan Speed |
Effective Command |
|
VSD Bypass Drive BV |
RLF-BYPASS |
Relief Fan |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
RLF-RESET |
Relief Fan |
Reset Drive Fault |
N/A |
|||
|
Relief Fan2 BO |
RLF2-C |
Relief Fan2 |
Command |
N/A |
|||
|
Relief Fan2 BO |
RLF2-C |
Relief Fan2 |
Run/Stop |
N/A |
|||
|
Relief Fan2 Speed AO |
RLF2-O |
Relief Fan2 |
Output |
Eff Relief Fan2 Speed Cmd |
RLF2-% |
Relief Fan2 Speed |
Effective Command |
|
Return Air Damper AO |
RAD-O |
Return Air Damper |
Output |
Eff Return Air Damper Cmd |
RAD-% |
Return Air Damper |
Effective Command |
|
Return Fan BO |
RF-C |
Return Fan |
Command |
N/A |
|||
|
Return Fan BO |
RF-C |
Return Fan |
Run/Stop |
N/A |
|||
|
Return Fan Speed AO |
RF-O |
Return Fan |
Output |
Eff Return Fan Speed Cmd |
RF-% |
Return Fan Speed |
Effective Command |
|
VSD Bypass Drive BV |
RF-BYPASS |
Return Fan |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
RF-RESET |
Return Fan |
Reset Drive Fault |
N/A |
|||
|
Return Fan2 BO |
RF2-C |
Return Fan2 |
Command |
N/A |
|||
|
Return Fan2 BO |
RF2-C |
Return Fan2 |
Run/Stop |
N/A |
|||
|
Return Fan2 Speed AO |
RF2-O |
Return Fan2 |
Output |
Eff Return Fan2 Speed Cmd |
RF2-% |
Return Fan2 Speed |
Effective Command |
|
Reversing Valve 1 BO |
REV1-C |
Reversing Valve 1 |
Binary Output |
N/A |
|||
|
Reversing Valve 2 BO |
REV2-C |
Reversing Valve 2 |
Binary Output |
N/A |
|||
|
Sand Filter Command BO |
SANDFILT-C |
Sand Filter |
Command |
N/A |
|||
|
Drain Valve BO |
HDV-C |
Scrubber Drain |
Command |
N/A |
|||
|
Fill Valve BO |
HFV-C |
Scrubber Fill |
Command |
N/A |
|||
|
SCHWP1 AO |
SCHWP1-O |
Sec CHW Pump1 |
Output |
Eff SCHWP1 Cmd |
SCHWP1-% |
SCHWP1 |
Effective Command |
|
SCHWP1 BO |
SCHWP1-C |
Sec CHW Pump1 |
Command |
Eff SCHWP1 Binary Cmd |
SCHWP1-EC |
SCHWP1 |
Effective Stg Command |
|
VSD Bypass Drive BV |
SCHWP1-BYPASS |
Sec CHW Pump1 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
SCHWP1-RESET |
Sec CHW Pump1 |
Reset Drive Fault |
N/A |
|||
|
SCHWP2 AO |
SCHWP2-O |
Sec CHW Pump2 |
Output |
Eff SCHWP2 Cmd |
SCHWP2-% |
SCHWP2 |
Effective Command |
|
SCHWP2 BO |
SCHWP2-C |
Sec CHW Pump2 |
Command |
Eff SCHWP2 Binary Cmd |
SCHWP2-EC |
SCHWP2 |
Effective Stg Command |
|
VSD Bypass Drive BV |
SCHWP2-BYPASS |
Sec CHW Pump2 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
SCHWP2-RESET |
Sec CHW Pump2 |
Reset Drive Fault |
N/A |
|||
|
SCHWP3 AO |
SCHWP3-O |
Sec CHW Pump3 |
Output |
Eff SCHWP3 Cmd |
SCHWP3-% |
SCHWP3 |
Effective Command |
|
SCHWP3 BO |
SCHWP3-C |
Sec CHW Pump3 |
Command |
Eff SCHWP3 Binary Cmd |
SCHWP3-EC |
SCHWP3 |
Effective Stg Command |
|
VSD Bypass Drive BV |
SCHWP3-BYPASS |
Sec CHW Pump3 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
SCHWP3-RESET |
Sec CHW Pump3 |
Reset Drive Fault |
N/A |
|||
|
SCHWP4 AO |
SCHWP4-O |
Sec CHW Pump4 |
Output |
Eff SCHWP4 Cmd |
SCHWP4-% |
SCHWP4 |
Effective Command |
|
SCHWP4 BO |
SCHWP4-C |
Sec CHW Pump4 |
Command |
Eff SCHWP4 Binary Cmd |
SCHWP4-EC |
SCHWP4 |
Effective Stg Command |
|
VSD Bypass Drive BV |
SCHWP4-BYPASS |
Sec CHW Pump4 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
SCHWP4-RESET |
Sec CHW Pump4 |
Reset Drive Fault |
N/A |
|||
|
SCHWP5 AO |
SCHWP5-O |
Sec CHW Pump5 |
Output |
Eff SCHWP5 Cmd |
SCHWP5-% |
SCHWP5 |
Effective Command |
|
SCHWP5 BO |
SCHWP5-C |
Sec CHW Pump5 |
Command |
Eff SCHWP5 Binary Cmd |
SCHWP5-EC |
SCHWP5 |
Effective Stg Command |
|
VSD Bypass Drive BV |
SCHWP5-BYPASS |
Sec CHW Pump5 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
SCHWP5-RESET |
Sec CHW Pump5 |
Reset Drive Fault |
N/A |
|||
|
SCHWP6 AO |
SCHWP6-O |
Sec CHW Pump6 |
Output |
Eff SCHWP6 Cmd |
SCHWP6-% |
SCHWP6 |
Effective Command |
|
SCHWP6 BO |
SCHWP6-C |
Sec CHW Pump6 |
Command |
Eff SCHWP6 Binary Cmd |
SCHWP6-EC |
SCHWP6 |
Effective Stg Command |
|
VSD Bypass Drive BV |
SCHWP6-BYPASS |
Sec CHW Pump6 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
SCHWP6-RESET |
Sec CHW Pump6 |
Reset Drive Fault |
N/A |
|||
|
SCHWP7 AO |
SCHWP7-O |
Sec CHW Pump7 |
Output |
Eff SCHWP7 Cmd |
SCHWP7-% |
SCHWP7 |
Effective Command |
|
SCHWP7 BO |
SCHWP7-C |
Sec CHW Pump7 |
Command |
Eff SCHWP7 Binary Cmd |
SCHWP7-EC |
SCHWP7 |
Effective Stg Command |
|
VSD Bypass Drive BV |
SCHWP7-BYPASS |
Sec CHW Pump7 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
SCHWP7-RESET |
Sec CHW Pump7 |
Reset Drive Fault |
N/A |
|||
|
SCHWP8 AO |
SCHWP8-O |
Sec CHW Pump8 |
Output |
Eff SCHWP8 Cmd |
SCHWP8-% |
SCHWP8 |
Effective Command |
|
SCHWP8 BO |
SCHWP8-C |
Sec CHW Pump8 |
Command |
Eff SCHWP8 Binary Cmd |
SCHWP8-EC |
SCHWP8 |
Effective Stg Command |
|
VSD Bypass Drive BV |
SCHWP8-BYPASS |
Sec CHW Pump8 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
SCHWP8-RESET |
Sec CHW Pump8 |
Reset Drive Fault |
N/A |
|||
|
SHWP1 AO |
SHWP1-O |
Sec HW Pump1 |
Output |
Eff SHWP1 Cmd |
SHWP1-% |
SHWP1 |
Effective Command |
|
SHWP1 BO |
SHWP1-C |
Sec HW Pump1 |
Command |
Eff SHWP1 Binary Cmd |
SHWP1-EC |
SHWP1 |
Effective Stg Command |
|
VSD Bypass Drive BV |
SHWP1-BYPASS |
Sec HW Pump1 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
SHWP1-RESET |
Sec HW Pump1 |
Reset Drive Fault |
N/A |
|||
|
SHWP2 AO |
SHWP2-O |
Sec HW Pump2 |
Output |
Eff SHWP2 Cmd |
SHWP2-% |
SHWP2 |
Effective Command |
|
SHWP2 BO |
SHWP2-C |
Sec HW Pump2 |
Command |
Eff SHWP2 Binary Cmd |
SHWP2-EC |
SHWP2 |
Effective Stg Command |
|
VSD Bypass Drive BV |
SHWP2-BYPASS |
Sec HW Pump2 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
SHWP2-RESET |
Sec HW Pump2 |
Reset Drive Fault |
N/A |
|||
|
SHWP3 AO |
SHWP3-O |
Sec HW Pump3 |
Output |
Eff SHWP3 Cmd |
SHWP3-% |
SHWP3 |
Effective Command |
|
SHWP3 BO |
SHWP3-C |
Sec HW Pump3 |
Command |
Eff SHWP3 Binary Cmd |
SHWP3-EC |
SHWP3 |
Effective Stg Command |
|
VSD Bypass Drive BV |
SHWP3-BYPASS |
Sec HW Pump3 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
SHWP3-RESET |
Sec HW Pump3 |
Reset Drive Fault |
N/A |
|||
|
SHWP4 AO |
SHWP4-O |
Sec HW Pump4 |
Output |
Eff SHWP4 Cmd |
SHWP4-% |
SHWP4 |
Effective Command |
|
SHWP4 BO |
SHWP4-C |
Sec HW Pump4 |
Command |
Eff SHWP4 Binary Cmd |
SHWP4-EC |
SHWP4 |
Effective Stg Command |
|
VSD Bypass Drive BV |
SHWP4-BYPASS |
Sec HW Pump4 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
SHWP4-RESET |
Sec HW Pump4 |
Reset Drive Fault |
N/A |
|||
|
SHWP5 AO |
SHWP5-O |
Sec HW Pump5 |
Output |
Eff SHWP5 Cmd |
SHWP5-% |
SHWP5 |
Effective Command |
|
SHWP5 BO |
SHWP5-C |
Sec HW Pump5 |
Command |
Eff SHWP5 Binary Cmd |
SHWP5-EC |
SHWP5 |
Effective Stg Command |
|
VSD Bypass Drive BV |
SHWP5-BYPASS |
Sec HW Pump5 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
SHWP5-RESET |
Sec HW Pump5 |
Reset Drive Fault |
N/A |
|||
|
SHWP6 AO |
SHWP6-O |
Sec HW Pump6 |
Output |
Eff SHWP6 Cmd |
SHWP6-% |
SHWP6 |
Effective Command |
|
SHWP6 BO |
SHWP6-C |
Sec HW Pump6 |
Command |
Eff SHWP6 Binary Cmd |
SHWP6-EC |
SHWP6 |
Effective Stg Command |
|
VSD Bypass Drive BV |
SHWP6-BYPASS |
Sec HW Pump6 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
SHWP6-RESET |
Sec HW Pump6 |
Reset Drive Fault |
N/A |
|||
|
SHWP7 AO |
SHWP7-O |
Sec HW Pump7 |
Output |
Eff SHWP7 Cmd |
SHWP7-% |
SHWP7 |
Effective Command |
|
SHWP7 BO |
SHWP7-C |
Sec HW Pump7 |
Command |
Eff SHWP7 Binary Cmd |
SHWP7-EC |
SHWP7 |
Effective Stg Command |
|
VSD Bypass Drive BV |
SHWP7-BYPASS |
Sec HW Pump7 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
SHWP7-RESET |
Sec HW Pump7 |
Reset Drive Fault |
N/A |
|||
|
SHWP8 AO |
SHWP8-O |
Sec HW Pump8 |
Output |
Eff SHWP8 Cmd |
SHWP8-% |
SHWP8 |
Effective Command |
|
SHWP8 BO |
SHWP8-C |
Sec HW Pump8 |
Command |
Eff SHWP8 Binary Cmd |
SHWP8-EC |
SHWP8 |
Effective Stg Command |
|
VSD Bypass Drive BV |
SHWP8-BYPASS |
Sec HW Pump8 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
SHWP8-RESET |
Sec HW Pump8 |
Reset Drive Fault |
N/A |
|||
|
Sequenced Valves AO |
HC-O |
Sequenced Valves - Heating Cooling |
Output |
N/A |
|||
|
Fan BO |
SF-C |
Series Supply Fan |
Command |
N/A |
|||
|
Fan Speed AO |
SF-O |
Series Supply Fan |
Output |
N/A |
|||
|
Sideloop AO |
SL-O |
Sideloop |
Output |
Eff Sideloop Cmd |
SL-% |
Sideloop |
Effective Command |
|
Sideloop BO |
SL-C |
Sideloop |
Command |
Eff Sideloop Binary Cmd |
SL-EC |
Sideloop |
Effective Vlv Command |
|
Sideloop PAO |
SL-O |
Sideloop |
Output_PAO |
Eff Sideloop Cmd |
SL-% |
Sideloop |
Effective Command |
|
Sideloop Stage 1 BO |
SL1-C |
Sideloop |
Stage 1 Command |
Eff Sideloop Stage 1 Binary Cmd |
SL1-EC |
Sideloop Stage 1 |
Effective Stg Command |
|
Sideloop Stage 2 BO |
SL2-C |
Sideloop |
Stage 2 Command |
Eff Sideloop Stage 2 Binary Cmd |
SL2-EC |
Sideloop Stage 2 |
Effective Stg Command |
|
Sideloop Stage 3 BO |
SL3-C |
Sideloop |
Stage 3 Command |
Eff Sideloop Stage 3 Binary Cmd |
SL3-EC |
Sideloop Stage 3 |
Effective Stg Command |
|
Sideloop Stage 4 BO |
SL4-C |
Sideloop |
Stage 4 Command |
Eff Sideloop Stage 4 Binary Cmd |
SL4-EC |
Sideloop Stage 4 |
Effective Stg Command |
|
Sideloop Stage 5 BO |
SL5-C |
Sideloop |
Stage 5 Command |
Eff Sideloop Stage 5 Binary Cmd |
SL5-EC |
Sideloop Stage 5 |
Effective Stg Command |
|
Sideloop Stage 6 BO |
SL6-C |
Sideloop |
Stage 6 Command |
Eff Sideloop Stage 6 Binary Cmd |
SL6-EC |
Sideloop Stage 6 |
Effective Stg Command |
|
Sideloop Stage 7 BO |
SL7-C |
Sideloop |
Stage 7 Command |
Eff Sideloop Stage 7 Binary Cmd |
SL7-EC |
Sideloop Stage 7 |
Effective Stg Command |
|
Sideloop Stage 8 BO |
SL8-C |
Sideloop |
Stage 8 Command |
Eff Sideloop Stage 8 Binary Cmd |
SL8-EC |
Sideloop Stage 8 |
Effective Stg Command |
|
Steam Isolation Valve BO |
STMISO-C |
Steam Isolation Valve |
Command |
N/A |
|||
|
Supp Heating Stage 1 BO |
SUPHTG1-C |
Supplemental Heating |
Stage 1 Command |
Eff Supp Heating Stage 1 Binary Cmd |
SUPHTG1-EC |
Supp Heating Stage 1 |
Effective Stg Command |
|
Supp Heating Valve AO |
SUPHTG-O |
Supplemental Heating |
Output |
Eff Supp Heating Valve Cmd |
SUPHTG-% |
Supplemental Heating |
Effective Command |
|
Supp Heating Valve BO |
SUPHTG-C |
Supplemental Heating |
Command |
Eff Supp Heating Valve Binary Cmd |
SUPHTG-EC |
Supp Heating Valve |
Effective Vlv Command |
|
Supp Heating Valve PAO |
SUPHTG-O |
Supplemental Heating |
Output_PAO |
Eff Supp Heating Valve Cmd |
SUPHTG-% |
Supplemental Heating |
Effective Command |
|
Supplemental Heating Enable BO |
SUPHTG-EN |
Supplemental Heating Enable |
Command |
N/A |
|||
|
Supplemental Heating Pump BO |
SUPHTGP-C |
Supplemental Heating Pump |
Command |
N/A |
|||
|
Supply Damper AO |
DPR-O |
Supply Air Damper |
Output |
Eff Damper Cmd |
DPR-% |
Damper |
Effective Command |
|
Supply Damper PAO |
DPR-O |
Supply Air Damper |
Output_PAO |
Eff Damper Cmd |
DPR-% |
Damper |
Effective Command |
|
Supply Damper PAO |
DPR-O |
Supply Air Damper |
Output_PAO _Integrated |
Eff Damper Cmd |
DPR-% |
Damper |
Effective Command |
|
Supply Damper PAO - Minimum Pulse Width |
PARAM-DPR-MINP |
Supply Air Damper |
MinPulse |
N/A |
|||
|
Supply Damper PAO Stroke Time |
PARAM-DPR-ST |
Supply Air Damper |
StrokeTime |
N/A |
|||
|
Supply Fan BO |
SF-C |
Supply Fan |
Command |
N/A |
|||
|
Supply Fan BO |
SF-C |
Supply Fan |
Run/Stop |
N/A |
|||
|
Supply Fan Speed AO |
SF-O |
Supply Fan |
Output |
Eff Supply Fan Speed Cmd |
SF-% |
Supply Fan Speed |
Effective Command |
|
VSD Bypass Drive BV |
SF-BYPASS |
Supply Fan |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
SF-RESET |
Supply Fan |
Reset Drive Fault |
N/A |
|||
|
Supply Fan2 BO |
SF2-C |
Supply Fan2 |
Command |
N/A |
|||
|
Supply Fan2 BO |
SF2-C |
Supply Fan2 |
Run/Stop |
N/A |
|||
|
Supply Fan2 Speed AO |
SF2-O |
Supply Fan2 |
Output |
Eff Supply Fan2 Speed Cmd |
SF2-% |
Supply Fan2 Speed |
Effective Command |
|
TEF BO |
TEF-C |
TEF |
Command |
N/A |
|||
|
Tower Basin Heater BO |
CTBH-EN |
Tower Basin Heater |
Command |
N/A |
|||
|
Tower Basin MUV BO |
CTMUV-C |
Tower Basin MU Valve |
Command |
N/A |
|||
|
Twr Bypass Valve AO |
CTV-O |
Tower Bypass Valve |
Output |
N/A |
|||
|
Twr1 Basin Heater BO |
CT1BH-EN |
Tower1 Basin Heater |
Command |
N/A |
|||
|
Twr1 Basin MU BO |
CT1MUV-C |
Tower1 Basin MU Valve |
Command |
N/A |
|||
|
Twr1 Iso Valve BO |
CT1ISOV-C |
Tower1 Iso Valve |
Command |
N/A |
|||
|
Twr2 Basin Heater BO |
CT2BH-EN |
Tower2 Basin Heater |
Command |
N/A |
|||
|
Twr2 Basin MU BO |
CT2MUV-C |
Tower2 Basin MU Valve |
Command |
N/A |
|||
|
Twr2 Iso Valve BO |
CT2ISOV-C |
Tower2 Iso Valve |
Command |
N/A |
|||
|
Twr3 Basin Heater BO |
CT3BH-EN |
Tower3 Basin Heater |
Command |
N/A |
|||
|
Twr3 Basin MU BO |
CT3MUV-C |
Tower3 Basin MU Valve |
Command |
N/A |
|||
|
Twr3 Iso Valve BO |
CT3ISOV-C |
Tower3 Iso Valve |
Command |
N/A |
|||
|
Twr4 Basin Heater BO |
CT4BH-EN |
Tower4 Basin Heater |
Command |
N/A |
|||
|
Twr4 Basin MU BO |
CT4MUV-C |
Tower4 Basin MU Valve |
Command |
N/A |
|||
|
Twr4 Iso Valve BO |
CT4ISOV-C |
Tower4 Iso Valve |
Command |
N/A |
|||
|
Twr5 Basin Heater BO |
CT5BH-EN |
Tower5 Basin Heater |
Command |
N/A |
|||
|
Twr5 Basin MU BO |
CT5MUV-C |
Tower5 Basin MU Valve |
Command |
N/A |
|||
|
Twr5 Iso Valve BO |
CT5ISOV-C |
Tower5 Iso Valve |
Command |
N/A |
|||
|
Twr6 Basin Heater BO |
CT6BH-EN |
Tower6 Basin Heater |
Command |
N/A |
|||
|
Twr6 Basin MU BO |
CT6MUV-C |
Tower6 Basin MU Valve |
Command |
N/A |
|||
|
Twr6 Iso Valve BO |
CT6ISOV-C |
Tower6 Iso Valve |
Command |
N/A |
|||
|
Twr7 Basin Heater BO |
CT7BH-EN |
Tower7 Basin Heater |
Command |
N/A |
|||
|
Twr7 Basin MU BO |
CT7MUV-C |
Tower7 Basin MU Valve |
Command |
N/A |
|||
|
Twr7 Iso Valve BO |
CT7ISOV-C |
Tower7 Iso Valve |
Command |
N/A |
|||
|
Twr8 Basin Heater BO |
CT8BH-EN |
Tower8 Basin Heater |
Command |
N/A |
|||
|
Twr8 Basin MU BO |
CT8MUV-C |
Tower8 Basin MU Valve |
Command |
N/A |
|||
|
Twr8 Iso Valve BO |
CT8ISOV-C |
Tower8 Iso Valve |
Command |
N/A |
|||
|
TwrFan1 AO |
CT1-O |
TowerFan1 |
Output |
Eff TwrFan1 Cmd |
CT1-% |
TwrFan1 |
Effective Command |
|
TwrFan1 BO |
CT1-C |
TowerFan1 |
Command |
Eff TwrFan1 Binary Cmd |
CT1-EC |
TwrFan1 |
Effective Stg Command |
|
TwrFan1 Speed 1 BO |
CT1L-C |
TowerFan1 |
Command LO |
Eff TwrFan1 Speed 1 Binary Cmd |
CT1L-EC |
TwrFan1 Speed 1 |
Effective Stg Command |
|
TwrFan1 Speed 2 BO |
CT1M-C |
TowerFan1 |
Command MED |
Eff TwrFan1 Speed 2 Binary Cmd |
CT1M-EC |
TwrFan1 Speed 2 |
Effective Stg Command |
|
TwrFan1 Speed 3 BO |
CT1H-C |
TowerFan1 |
Command HI |
Eff TwrFan1 Speed 3 Binary Cmd |
CT1H-EC |
TwrFan1 Speed 3 |
Effective Stg Command |
|
VSD Bypass Drive BV |
CT1-BYPASS |
TowerFan1 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
CT1-RESET |
TowerFan1 |
Reset Drive Fault |
N/A |
|||
|
TwrFan1 IsoVlv BO |
CT1ISOV-C |
TowerFan1 Iso Valve |
Command |
N/A |
|||
|
TwrFan2 AO |
CT2-O |
TowerFan2 |
Output |
Eff TwrFan2 Cmd |
CT2-% |
TwrFan2 |
Effective Command |
|
TwrFan2 BO |
CT2-C |
TowerFan2 |
Command |
Eff TwrFan2 Binary Cmd |
CT2-EC |
TwrFan2 |
Effective Stg Command |
|
TwrFan2 Speed 1 BO |
CT2L-C |
TowerFan2 |
Command LO |
Eff TwrFan2 Speed 2 Binary Cmd |
CT2L-EC |
TwrFan2 Speed 2 |
Effective Stg Command |
|
TwrFan2 Speed 2 BO |
CT2M-C |
TowerFan2 |
Command MED |
Eff TwrFan2 Speed 2 Binary Cmd |
CT2M-EC |
TwrFan2 Speed 2 |
Effective Stg Command |
|
TwrFan2 Speed 3 BO |
CT2H-C |
TowerFan2 |
Command HI |
Eff TwrFan2 Speed 3 Binary Cmd |
CT2H-EC |
TwrFan2 Speed 3 |
Effective Stg Command |
|
VSD Bypass Drive BV |
CT2-BYPASS |
TowerFan2 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
CT2-RESET |
TowerFan2 |
Reset Drive Fault |
N/A |
|||
|
TwrFan2 IsoVlv BO |
CT2ISOV-C |
TowerFan2 Iso Valve |
Command |
N/A |
|||
|
TwrFan3 AO |
CT3-O |
TowerFan3 |
Output |
Eff TwrFan3 Cmd |
CT3-% |
TwrFan3 |
Effective Command |
|
TwrFan3 BO |
CT3-C |
TowerFan3 |
Command |
Eff TwrFan3 Binary Cmd |
CT3-EC |
TwrFan3 |
Effective Stg Command |
|
TwrFan3 Speed 1 BO |
CT3L-C |
TowerFan3 |
Command LO |
Eff TwrFan3 Speed 3 Binary Cmd |
CT3M-EC |
TwrFan3 Speed 3 |
Effective Stg Command |
|
TwrFan3 Speed 2 BO |
CT3M-C |
TowerFan3 |
Command MED |
Eff TwrFan3 Speed 2 Binary Cmd |
CT3L-EC |
TwrFan3 Speed 2 |
Effective Stg Command |
|
TwrFan3 Speed 3 BO |
CT3H-C |
TowerFan3 |
Command HI |
Eff TwrFan3 Speed 3 Binary Cmd |
CT3H-EC |
TwrFan3 Speed 3 |
Effective Stg Command |
|
VSD Bypass Drive BV |
CT3-BYPASS |
TowerFan3 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
CT3-RESET |
TowerFan3 |
Reset Drive Fault |
N/A |
|||
|
TwrFan3 IsoVlv BO |
CT3ISOV-C |
TowerFan3 Iso Valve |
Command |
N/A |
|||
|
TwrFan4 AO |
CT4-O |
TowerFan4 |
Output |
Eff TwrFan4 Cmd |
CT4-% |
TwrFan4 |
Effective Command |
|
TwrFan4 BO |
CT4-C |
TowerFan4 |
Command |
Eff TwrFan4 Binary Cmd |
CT4-EC |
TwrFan4 |
Effective Stg Command |
|
TwrFan4 Speed 1 BO |
CT4L-C |
TowerFan4 |
Command LO |
Eff TwrFan4 Speed 4 Binary Cmd |
CT4H-EC |
TwrFan4 Speed 4 |
Effective Stg Command |
|
TwrFan4 Speed 2 BO |
CT4M-C |
TowerFan4 |
Command MED |
Eff TwrFan4 Speed 2 Binary Cmd |
CT4L-EC |
TwrFan4 Speed 2 |
Effective Stg Command |
|
TwrFan4 Speed 3 BO |
CT4H-C |
TowerFan4 |
Command HI |
Eff TwrFan4 Speed 3 Binary Cmd |
CT4M-EC |
TwrFan4 Speed 3 |
Effective Stg Command |
|
VSD Bypass Drive BV |
CT4-BYPASS |
TowerFan4 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
CT4-RESET |
TowerFan4 |
Reset Drive Fault |
N/A |
|||
|
TwrFan4 IsoVlv BO |
CT4ISOV-C |
TowerFan4 Iso Valve |
Command |
N/A |
|||
|
TwrFan5 AO |
CT5-O |
TowerFan5 |
Output |
Eff TwrFan5 Cmd |
CT5-% |
TwrFan5 |
Effective Command |
|
TwrFan5 BO |
CT5-C |
TowerFan5 |
Command |
Eff TwrFan5 Binary Cmd |
CT5-EC |
TwrFan5 |
Effective Stg Command |
|
TwrFan5 Speed 1 BO |
CT5L-C |
TowerFan5 |
Command LO |
Eff TwrFan5 Speed 5 Binary Cmd |
CT5H-EC |
TwrFan5 Speed 5 |
Effective Stg Command |
|
TwrFan5 Speed 2 BO |
CT5M-C |
TowerFan5 |
Command MED |
Eff TwrFan5 Speed 2 Binary Cmd |
CT5L-EC |
TwrFan5 Speed 2 |
Effective Stg Command |
|
TwrFan5 Speed 3 BO |
CT5H-C |
TowerFan5 |
Command HI |
Eff TwrFan5 Speed 3 Binary Cmd |
CT5M-EC |
TwrFan5 Speed 3 |
Effective Stg Command |
|
VSD Bypass Drive BV |
CT5-BYPASS |
TowerFan5 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
CT5-RESET |
TowerFan5 |
Reset Drive Fault |
N/A |
|||
|
TwrFan5 IsoVlv BO |
CT5ISOV-C |
TowerFan5 Iso Valve |
Command |
N/A |
|||
|
TwrFan6 AO |
CT6-O |
TowerFan6 |
Output |
Eff TwrFan6 Cmd |
CT6-% |
TwrFan6 |
Effective Command |
|
TwrFan6 BO |
CT6-C |
TowerFan6 |
Command |
Eff TwrFan6 Binary Cmd |
CT6-EC |
TwrFan6 |
Effective Stg Command |
|
TwrFan6 Speed 1 BO |
CT6L-C |
TowerFan6 |
Command LO |
Eff TwrFan6 Speed 6 Binary Cmd |
CT6H-EC |
TwrFan6 Speed 6 |
Effective Stg Command |
|
TwrFan6 Speed 2 BO |
CT6M-C |
TowerFan6 |
Command MED |
Eff TwrFan6 Speed 2 Binary Cmd |
CT6L-EC |
TwrFan6 Speed 2 |
Effective Stg Command |
|
TwrFan6 Speed 3 BO |
CT6H-C |
TowerFan6 |
Command HI |
Eff TwrFan6 Speed 3 Binary Cmd |
CT6M-EC |
TwrFan6 Speed 3 |
Effective Stg Command |
|
VSD Bypass Drive BV |
CT6-BYPASS |
TowerFan6 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
CT6-RESET |
TowerFan6 |
Reset Drive Fault |
N/A |
|||
|
TwrFan6 IsoVlv BO |
CT6ISOV-C |
TowerFan6 Iso Valve |
Command |
N/A |
|||
|
TwrFan7 AO |
CT7-O |
TowerFan7 |
Output |
Eff TwrFan7 Cmd |
CT7-% |
TwrFan7 |
Effective Command |
|
TwrFan7 BO |
CT7-C |
TowerFan7 |
Command |
Eff TwrFan7 Binary Cmd |
CT7-EC |
TwrFan7 |
Effective Stg Command |
|
TwrFan7 Speed 1 BO |
CT7L-C |
TowerFan7 |
Command LO |
Eff TwrFan7 Speed 7 Binary Cmd |
CT7H-EC |
TwrFan7 Speed 7 |
Effective Stg Command |
|
TwrFan7 Speed 2 BO |
CT7M-C |
TowerFan7 |
Command MED |
Eff TwrFan7 Speed 2 Binary Cmd |
CT7L-EC |
TwrFan7 Speed 2 |
Effective Stg Command |
|
TwrFan7 Speed 3 BO |
CT7H-C |
TowerFan7 |
Command HI |
Eff TwrFan7 Speed 3 Binary Cmd |
CT7M-EC |
TwrFan7 Speed 3 |
Effective Stg Command |
|
VSD Bypass Drive BV |
CT7-BYPASS |
TowerFan7 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
CT7-RESET |
TowerFan7 |
Reset Drive Fault |
N/A |
|||
|
TwrFan7 IsoVlv BO |
CT7ISOV-C |
TowerFan7 Iso Valve |
Command |
N/A |
|||
|
TwrFan8 AO |
CT8-O |
TowerFan8 |
Output |
Eff TwrFan8 Cmd |
CT8-% |
TwrFan8 |
Effective Command |
|
TwrFan8 BO |
CT8-C |
TowerFan8 |
Command |
Eff TwrFan8 Binary Cmd |
CT8-EC |
TwrFan8 |
Effective Stg Command |
|
TwrFan8 Speed 1 BO |
CT8L-C |
TowerFan8 |
Command LO |
Eff TwrFan8 Speed 8 Binary Cmd |
CT8H-EC |
TwrFan8 Speed 8 |
Effective Stg Command |
|
TwrFan8 Speed 2 BO |
CT8M-C |
TowerFan8 |
Command MED |
Eff TwrFan8 Speed 2 Binary Cmd |
CT8L-EC |
TwrFan8 Speed 2 |
Effective Stg Command |
|
TwrFan8 Speed 3 BO |
CT8H-C |
TowerFan8 |
Command HI |
Eff TwrFan8 Speed 3 Binary Cmd |
CT8M-EC |
TwrFan8 Speed 3 |
Effective Stg Command |
|
VSD Bypass Drive BV |
CT8-BYPASS |
TowerFan8 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
CT8-RESET |
TowerFan8 |
Reset Drive Fault |
N/A |
|||
|
TwrFan8 IsoVlv BO |
CT8ISOV-C |
TowerFan8 Iso Valve |
Command |
N/A |
|||
|
Voltage Out 1 AO |
VOLT1-O |
Voltage 1 |
Output |
N/A |
|||
|
Voltage Out 2 AO |
VOLT2-O |
Voltage 2 |
Output |
N/A |
|||
|
Voltage Out 3 AO |
VOLT3-O |
Voltage 3 |
Output |
N/A |
|||
|
Voltage Out 4 AO |
VOLT4-O |
Voltage 4 |
Output |
N/A |
|||
|
Voltage Out 5 AO |
VOLT5-O |
Voltage 5 |
Output |
N/A |
|||
|
Voltage Out 6 AO |
VOLT6-O |
Voltage 6 |
Output |
N/A |
|||
|
Supply Fan BO |
VSD1-C |
VSD1 |
Run/Stop |
N/A |
|||
|
Supply Fan Speed AO |
VSD1-O |
VSD1 |
Output |
Eff Supply Fan Speed Cmd |
SF-% |
Supply Fan Speed |
Effective Command |
|
VSD Bypass Drive BV |
VSD1-BYPASS |
VSD1 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
VSD1-RESET |
VSD1 |
Reset Drive Fault |
N/A |
|||
|
Supply Fan BO |
VSD2-C |
VSD2 |
Run/Stop |
N/A |
|||
|
Supply Fan Speed AO |
VSD2-O |
VSD2 |
Output |
Eff Supply Fan Speed Cmd |
SF-% |
Supply Fan Speed |
Effective Command |
|
VSD Bypass Drive BV |
VSD2-BYPASS |
VSD2 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
VSD2-RESET |
VSD2 |
Reset Drive Fault |
N/A |
|||
|
Supply Fan BO |
VSD3-C |
VSD3 |
Run/Stop |
N/A |
|||
|
Supply Fan Speed AO |
VSD3-O |
VSD3 |
Output |
Eff Supply Fan Speed Cmd |
SF-% |
Supply Fan Speed |
Effective Command |
|
VSD Bypass Drive BV |
VSD3-BYPASS |
VSD3 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
VSD3-RESET |
VSD3 |
Reset Drive Fault |
N/A |
|||
|
Supply Fan BO |
VSD4-C |
VSD4 |
Run/Stop |
N/A |
|||
|
Supply Fan Speed AO |
VSD4-O |
VSD4 |
Output |
Eff Supply Fan Speed Cmd |
SF-% |
Supply Fan Speed |
Effective Command |
|
VSD Bypass Drive BV |
VSD4-BYPASS |
VSD4 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
VSD4-RESET |
VSD4 |
Reset Drive Fault |
N/A |
|||
|
Supply Fan BO |
VSD5-C |
VSD5 |
Run/Stop |
N/A |
|||
|
Supply Fan Speed AO |
VSD5-O |
VSD5 |
Output |
Eff Supply Fan Speed Cmd |
SF-% |
Supply Fan Speed |
Effective Command |
|
VSD Bypass Drive BV |
VSD5-BYPASS |
VSD5 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
VSD5-RESET |
VSD5 |
Reset Drive Fault |
N/A |
|||
|
Supply Fan BO |
VSD6-C |
VSD6 |
Run/Stop |
N/A |
|||
|
Supply Fan Speed AO |
VSD6-O |
VSD6 |
Output |
Eff Supply Fan Speed Cmd |
SF-% |
Supply Fan Speed |
Effective Command |
|
VSD Bypass Drive BV |
VSD6-BYPASS |
VSD6 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
VSD6-RESET |
VSD6 |
Reset Drive Fault |
N/A |
|||
|
Supply Fan BO |
VSD7-C |
VSD7 |
Run/Stop |
N/A |
|||
|
Supply Fan Speed AO |
VSD7-O |
VSD7 |
Output |
Eff Supply Fan Speed Cmd |
SF-% |
Supply Fan Speed |
Effective Command |
|
VSD Bypass Drive BV |
VSD7-BYPASS |
VSD7 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
VSD7-RESET |
VSD7 |
Reset Drive Fault |
N/A |
|||
|
Supply Fan BO |
VSD8-C |
VSD8 |
Run/Stop |
N/A |
|||
|
Supply Fan Speed AO |
VSD8-O |
VSD8 |
Output |
Eff Supply Fan Speed Cmd |
SF-% |
Supply Fan Speed |
Effective Command |
|
VSD Bypass Drive BV |
VSD8-BYPASS |
VSD8 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
VSD8-RESET |
VSD8 |
Reset Drive Fault |
N/A |
|||
|
Supply Fan BO |
VSD9-C |
VSD9 |
Run/Stop |
N/A |
|||
|
Supply Fan Speed AO |
VSD9-O |
VSD9 |
Output |
Eff Supply Fan Speed Cmd |
SF-% |
Supply Fan Speed |
Effective Command |
|
VSD Bypass Drive BV |
VSD9-BYPASS |
VSD9 |
Bypass Drive |
N/A |
|||
|
VSD Reset Drive Fault BV |
VSD9-RESET |
VSD9 |
Reset Drive Fault |
N/A |
|||
|
Fan Speed Status Display MSV |
ZNF-% |
Zone |
Fan Speed Status |
N/A |
|||
|
Occupancy Status Display MSV |
OCC-MODE |
Zone |
Occ Status |
N/A |
|||
|
Zone 1 Heating Pump BO |
ZHLP1-C |
Zone Loop Heating Pump 1 |
Command |
N/A |
|||
|
Zone 2 Heating Pump BO |
ZHLP2-C |
Zone Loop Heating Pump 2 |
Command |
N/A |
|||
|
Zone 3 Heating Pump BO |
ZHLP3-C |
Zone Loop Heating Pump 3 |
Command |
N/A |
|||
|
Zone 4 Heating Pump BO |
ZHLP4-C |
Zone Loop Heating Pump 4 |
Command |
N/A |
|||
|
Zone 5 Heating Pump BO |
ZHLP5-C |
Zone Loop Heating Pump 5 |
Command |
N/A |
|||
|
Zone 6 Heating Pump BO |
ZHLP6-C |
Zone Loop Heating Pump 6 |
Command |
N/A |
|||
|
Zone 7 Heating Pump BO |
ZHLP7-C |
Zone Loop Heating Pump 7 |
Command |
N/A |
|||
|
Zone 8 Heating Pump BO |
ZHLP8-C |
Zone Loop Heating Pump 8 |
Command |
N/A |
|||
|
Occupancy Status Display MSV |
OCC-MODE1 |
Zone1 |
Occ Status |
N/A |
|||
|
Zone 1 Damper AO |
ZN1D-O |
Zone1 Damper |
Output |
Eff Zone 1 Damper Cmd |
ZN1D-% |
Zone 1 Damper |
Effective Command |
|
Zone 1 Damper PAO |
ZN1D-O |
Zone1 Damper |
Output_PAO |
Eff Zone 1 Damper Cmd |
ZN1D-% |
Zone 1 Damper |
Effective Command |
|
Zone 1 Heating Stage 1 BO |
ZN1HTG1-C |
Zone1 Heating |
Stage 1 Command |
Eff Zone 1 Heating Stage 1 Binary Cmd |
ZN1HTG1-EC |
Zone 1 Heating Stage 1 |
Effective Stg Command |
|
Zone 1 Heating Stage 2 BO |
ZN1HTG2-C |
Zone1 Heating |
Stage 2 Command |
Eff Zone 1 Heating Stage 2 Binary Cmd |
ZN1HTG2-EC |
Zone 1 Heating Stage 2 |
Effective Stg Command |
|
Zone 1 Heating Stage 3 BO |
ZN1HTG3-C |
Zone1 Heating |
Stage 3 Command |
Eff Zone 1 Heating Stage 3 Binary Cmd |
ZN1HTG3-EC |
Zone 1 Heating Stage 3 |
Effective Stg Command |
|
Zone 1 Heating Valve AO |
ZN1HTG-O |
Zone1 Heating |
Output |
Eff Zone 1 Heating Valve Cmd |
ZN1HTG-% |
Zone 1 Heating Valve |
Effective Command |
|
Zone 1 Heating Valve BO |
ZN1HTG-C |
Zone1 Heating |
Command |
Eff Zone 1 Heating Valve Binary Cmd |
ZN1HTG-EC |
Zone 1 Heating Valve |
Effective Vlv Command |
|
Zone 1 Heating Valve PAO |
ZN1HTG-O |
Zone1 Heating |
Output_PAO |
Eff Zone 1 Heating Valve Cmd |
ZN1HTG-% |
Zone 1 Heating Valve |
Effective Command |
|
Occupancy Status Display MSV |
OCC-MODE2 |
Zone2 |
Occ Status |
N/A |
|||
|
Zone 2 Damper AO |
ZN2D-O |
Zone2 Damper |
Output |
Eff Zone 2 Damper Cmd |
ZN2D-% |
Zone 2 Damper |
Effective Command |
|
Zone 2 Damper PAO |
ZN2D-O |
Zone2 Damper |
Output_PAO |
Eff Zone 2 Damper Cmd |
ZN2D-% |
Zone 2 Damper |
Effective Command |
|
Zone 2 Heating Stage 1 BO |
ZN2HTG1-C |
Zone2 Heating |
Stage 1 Command |
Eff Zone 2 Heating Stage 2 Binary Cmd |
ZN2HTG1-EC |
Zone 2 Heating Stage 2 |
Effective Stg Command |
|
Zone 2 Heating Stage 2 BO |
ZN2HTG2-C |
Zone2 Heating |
Stage 2 Command |
Eff Zone 2 Heating Stage 2 Binary Cmd |
ZN2HTG2-EC |
Zone 2 Heating Stage 2 |
Effective Stg Command |
|
Zone 2 Heating Stage 3 BO |
ZN2HTG3-C |
Zone2 Heating |
Stage 3 Command |
Eff Zone 2 Heating Stage 3 Binary Cmd |
ZN2HTG3-EC |
Zone 2 Heating Stage 3 |
Effective Stg Command |
|
Zone 2 Heating Valve AO |
ZN2HTG-O |
Zone2 Heating |
Output |
Eff Zone 2 Heating Valve Cmd |
ZN2HTG-% |
Zone 2 Heating Valve |
Effective Command |
|
Zone 2 Heating Valve BO |
ZN2HTG-C |
Zone2 Heating |
Command |
Eff Zone 2 Heating Valve Binary Cmd |
ZN2HTG-EC |
Zone 2 Heating Valve |
Effective Vlv Command |
|
Zone 2 Heating Valve PAO |
ZN2HTG-O |
Zone2 Heating |
Output_PAO |
Eff Zone 2 Heating Valve Cmd |
ZN2HTG-% |
Zone 2 Heating Valve |
Effective Command |
|
Occupancy Status Display MSV |
OCC-MODE3 |
Zone3 |
Occ Status |
N/A |
|||
|
Zone 3 Damper AO |
ZN3D-O |
Zone3 Damper |
Output |
Eff Zone 3 Damper Cmd |
ZN3D-% |
Zone 3 Damper |
Effective Command |
|
Zone 3 Damper PAO |
ZN3D-O |
Zone3 Damper |
Output_PAO |
Eff Zone 3 Damper Cmd |
ZN3D-% |
Zone 3 Damper |
Effective Command |
|
Zone 3 Heating Stage 1 BO |
ZN3HTG1-C |
Zone3 Heating |
Stage 1 Command |
Eff Zone 3 Heating Stage 3 Binary Cmd |
ZN3HTG2-EC |
Zone 3 Heating Stage 3 |
Effective Stg Command |
|
Zone 3 Heating Stage 2 BO |
ZN3HTG2-C |
Zone3 Heating |
Stage 2 Command |
Eff Zone 3 Heating Stage 2 Binary Cmd |
ZN3HTG3-EC |
Zone 3 Heating Stage 2 |
Effective Stg Command |
|
Zone 3 Heating Stage 3 BO |
ZN3HTG3-C |
Zone3 Heating |
Stage 3 Command |
Eff Zone 3 Heating Stage 3 Binary Cmd |
ZN3HTG3-EC |
Zone 3 Heating Stage 3 |
Effective Stg Command |
|
Zone 3 Heating Valve AO |
ZN3HTG-O |
Zone3 Heating |
Output |
Eff Zone 3 Heating Valve Cmd |
ZN3HTG-% |
Zone 3 Heating Valve |
Effective Command |
|
Zone 3 Heating Valve BO |
ZN3HTG-C |
Zone3 Heating |
Command |
Eff Zone 3 Heating Valve Binary Cmd |
ZN3HTG-EC |
Zone 3 Heating Valve |
Effective Vlv Command |
|
Zone 3 Heating Valve PAO |
ZN3HTG-O |
Zone3 Heating |
Output_PAO |
Eff Zone 3 Heating Valve Cmd |
ZN3HTG-% |
Zone 3 Heating Valve |
Effective Command |
|
Occupancy Status Display MSV |
OCC-MODE4 |
Zone4 |
Occ Status |
N/A |
|||
|
Zone 4 Damper AO |
ZN4D-O |
Zone4 Damper |
Output |
Eff Zone 4 Damper Cmd |
ZN4D-% |
Zone 4 Damper |
Effective Command |
|
Zone 4 Damper PAO |
ZN4D-O |
Zone4 Damper |
Output_PAO |
Eff Zone 4 Damper Cmd |
ZN4D-% |
Zone 4 Damper |
Effective Command |
|
Zone 4 Heating Stage 1 BO |
ZN4HTG1-C |
Zone4 Heating |
Stage 1 Command |
Eff Zone 4 Heating Stage 4 Binary Cmd |
ZN4HTG3-EC |
Zone 4 Heating Stage 4 |
Effective Stg Command |
|
Zone 4 Heating Stage 2 BO |
ZN4HTG2-C |
Zone4 Heating |
Stage 2 Command |
Eff Zone 4 Heating Stage 2 Binary Cmd |
ZN4HTG4-EC |
Zone 4 Heating Stage 2 |
Effective Stg Command |
|
Zone 4 Heating Stage 3 BO |
ZN4HTG3-C |
Zone4 Heating |
Stage 3 Command |
Eff Zone 4 Heating Stage 3 Binary Cmd |
ZN4HTG2-EC |
Zone 4 Heating Stage 3 |
Effective Stg Command |
|
Zone 4 Heating Valve AO |
ZN4HTG-O |
Zone4 Heating |
Output |
Eff Zone 4 Heating Valve Cmd |
ZN4HTG-% |
Zone 4 Heating Valve |
Effective Command |
|
Zone 4 Heating Valve BO |
ZN4HTG-C |
Zone4 Heating |
Command |
Eff Zone 4 Heating Valve Binary Cmd |
ZN4HTG-EC |
Zone 4 Heating Valve |
Effective Vlv Command |
|
Zone 4 Heating Valve PAO |
ZN4HTG-O |
Zone4 Heating |
Output_PAO |
Eff Zone 4 Heating Valve Cmd |
ZN4HTG-% |
Zone 4 Heating Valve |
Effective Command |
|
Zone 5 Damper AO |
ZN5D-O |
Zone5 Damper |
Output |
Eff Zone 5 Damper Cmd |
ZN5D-% |
Zone 5 Damper |
Effective Command |
|
Zone 5 Damper PAO |
ZN5D-O |
Zone5 Damper |
Output_PAO |
Eff Zone 5 Damper Cmd |
ZN5D-% |
Zone 5 Damper |
Effective Command |
|
Zone 5 Heating Stage 1 BO |
ZN5HTG1-C |
Zone5 Heating |
Stage 1 Command |
Eff Zone 5 Heating Stage 5 Binary Cmd |
ZN5HTG3-EC |
Zone 5 Heating Stage 5 |
Effective Stg Command |
|
Zone 5 Heating Stage 2 BO |
ZN5HTG2-C |
Zone5 Heating |
Stage 2 Command |
Eff Zone 5 Heating Stage 2 Binary Cmd |
ZN5HTG5-EC |
Zone 5 Heating Stage 2 |
Effective Stg Command |
|
Zone 5 Heating Stage 3 BO |
ZN5HTG3-C |
Zone5 Heating |
Stage 3 Command |
Eff Zone 5 Heating Stage 3 Binary Cmd |
ZN5HTG2-EC |
Zone 5 Heating Stage 3 |
Effective Stg Command |
|
Zone 5 Heating Valve AO |
ZN5HTG-O |
Zone5 Heating |
Output |
Eff Zone 5 Heating Valve Cmd |
ZN5HTG-% |
Zone 5 Heating Valve |
Effective Command |
|
Zone 5 Heating Valve BO |
ZN5HTG-C |
Zone5 Heating |
Command |
Eff Zone 5 Heating Valve Binary Cmd |
ZN5HTG-EC |
Zone 5 Heating Valve |
Effective Vlv Command |
|
Zone 5 Heating Valve PAO |
ZN5HTG-O |
Zone5 Heating |
Output_PAO |
Eff Zone 5 Heating Valve Cmd |
ZN5HTG-% |
Zone 5 Heating Valve |
Effective Command |
|
Zone 6 Damper AO |
ZN6D-O |
Zone6 Damper |
Output |
Eff Zone 6 Damper Cmd |
ZN6D-% |
Zone 6 Damper |
Effective Command |
|
Zone 6 Damper PAO |
ZN6D-O |
Zone6 Damper |
Output_PAO |
Eff Zone 6 Damper Cmd |
ZN6D-% |
Zone 6 Damper |
Effective Command |
|
Zone 6 Heating Stage 1 BO |
ZN6HTG1-C |
Zone6 Heating |
Stage 1 Command |
Eff Zone 6 Heating Stage 6 Binary Cmd |
ZN6HTG3-EC |
Zone 6 Heating Stage 6 |
Effective Stg Command |
|
Zone 6 Heating Stage 2 BO |
ZN6HTG2-C |
Zone6 Heating |
Stage 2 Command |
Eff Zone 6 Heating Stage 2 Binary Cmd |
ZN6HTG6-EC |
Zone 6 Heating Stage 2 |
Effective Stg Command |
|
Zone 6 Heating Stage 3 BO |
ZN6HTG3-C |
Zone6 Heating |
Stage 3 Command |
Eff Zone 6 Heating Stage 3 Binary Cmd |
ZN6HTG2-EC |
Zone 6 Heating Stage 3 |
Effective Stg Command |
|
Zone 6 Heating Valve AO |
ZN6HTG-O |
Zone6 Heating |
Output |
Eff Zone 6 Heating Valve Cmd |
ZN6HTG-% |
Zone 6 Heating Valve |
Effective Command |
|
Zone 6 Heating Valve BO |
ZN6HTG-C |
Zone6 Heating |
Command |
Eff Zone 6 Heating Valve Binary Cmd |
ZN6HTG-EC |
Zone 6 Heating Valve |
Effective Vlv Command |
|
Zone 6 Heating Valve PAO |
ZN6HTG-O |
Zone6 Heating |
Output_PAO |
Eff Zone 6 Heating Valve Cmd |
ZN6HTG-% |
Zone 6 Heating Valve |
Effective Command |
|
Zone 7 Damper AO |
ZN7D-O |
Zone7 Damper |
Output |
Eff Zone 7 Damper Cmd |
ZN7D-% |
Zone 7 Damper |
Effective Command |
|
Zone 7 Damper PAO |
ZN7D-O |
Zone7 Damper |
Output_PAO |
Eff Zone 7 Damper Cmd |
ZN7D-% |
Zone 7 Damper |
Effective Command |
|
Zone 7 Heating Stage 1 BO |
ZN7HTG1-C |
Zone7 Heating |
Stage 1 Command |
Eff Zone 7 Heating Stage 7 Binary Cmd |
ZN7HTG3-EC |
Zone 7 Heating Stage 7 |
Effective Stg Command |
|
Zone 7 Heating Stage 2 BO |
ZN7HTG2-C |
Zone7 Heating |
Stage 2 Command |
Eff Zone 7 Heating Stage 2 Binary Cmd |
ZN7HTG7-EC |
Zone 7 Heating Stage 2 |
Effective Stg Command |
|
Zone 7 Heating Stage 3 BO |
ZN7HTG3-C |
Zone7 Heating |
Stage 3 Command |
Eff Zone 7 Heating Stage 3 Binary Cmd |
ZN7HTG2-EC |
Zone 7 Heating Stage 3 |
Effective Stg Command |
|
Zone 7 Heating Valve AO |
ZN7HTG-O |
Zone7 Heating |
Output |
Eff Zone 7 Heating Valve Cmd |
ZN7HTG-% |
Zone 7 Heating Valve |
Effective Command |
|
Zone 7 Heating Valve BO |
ZN7HTG-C |
Zone7 Heating |
Command |
Eff Zone 7 Heating Valve Binary Cmd |
ZN7HTG-EC |
Zone 7 Heating Valve |
Effective Vlv Command |
|
Zone 7 Heating Valve PAO |
ZN7HTG-O |
Zone7 Heating |
Output_PAO |
Eff Zone 7 Heating Valve Cmd |
ZN7HTG-% |
Zone 7 Heating Valve |
Effective Command |
|
Zone 8 Damper AO |
ZN8D-O |
Zone8 Damper |
Output |
Eff Zone 8 Damper Cmd |
ZN8D-% |
Zone 8 Damper |
Effective Command |
|
Zone 8 Damper PAO |
ZN8D-O |
Zone8 Damper |
Output_PAO |
Eff Zone 8 Damper Cmd |
ZN8D-% |
Zone 8 Damper |
Effective Command |
|
Zone 8 Heating Stage 1 BO |
ZN8HTG1-C |
Zone8 Heating |
Stage 1 Command |
Eff Zone 8 Heating Stage 8 Binary Cmd |
ZN8HTG3-EC |
Zone 8 Heating Stage 8 |
Effective Stg Command |
|
Zone 8 Heating Stage 2 BO |
ZN8HTG2-C |
Zone8 Heating |
Stage 2 Command |
Eff Zone 8 Heating Stage 2 Binary Cmd |
ZN8HTG8-EC |
Zone 8 Heating Stage 2 |
Effective Stg Command |
|
Zone 8 Heating Stage 3 BO |
ZN8HTG3-C |
Zone8 Heating |
Stage 3 Command |
Eff Zone 8 Heating Stage 3 Binary Cmd |
ZN8HTG2-EC |
Zone 8 Heating Stage 3 |
Effective Stg Command |
|
Zone 8 Heating Valve AO |
ZN8HTG-O |
Zone8 Heating |
Output |
Eff Zone 8 Heating Valve Cmd |
ZN8HTG-% |
Zone 8 Heating Valve |
Effective Command |
|
Zone 8 Heating Valve BO |
ZN8HTG-C |
Zone8 Heating |
Command |
Eff Zone 8 Heating Valve Binary Cmd |
ZN8HTG-EC |
Zone 8 Heating Valve |
Effective Vlv Command |
|
Zone 8 Heating Valve PAO |
ZN8HTG-O |
Zone8 Heating |
Output_PAO |
Eff Zone 8 Heating Valve Cmd |
ZN8HTG-% |
Zone 8 Heating Valve |
Effective Command |