Adding an Effective Command Miscellaneous Input for an Output (Override Monitoring Feature) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This topic explains how to implement the Output Override Monitoring feature.

Effective Command inputs monitor the current command and the priority of the current command to an output object and make these values available for use within the application. These values are currently used by the Override Monitoring feature that prevents PID logic blocks from winding up and tuning incorrectly when the actual control outputs are overridden.

Scenarios where you might want to add an Effective Command input for an output include:

  • when a system has more stages than are currently supported by the application. An example of this scenario is a unit with more than eight stages of cooling. This configuration requires that you manually add extra binary outputs for the additional stages. Then, you must replace the MSC 08 module with the appropriate MSC for the actual number of stages present in your application (up to 12 stages). To add override monitoring for the additional stages, you must add Effective Command inputs to match the new binary outputs you just added.

  • when you need to add a custom control loop. We recommended you select a Sideloop for a custom control loop. Even if the logic within the sideloop is not complete enough to meet the specification for your application, the override monitoring feature for the outputs is automatically added. Then, you can modify the logic that enables the control loop to meet the specification.

If a loop requires that you manually add an analog output, and you want to use the override monitoring feature, you must add an associated Effective Command input to the Miscellaneous Inputs column of the Control View to provide this feature.

To add an effective command input for an output:

  1. Add the output module. For detailed instructions on how to add an output to your application, see Adding an Output or Miscellaneous Output.
  2. Select and add the appropriate effective command miscellaneous input module using Table 1. For detailed instructions on how to add an input to your application, see Adding an Input or Miscellaneous Input.

    On the left side of the table, identify the output you added in Step 1. The right side of the table indicates the criteria to use when adding the associated effective command miscellaneous input module. The table includes the following columns to help configure the input/output pair:

    • Standard Name - Indicates the standard name of the module visible via the Rename dialog box.
    • Name - Indicates the name of the module visible in the Output and Miscellaneous Input columns of the Control View after the module is added to the application. A value of N/A in this column indicates that there is no available input/output pair.
    • Application - Indicates the Application filter to select in the Input Selection and Output Selection dialog boxes.
    • Function - Indicates the Function filter to select in the Input Selection and Output Selection dialog boxes.

      To add more than one input/output pair, the output must have a unique standard name within the application (visible via the Rename dialog box).

  3. Verify that the Object Identifier of the miscellaneous input module matches that of the associated output module by viewing the Object Identifier attribute in the Details dialog box for both modules.
Table 1. Effective Command Configuration Information

Output Configuration

Miscellaneous Input Configuration

Standard Name Name Application Function Standard Name Name Application Function
2 Pipe Circulation Pump 1 BO HCP1-C 2 Pipe Circulation Pump 1 Command        
2 Pipe Circulation Pump 2 BO HCP2-C 3 Pipe Circulation Pump 2 Command        

Blr1 AO

BLR1-O

Boiler1

Output

Eff Blr1 Cmd

BLR1-%

Blr1

Effective Command

Blr1 BO

BLR1-C

Boiler1

Command

 

N/A

   

Blr1 Pump AO

BP1-O

Boiler1 Circ Pmp

Output

Eff Blr1 Pump Cmd

BP1-%

Boiler1 Circ Pmp

Effective Command

Blr1 Pump BO

BP1-C

Boiler1 Circ Pmp

Command

 

N/A

   

Blr1 BO

BLR1-EN

Boiler1 Ena

Command

 

N/A

   

Blr1 Iso Valve BO

BLR1ISOV-C

Boiler1 Iso Valve

Command

 

N/A

   

Boiler 1 SP AO

BLR1SP-O

Boiler1 SP

Output

 

N/A

   

Blr2 AO

BLR2-O

Boiler2

Output

Eff Blr2 Cmd

BLR2-%

Blr2

Effective Command

Blr2 BO

BLR2-C

Boiler2

Command

 

N/A

   

Blr2 Pump AO

BP2-O

Boiler2 Circ Pmp

Output

Eff Blr2 Pump Cmd

BP2-%

Boiler2 Circ Pmp

Effective Command

Blr2 Pump BO

BP2-C

Boiler2 Circ Pmp

Command

 

N/A

   

Blr2 BO

BLR2-EN

Boiler2 Ena

Command

 

N/A

   

Blr2 Iso Valve BO

BLR2ISOV-C

Boiler2 Iso Valve

Command

 

N/A

   

Boiler 2 SP AO

BLR2SP-O

Boiler2 SP

Output

 

N/A

   

Blr3 AO

BLR3-O

Boiler3

Output

Eff Blr3 Cmd

BLR3-%

Blr3

Effective Command

Blr3 BO

BLR3-C

Boiler3

Command

 

N/A

   

Blr3 Pump AO

BP3-O

Boiler3 Circ Pmp

Output

Eff Blr3 Pump Cmd

BP3-%

Boiler3 Circ Pmp

Effective Command

Blr3 Pump BO

BP3-C

Boiler3 Circ Pmp

Command

 

N/A

   

Blr3 BO

BLR3-EN

Boiler3 Ena

Command

 

N/A

   

Blr3 Iso Valve BO

BLR3ISOV-C

Boiler3 Iso Valve

Command

 

N/A

   

Boiler 3 SP AO

BLR3SP-O

Boiler3 SP

Output

 

N/A

   

Blr4 AO

BLR4-O

Boiler4

Output

Eff Blr4 Cmd

BLR4-%

Blr4

Effective Command

Blr4 BO

BLR4-C

Boiler4

Command

 

N/A

   

Blr4 Pump AO

BP4-O

Boiler4 Circ Pmp

Output

Eff Blr4 Pump Cmd

BP4-%

Boiler4 Circ Pmp

Effective Command

Blr4 Pump BO

BP4-C

Boiler4 Circ Pmp

Command

 

N/A

   

Blr4 BO

BLR4-EN

Boiler4 Ena

Command

 

N/A

   

Blr4 Iso Valve BO

BLR4ISOV-C

Boiler4 Iso Valve

Command

 

N/A

   

Boiler 4 SP AO

BLR4SP-O

Boiler4 SP

Output

 

N/A

   

Blr5 AO

BLR5-O

Boiler5

Output

Eff Blr5 Cmd

BLR5-%

Blr5

Effective Command

Blr5 BO

BLR5-C

Boiler5

Command

 

N/A

   

Blr5 Pump AO

BP5-O

Boiler5 Circ Pmp

Output

Eff Blr5 Pump Cmd

BP5-%

Boiler5 Circ Pmp

Effective Command

Blr5 Pump BO

BP5-C

Boiler5 Circ Pmp

Command

 

N/A

   

Blr5 BO

BLR5-EN

Boiler5 Ena

Command

 

N/A

   

Blr5 Iso Valve BO

BLR5ISOV-C

Boiler5 Iso Valve

Command

 

N/A

   

Boiler 5 SP AO

BLR5SP-O

Boiler5 SP

Output

 

N/A

   

Blr6 AO

BLR6-O

Boiler6

Output

Eff Blr6 Cmd

BLR6-%

Blr6

Effective Command

Blr6 BO

BLR6-C

Boiler6

Command

 

N/A

   

Blr6 Pump AO

BP6-O

Boiler6 Circ Pmp

Output

Eff Blr6 Pump Cmd

BP6-%

Boiler6 Circ Pmp

Effective Command

Blr6 Pump BO

BP6-C

Boiler6 Circ Pmp

Command

 

N/A

   

Blr6 BO

BLR6-EN

Boiler6 Ena

Command

 

N/A

   

Blr6 Iso Valve BO

BLR6ISOV-C

Boiler6 Iso Valve

Command

 

N/A

   

Boiler 6 SP AO

BLR6SP-O

Boiler6 SP

Output

 

N/A

   

Blr7 AO

BLR7-O

Boiler7

Output

Eff Blr7 Cmd

BLR7-%

Blr7

Effective Command

Blr7 BO

BLR7-C

Boiler7

Command

 

N/A

   

Blr7 Pump AO

BP7-O

Boiler7 Circ Pmp

Output

Eff Blr7 Pump Cmd

BP7-%

Boiler7 Circ Pmp

Effective Command

Blr7 Pump BO

BP7-C

Boiler7 Circ Pmp

Command

 

N/A

   

Blr7 BO

BLR7-EN

Boiler7 Ena

Command

 

N/A

   

Blr7 Iso Valve BO

BLR7ISOV-C

Boiler7 Iso Valve

Command

 

N/A

   

Boiler 7 SP AO

BLR7SP-O

Boiler7 SP

Output

 

N/A

   

Blr8 AO

BLR8-O

Boiler8

Output

Eff Blr8 Cmd

BLR8-%

Blr8

Effective Command

Blr8 BO

BLR8-C

Boiler8

Command

 

N/A

   

Blr8 Pump AO

BP8-O

Boiler8 Circ Pmp

Output

Eff Blr8 Pump Cmd

BP8-%

Boiler8 Circ Pmp

Effective Command

Blr8 Pump BO

BP8-C

Boiler8 Circ Pmp

Command

 

N/A

   

Blr8 BO

BLR8-EN

Boiler8 Ena

Command

 

N/A

   

Blr8 Iso Valve BO

BLR8ISOV-C

Boiler8 Iso Valve

Command

 

N/A

   

Boiler 8 SP AO

BLR8SP-O

Boiler8 SP

Output

 

N/A

   

Box Heating 2 Position BO

HTG-C

Box Heating

Command

Eff Box Heating 2 Position Binary Cmd

HTG-EC

Box Heating 2 Position

Effective Vlv Command

Box Heating Stage 1 BO

HTG1-C

Box Heating

Stage 1 Command

Eff Box Heating Stage 1 Binary Cmd

HTG1-EC

Box Heating Stage 1

Effective Stg Command

Box Heating Stage 2 BO

HTG2-C

Box Heating

Stage 2 Command

Eff Box Heating Stage 2 Binary Cmd

HTG2-EC

Box Heating Stage 2

Effective Stg Command

Box Heating Stage 3 BO

HTG3-C

Box Heating

Stage 3 Command

Eff Box Heating Stage 3 Binary Cmd

HTG3-EC

Box Heating Stage 3

Effective Stg Command

Box Heating Valve AO

HTG-O

Box Heating

Output

Eff Box Heating Valve Cmd

HTG-%

Box Heating

Effective Command

Box Heating Valve PAO

HTG-O

Box Heating

Output_PAO

Eff Box Heating Valve Cmd

HTG-%

Box Heating

Effective Command

Box Heating Enable BO

HTG-EN

Box Heating Enable

Command

 

N/A

   

HW Bypass Valve AO

BYPV-O

Bypass Loop

Output

Eff HW Bypass Valve Cmd

BYPV-%

HW Bypass Valve

Effective Command

Calibration Solenoid BO

ACSOL-C

Calibration

Command

 

N/A

   

Chiller 1 CHW Iso Valve BO

CH1CHWISOV

-C

Chiller 1 CHW Iso Valve

Command

 

N/A

   

Chiller 1 CW Iso Valve BO

CH1CWISOV-C

Chiller 1 CW Iso Valve

Command

 

N/A

   

Chiller 2 CHW Iso Valve BO

CH2CHWISOV-C

Chiller 2 CHW Iso Valve

Command

 

N/A

   

Chiller 2 CW Iso Valve BO

CH2CWISOV-C

Chiller 2 CW Iso Valve

Command

 

N/A

   

Chiller 3 CHW Iso Valve BO

CH3CHWISOV-C

Chiller 3 CHW Iso Valve

Command

 

N/A

   

Chiller 3 CW Iso Valve BO

CH3CWISOV-C

Chiller 3 CW Iso Valve

Command

 

N/A

   

Chiller 4 CHW Iso Valve BO

CH4CHWISOV-C

Chiller 4 CHW Iso Valve

Command

 

N/A

   

Chiller 4 CW Iso Valve BO

CH4CWISOV-C

Chiller 4 CW Iso Valve

Command

 

N/A

   

Chiller 5 CHW Iso Valve BO

CH5CHWISOV-C

Chiller 5 CHW Iso Valve

Command

 

N/A

   

Chiller 5 CW Iso Valve BO

CH5CWISOV-C

Chiller 5 CW Iso Valve

Command

 

N/A

   

Chiller 6 CHW Iso Valve BO

CH6CHWISOV-C

Chiller 6 CHW Iso Valve

Command

 

N/A

   

Chiller 6 CW Iso Valve BO

CH6CWISOV-C

Chiller 6 CW Iso Valve

Command

 

N/A

   

Chiller 7 CHW Iso Valve BO

CH7CHWISOV-C

Chiller 7 CHW Iso Valve

Command

 

N/A

   

Chiller 7 CW Iso Valve BO

CH7CWISOV-C

Chiller 7 CW Iso Valve

Command

 

N/A

   

Chiller 8 CHW Iso Valve BO

CH8CHWISOV-C

Chiller 8 CHW Iso Valve

Command

 

N/A

   

Chiller 8 CW Iso Valve BO

CH8CWISOV-C

Chiller 8 CW Iso Valve

Command

 

N/A

   

Chlr1 BO

CH1-EN

Chiller1

Command

 

N/A

   

Chlr1 CHW ISO Valve AO

CH1CHWISOV-O

Chiller1 CHW Iso Valve

Output

 

N/A

   

Chlr1 CHW Iso Valve BO

CH1CHWISOV-C

Chiller1 CHW Iso Valve

Command

 

N/A

   

Chlr1 Curr Limit AO

CH1CL-O

Chiller1 CurrLim

Output

Eff Chlr1 Curr Limit Cmd

CH1CL-%

Chlr1 Curr Limit

Effective Command

Chlr1 CW ISO Valve AO

CH1CWISOV-O

Chiller1 CW Iso Valve

Output

 

N/A

   

Chlr1 CW Iso Valve BO

CH1CWISOV-C

Chiller1 CW Iso Valve

Command

 

N/A

   

Chlr1 Setpoint AO

CH1SP-O

Chiller1 Setpoint

Output

Eff Chlr1 Setpoint Cmd

CH1SP-%

Chlr1 Setpoint

Effective Command

Chlr2 BO

CH2-EN

Chiller2

Command

 

N/A

   

Chlr2 CHW ISO Valve AO

CH2CHWISOV-O

Chiller2 CHW Iso Valve

Output

 

N/A

   

Chlr2 CHW Iso Valve BO

CH2CHWISOV-C

Chiller2 CHW Iso Valve

Command

 

N/A

   

Chlr2 Curr Limit AO

CH2CL-O

Chiller2 CurrLim

Output

Eff Chlr2 Curr Limit Cmd

CH2CL-%

Chlr2 Curr Limit

Effective Command

Chlr2 CW ISO Valve AO

CH2CWISOV-O

Chiller2 CW Iso Valve

Output

 

N/A

   

Chlr2 CW Iso Valve BO

CH2CWISOV-C

Chiller2 CW Iso Valve

Command

 

N/A

   

Chlr2 Setpoint AO

CH2SP-O

Chiller2 Setpoint

Output

Eff Chlr2 Setpoint Cmd

CH2SP-%

Chlr2 Setpoint

Effective Command

Chlr3 BO

CH3-EN

Chiller3

Command

 

N/A

   

Chlr3 CHW ISO Valve AO

CH3CHWISOV-O

Chiller3 CHW Iso Valve

Output

 

N/A

   

Chlr3 CHW Iso Valve BO

CH3CHWISOV-C

Chiller3 CHW Iso Valve

Command

 

N/A

   

Chlr3 Curr Limit AO

CH3CL-O

Chiller3 CurrLim

Output

Eff Chlr3 Curr Limit Cmd

CH3CL-%

Chlr3 Curr Limit

Effective Command

Chlr3 CW ISO Valve AO

CH3CWISOV-O

Chiller3 CW Iso Valve

Output

 

N/A

   

Chlr3 CW Iso Valve BO

CH3CWISOV-C

Chiller3 CW Iso Valve

Command

 

N/A

   

Chlr3 Setpoint AO

CH3SP-O

Chiller3 Setpoint

Output

Eff Chlr3 Setpoint Cmd

CH3SP-%

Chlr3 Setpoint

Effective Command

Chlr4 BO

CH4-EN

Chiller4

Command

 

N/A

   

Chlr4 CHW ISO Valve AO

CH4CHWISOV-O

Chiller4 CHW Iso Valve

Output

 

N/A

   

Chlr4 CHW Iso Valve BO

CH4CHWISOV-C

Chiller4 CHW Iso Valve

Command

 

N/A

   

Chlr4 Curr Limit AO

CH4CL-O

Chiller4 CurrLim

Output

Eff Chlr4 Curr Limit Cmd

CH4CL-%

Chlr4 Curr Limit

Effective Command

Chlr4 CW ISO Valve AO

CH4CWISOV-O

Chiller4 CW Iso Valve

Output

 

N/A

   

Chlr4 CW Iso Valve BO

CH4CWISOV-C

Chiller4 CW Iso Valve

Command

 

N/A

   

Chlr4 Setpoint AO

CH4SP-O

Chiller4 Setpoint

Output

Eff Chlr4 Setpoint Cmd

CH4SP-%

Chlr4 Setpoint

Effective Command

Chlr5 BO

CH5-EN

Chiller5

Command

 

N/A

   

Chlr5 CHW ISO Valve AO

CH5CHWISOV-O

Chiller5 CHW Iso Valve

Output

 

N/A

   

Chlr5 CHW Iso Valve BO

CH5CHWISOV-C

Chiller5 CHW Iso Valve

Command

 

N/A

   

Chlr5 Curr Limit AO

CH5CL-O

Chiller5 CurrLim

Output

Eff Chlr5 Curr Limit Cmd

CH5CL-%

Chlr5 Curr Limit

Effective Command

Chlr5 CW ISO Valve AO

CH5CWISOV-O

Chiller5 CW Iso Valve

Output

 

N/A

   

Chlr5 CW Iso Valve BO

CH5CWISOV-C

Chiller5 CW Iso Valve

Command

 

N/A

   

Chlr5 Setpoint AO

CH5SP-O

Chiller5 Setpoint

Output

Eff Chlr5 Setpoint Cmd

CH5SP-%

Chlr5 Setpoint

Effective Command

Chlr6 BO

CH6-EN

Chiller6

Command

 

N/A

   

Chlr6 CHW ISO Valve AO

CH6CHWISOV-O

Chiller6 CHW Iso Valve

Output

 

N/A

   

Chlr6 CHW Iso Valve BO

CH6CHWISOV-C

Chiller6 CHW Iso Valve

Command

 

N/A

   

Chlr6 Curr Limit AO

CH6CL-O

Chiller6 CurrLim

Output

Eff Chlr6 Curr Limit Cmd

CH6CL-%

Chlr6 Curr Limit

Effective Command

Chlr6 CW ISO Valve AO

CH6CWISOV-O

Chiller6 CW Iso Valve

Output

 

N/A

   

Chlr6 CW Iso Valve BO

CH6CWISOV-C

Chiller6 CW Iso Valve

Command

 

N/A

   

Chlr6 Setpoint AO

CH6SP-O

Chiller6 Setpoint

Output

Eff Chlr6 Setpoint Cmd

CH6SP-%

Chlr6 Setpoint

Effective Command

Chlr7 BO

CH7-EN

Chiller7

Command

 

N/A

   

Chlr7 CHW ISO Valve AO

CH7CHWISOV-O

Chiller7 CHW Iso Valve

Output

 

N/A

   

Chlr7 CHW Iso Valve BO

CH7CHWISOV-C

Chiller7 CHW Iso Valve

Command

 

N/A

   

Chlr7 Curr Limit AO

CH7CL-O

Chiller7 CurrLim

Output

Eff Chlr7 Curr Limit Cmd

CH7CL-%

Chlr7 Curr Limit

Effective Command

Chlr7 CW ISO Valve AO

CH7CWISOV-O

Chiller7 CW Iso Valve

Output

 

N/A

   

Chlr7 CW Iso Valve BO

CH7CWISOV-C

Chiller7 CW Iso Valve

Command

 

N/A

   

Chlr7 Setpoint AO

CH7SP-O

Chiller7 Setpoint

Output

Eff Chlr7 Setpoint Cmd

CH7SP-%

Chlr7 Setpoint

Effective Command

Chlr8 BO

CH8-EN

Chiller8

Command

 

N/A

   

Chlr8 CHW ISO Valve AO

CH8CHWISOV-O

Chiller8 CHW Iso Valve

Output

 

N/A

   

Chlr8 CHW Iso Valve BO

CH8CHWISOV-C

Chiller8 CHW Iso Valve

Command

 

N/A

   

Chlr8 Curr Limit AO

CH8CL-O

Chiller8 CurrLim

Output

Eff Chlr8 Curr Limit Cmd

CH8CL-%

Chlr8 Curr Limit

Effective Command

Chlr8 CW ISO Valve AO

CH8CWISOV-O

Chiller8 CW Iso Valve

Output

 

N/A

   

Chlr8 CW Iso Valve BO

CH8CWISOV-C

Chiller8 CW Iso Valve

Command

 

N/A

   

Chlr8 Setpoint AO

CH8SP-O

Chiller8 Setpoint

Output

Eff Chlr8 Setpoint Cmd

CH8SP-%

Chlr8 Setpoint

Effective Command

CHW Bypass Valve AO

CHWBYPV-O

CHW Bypass Loop

Output

Eff CHW Bypass Valve Cmd

CHWBYPV-%

CHW Bypass Valve

Effective Command

CD PAO Stroke Time

PARAM-CD-ST

Cold Deck Damper

StrokeTime

 

N/A

   

Cold Deck Damper AO

CD-O

Cold Deck Damper

Output

Eff Cold Deck Damper Cmd

CD-%

Cold Deck Damper

Effective Command

Cold Deck Damper PAO

CD-O

Cold Deck Damper

Output_ PAO

Eff Cold Deck Damper Cmd

CD-%

Cold Deck Damper

Effective Command

Cold Deck Damper PAO

CD-O

Cold Deck Damper

Output_PAO_ Integrated

Eff Cold Deck Damper Cmd

CD-%

Cold Deck Damper

Effective Command

Cold Deck PAO - Minimum Pulse Width

PARAM-CD-MINP

Cold Deck Damper

MinPulse

 

N/A

   

Combustion Damper BO

COMBDPR-C

Combustion Damper

Command

 

N/A

   

Compressor Stage 1 BO

COMP1-C

Compressor

Stage 1 Command

Eff Compressor Stage 1 Binary Cmd

COMP1-EC

Compressor Stage 1

Effective Stg Command

Compressor Stage 2 BO

COMP2-C

Compressor

Stage 2 Command

Eff Compressor Stage 2 Binary Cmd

COMP2-EC

Compressor Stage 2

Effective Stg Command

Cooling Circulation Pump 1 BO

CP1-C

2 Pipe Circulation Pump 1

Command

       

Cooling Circulation Pump 2 BO

CP2-C

2 Pipe Circulation Pump 2

Command

       

CWP1 AO

CWP1-O

Cond Water Pump1

Output

 

N/A

   

CWP1 BO

CWP1-C

Cond Water Pump1

Command

 

N/A

   

CWP2 AO

CWP2-O

Cond Water Pump2

Output

 

N/A

   

CWP2 BO

CWP2-C

Cond Water Pump2

Command

 

N/A

   

CWP3 AO

CWP3-O

Cond Water Pump3

Output

 

N/A

   

CWP3 BO

CWP3-C

Cond Water Pump3

Command

 

N/A

   

CWP4 AO

CWP4-O

Cond Water Pump4

Output

 

N/A

   

CWP4 BO

CWP4-C

Cond Water Pump4

Command

 

N/A

   

CWP5 AO

CWP5-O

Cond Water Pump5

Output

 

N/A

   

CWP5 BO

CWP5-C

Cond Water Pump5

Command

 

N/A

   

CWP6 AO

CWP6-O

Cond Water Pump6

Output

 

N/A

   

CWP6 BO

CWP6-C

Cond Water Pump6

Command

 

N/A

   

CWP7 AO

CWP7-O

Cond Water Pump7

Output

 

N/A

   

CWP7 BO

CWP7-C

Cond Water Pump7

Command

 

N/A

   

CWP8 AO

CWP8-O

Cond Water Pump8

Output

 

N/A

   

CWP8 BO

CWP8-C

Cond Water Pump8

Command

 

N/A

   

Cooling Valve AO

CLG-O

Cooling

Output

Eff Cooling Valve Cmd

CLG-%

Cooling Valve

Effective Command

Cooling Valve BO

CLG-C

Cooling

Command

Eff Cooling Valve Binary Cmd

CLG-EC

Cooling Valve

Effective Vlv Command

Cooling Valve PAO

CLG-O

Cooling

Output_PAO

Eff Cooling Valve Cmd

CLG-%

Cooling Valve

Effective Command

Cooling Damper AO

CLGFBD-O

Cooling Face & Bypass Damper

Output

Eff Cooling Damper Cmd

CLGFBD-%

Cooling Damper

Effective Command

Cooling Damper PAO

CLGFBD-O

Cooling Face & Bypass Damper

Output_PAO

Eff Cooling Damper Cmd

CLGFBD-%

Cooling Damper

Effective Command

Cooling Circulation Pump BO

CP-C

Cooling Pump

Command

 

N/A

   

Cooling Stage 1 BO

CLG1-C

Cooling Stage

Stage 1 Command

Eff Cooling Stage 1 Binary Cmd

CLG1-EC

Cooling Stage 1

Effective Stg Command

Cooling Stage 2 BO

CLG2-C

Cooling Stage

Stage 2 Command

Eff Cooling Stage 2 Binary Cmd

CLG2-EC

Cooling Stage 2

Effective Stg Command

Cooling Stage 3 BO

CLG3-C

Cooling Stage

Stage 3 Command

Eff Cooling Stage 3 Binary Cmd

CLG3-EC

Cooling Stage 3

Effective Stg Command

Cooling Stage 4 BO

CLG4-C

Cooling Stage

Stage 4 Command

Eff Cooling Stage 4 Binary Cmd

CLG4-EC

Cooling Stage 4

Effective Stg Command

Cooling Stage 5 BO

CLG5-C

Cooling Stage

Stage 5 Command

Eff Cooling Stage 5 Binary Cmd

CLG5-EC

Cooling Stage 5

Effective Stg Command

Cooling Stage 6 BO

CLG6-C

Cooling Stage

Stage 6 Command

Eff Cooling Stage 6 Binary Cmd

CLG6-EC

Cooling Stage 6

Effective Stg Command

Cooling Stage 7 BO

CLG7-C

Cooling Stage

Stage 7 Command

Eff Cooling Stage 7 Binary Cmd

CLG7-EC

Cooling Stage 7

Effective Stg Command

Cooling Stage 8 BO

CLG8-C

Cooling Stage

Stage 8 Command

Eff Cooling Stage 8 Binary Cmd

CLG8-EC

Cooling Stage 8

Effective Stg Command

Cooling Valve Command BO

CLG-C

Cooling Valve

Command

Eff Cooling Valve Binary Cmd

CLG-EC

Cooling Valve

Effective Vlv Command

Current Out 1 AO

CURRENT1-O

Current 1

Output

 

N/A

   

Current Out 2 AO

CURRENT2-O

Current 2

Output

 

N/A

   

Current Out 3 AO

CURRENT3-O

Current 3

Output

 

N/A

   

Current Out 4 AO

CURRENT4-O

Current 4

Output

 

N/A

   

Current Out 5 AO

CURRENT5-O

Current 5

Output

 

N/A

   

Current Out 6 AO

CURRENT6-O

Current 6

Output

 

N/A

   

Domestic HW Valve AO

DHWV-O

Domestic HW Valve

Output

Eff Domestic HW Valve Cmd

DHWV-%

Domestic HW Valve

Effective Command

Economizer Enable BO

ECON-C

Economizer Enable

Command

 

N/A

   

Exhaust Air Damper AO

EAD-O

Exhaust Air Damper

Output

Eff Exhaust Air Damper Cmd

EAD-%

Exhaust Air Damper

Effective Command

Exhaust Air Damper BO

EAD-C

Exhaust Air Damper

Command

 

N/A

   

Exhaust Air Damper PAO

EAD-O

Exhaust Air Damper

Output_PAO

Eff Exhaust Air Damper Cmd

EAD-%

Exhaust Air Damper

Effective Command

Exhaust Air Damper PAO - Minimum Pulse Width

PARAM-EAD-MINP

Exhaust Air Damper

MinPulse

 

N/A

   

Exhaust Damper PAO Stroke Time

PARAM-EAD-ST

Exhaust Air Damper

StrokeTime

 

N/A

   
Exhaust Air Damper2 BO EAD2-C Exhaust Air Damper2 Command        

Exhaust Fan BO

EF-C

Exhaust Fan

Command

 

N/A

   

Exhaust Fan BO

EF-C

Exhaust Fan

Run/Stop

 

N/A

   

Exhaust Fan Speed AO

EF-O

Exhaust Fan

Output

Eff Exhaust Fan Speed Cmd

EF-%

Exhaust Fan Speed

Effective Command

VSD Bypass Drive BV

EF-BYPASS

Exhaust Fan

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

EF-RESET

Exhaust Fan

Reset Drive Fault

 

N/A

   

Exhaust Fan2 BO

EF2-C

Exhaust Fan2

Command

 

N/A

   

Exhaust Fan2 BO

EF2-C

Exhaust Fan2

Run/Stop

 

N/A

   

Exhaust Fan2 Speed AO

EF2-O

Exhaust Fan2

Output

Eff Exhaust Fan2 Speed Cmd

EF2-%

Exhaust Fan2 Speed

Effective Command

FBP Damper AO

FBD-O

Face & Bypass Damper

Output

Eff FBP Damper Cmd

FBD-%

FBP Damper

Effective Command

FBP Damper PAO

FBD-O

Face & Bypass Damper

Output_PAO

Eff FBP Damper Cmd

FBD-%

FBP Damper

Effective Command

Fan BO

SF-C

Fan

Command

 

N/A

   

Fan Speed 1 BO

SFL-C

Fan

Command LO

 

N/A

   

Fan Speed 2 BO

SFM-C

Fan

Command MED

 

N/A

   

Fan Speed 3 BO

SFH-C

Fan

Command HI

 

N/A

   

Fan Speed AO

SF-O

Fan

Output

 

N/A

   

GEF BO

GEF-C

GEF

Command

 

N/A

   

Heat Recovery Valve AO

HR-O

Heat Recovery

Output

Eff Heat Recovery Valve Cmd

HR-%

Heat Recovery Valve

Effective Command

Heat Recovery Valve BO

HR-C

Heat Recovery

Command

 

N/A

   

Heat Recovery Valve PAO

HR-O

Heat Recovery

Output_PAO

Eff Heat Recovery Valve Cmd

HR-%

Heat Recovery Valve

Effective Command

Heat Recovery Exhaust FBD AO

HREAFBD-O

Heat Recovery EA FBD AO

Output

 

N/A

   

Heat Recovery Exhaust FBD BO

HREAFBD-C

Heat Recovery EA FBD BO

Command

 

N/A

   

Heat Recovery OA FBD AO

HROAFBD-O

Heat Recovery OA FBD AO

Output

 

N/A

   

Heat Recovery OA FBD BO

HROAFBD-C

Heat Recovery OA FBD BO

Command

 

N/A

   

Heat Recovery Pump BO

HRP-C

Heat Recovery Pump

Command

 

N/A

   

Heat Recovery Wheel AO

HRW-O

Heat Recovery Wheel

Output

Eff Heat Recovery Wheel Cmd

HR-%

Heat Recovery Wheel

Effective Command

Heat Recovery Wheel BO

HRW-C

Heat Recovery Wheel

Command

 

N/A

   

Heat Tape 1 Command BO

HTAPE1-C

Heat Tape 1

Command

 

N/A

   

Heat Tape 2 Command BO

HTAPE2-C

Heat Tape 2

Command

 

N/A

   

Heat Tape 3 Command BO

HTAPE3-C

Heat Tape 3

Command

 

N/A

   

Heat Tape 4 Command BO

HTAPE4-C

Heat Tape 4

Command

 

N/A

   

Heat Tape 5 Command BO

HTAPE5-C

Heat Tape 5

Command

 

N/A

   

Heat Tape 6 Command BO

HTAPE6-C

Heat Tape 6

Command

 

N/A

   

Heating Stage 1 BO

HTG1-C

Heating

Stage 1 Command

Eff Heating Stage 1 Binary Cmd

HTG1-EC

Heating Stage 1

Effective Stg Command

Heating Stage 2 BO

HTG2-C

Heating

Stage 2 Command

Eff Heating Stage 2 Binary Cmd

HTG2-EC

Heating Stage 2

Effective Stg Command

Heating Stage 3 BO

HTG3-C

Heating

Stage 3 Command

Eff Heating Stage 3 Binary Cmd

HTG3-EC

Heating Stage 3

Effective Stg Command

Heating Valve AO

HTG-O

Heating

Output

Eff Heating Valve Cmd

HTG-%

Heating Valve

Effective Command

Heating Valve BO

HTG-C

Heating

Command

Eff Heating Valve Binary Cmd

HTG-EC

Heating Valve

Effective Vlv Command

Heating Valve PAO

HTG-O

Heating

Output_PAO

Eff Heating Valve Cmd

HTG-%

Heating Valve

Effective Command

Reheat Valve 1 AO

HTG1-O

Heating 1

Output

Eff Reheat Valve 1 Cmd

HTG1-%

Reheat Valve 1

Effective Command

Reheat Valve 2 AO

HTG2-O

Heating 2

Output

Eff Reheat Valve 2 Cmd

HTG2-%

Reheat Valve 2

Effective Command

Reheat Stage 1 BO

HTG1-C

Heating Stage

Stage 1 Command

Eff Reheat Stage 1 Binary Cmd

HTG1-EC

Reheat Stage 1

Effective Stg Command

Reheat Stage 2 BO

HTG2-C

Heating Stage

Stage 2 Command

Eff Reheat Stage 2 Binary Cmd

HTG2-EC

Reheat Stage 2

Effective Stg Command

Reheat Stage 3 BO

HTG3-C

Heating Stage

Stage 3 Command

Eff Reheat Stage 3 Binary Cmd

HTG3-EC

Reheat Stage 3

Effective Stg Command

Reheat Stage 4 BO

HTG4-C

Heating Stage

Stage 4 Command

Eff Reheat Stage 4 Binary Cmd

HTG4-EC

Reheat Stage 4

Effective Stg Command

Reheat Stage 5 BO

HTG5-C

Heating Stage

Stage 5 Command

Eff Reheat Stage 5 Binary Cmd

HTG5-EC

Reheat Stage 5

Effective Stg Command

Reheat Stage 6 BO

HTG6-C

Heating Stage

Stage 6 Command

Eff Reheat Stage 6 Binary Cmd

HTG6-EC

Reheat Stage 6

Effective Stg Command

Reheat Stage 7 BO

HTG7-C

Heating Stage

Stage 7 Command

Eff Reheat Stage 7 Binary Cmd

HTG7-EC

Reheat Stage 7

Effective Stg Command

Reheat Stage 8 BO

HTG8-C

Heating Stage

Stage 8 Command

Eff Reheat Stage 8 Binary Cmd

HTG8-EC

Reheat Stage 8

Effective Stg Command

Heating Valve Command BO

HTG-C

Heating Valve

Command

Eff Heating Valve Binary Cmd

HTG-EC

Heating Valve

Effective Vlv Command

2 Pipe Valve AO

HC-O

Heating/Cooling

Output

Eff 2 Pipe Valve Cmd

HC-%

2 Pipe Valve

Effective Command

2 Pipe Valve BO

HC-C

Heating/Cooling

Command

Eff 2 Pipe Valve Binary Cmd

HC-EC

2 Pipe Valve

Effective Vlv Command

2 Pipe Valve PAO

HC-O

Heating/Cooling

Output_PAO

Eff 2 Pipe Valve Cmd

HC-%

2 Pipe Valve

Effective Command

2 Pipe Damper AO

HCFBD-O

Heating/Cooling Face & Bypass Damper

Output

Eff 2 Pipe Damper Cmd

HCFBD-%

2 Pipe Damper

Effective Command

2 Pipe Damper PAO

HCFBD-O

Heating/Cooling Face & Bypass Damper

Output_PAO

Eff 2 Pipe Damper Cmd

HCFBD-%

2 Pipe Damper

Effective Command

2 Pipe Circulation Pump BO

HCP-C

Heating/Cooling Pump

Command

 

N/A

   

2 Pipe Valve Command BO

HC-C

Heating/Cooling Valve

Command

Eff 2 Pipe Valve Binary Cmd

HC-EC

2 Pipe Valve

Effective Vlv Command

HD PAO Stroke Time

PARAM-HD-ST

Hot Deck Damper

StrokeTime

 

N/A

   

Hot Deck Damper AO

HD-O

Hot Deck Damper

Output

Eff Hot Deck Damper Cmd

HD-%

Hot Deck Damper

Effective Command

Hot Deck Damper PAO

HD-O

Hot Deck Damper

Output_PAO

Eff Hot Deck Damper Cmd

HD-%

Hot Deck Damper

Effective Command

Hot Deck Damper PAO

HD-O

Hot Deck Damper

Output_PAO

_Integrated

Eff Hot Deck Damper Cmd

HD-%

Hot Deck Damper

Effective Command

Hot Deck PAO - Minimum Pulse Width

PARAM-HD-MINP

Hot Deck Damper

MinPulse

 

N/A

   

Hot Gas Bypass Valve BO

HGBPV-C

Hot Gas Bypass Valve

Command

 

N/A

   

Iso Valve BO

ISOVLV-C

HP Iso Valve

Command

 

N/A

   

Humidification AO

HUM-O

Humidifier

Output

Eff Humidification Cmd

HUM-%

Humidification

Effective Command

Humidifier Enable BO

HUM-C

Humidifier Enable

Command

 

N/A

   

Humidification Stage 1 BO

HUM1-C

Humidifier Stage

Stage 1 Command

Eff Humidification Stage 1 Binary Cmd

HUM1-EC

Humidification Stage 1

Effective Stg Command

Humidification Stage 2 BO

HUM2-C

Humidifier Stage

Stage 2 Command

Eff Humidification Stage 2 Binary Cmd

HUM2-EC

Humidification Stage 2

Effective Stg Command

Humidification Stage 3 BO

HUM3-C

Humidifier Stage

Stage 3 Command

Eff Humidification Stage 3 Binary Cmd

HUM3-EC

Humidification Stage 3

Effective Stg Command

Humidification Stage 4 BO

HUM4-C

Humidifier Stage

Stage 4 Command

Eff Humidification Stage 4 Binary Cmd

HUM4-EC

Humidification Stage 4

Effective Stg Command

HW Mixing Valve AO

HXMV-O

HX Mixing Valve

Output

Eff HW Mixing Valve Cmd

MIX-%

HW Mixing Valve

Effective Command

HX1 Iso Valve BO

HX1ISOV-C

HX1 Iso Valve

Command

 

N/A

   

HX1 AO1

HX1V1-O

HX1 Valve 1

Output

Eff HX1 Valve 1 Cmd

HX1V1-%

HX1 Valve 1

Effective Command

HX1 AO2

HX1V2-O

HX1 Valve 2

Output

Eff HX1 Valve 2 Cmd

HX1V2-%

HX1 Valve 2

Effective Command

HX2 Iso Valve BO

HX2ISOV-C

HX2 Iso Valve

Command

 

N/A

   

HX2 AO1

HX2V1-O

HX2 Valve 1

Output

Eff HX2 Valve 1 Cmd

HX2V1-%

HX2 Valve 1

Effective Command

HX2 AO2

HX2V2-O

HX2 Valve 2

Output

Eff HX2 Valve 2 Cmd

HX2V2-%

HX2 Valve 2

Effective Command

Lighting BO

LIGHT-C

Lighting

Command

 

N/A

   

Minimum OA Damper AO

MOAD-O

Min Outdoor Air Damper

Output

Eff Minimum OA Damper Cmd

MOAD-%

Minimum OA Damper

Effective Command

Minimum OA Damper BO

MOAD-C

Min Outdoor Air Damper

Command

 

N/A

   

Minimum OA Fan AO

MOAF-O

Min Outdoor Air Fan

Output

Eff Minimum OA Fan Cmd

MOAF-%

Minimum OA Fan

Effective Command

Minimum OA Fan BO

MOAF-C

Min Outdoor Air Fan

Command

 

N/A

   

Minimum OA Fan BO

MOAF-C

Min Outdoor Air Fan

Run/Stop

 

N/A

   

VSD Bypass Drive BV

MOAF-BYPASS

Min Outdoor Air Fan

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

MOAF-RESET

Min Outdoor Air Fan

Reset Drive Fault

 

N/A

   

Misc 1 Command BO

MISC1-C

Misc 1

Command

 

N/A

   

Misc 2 Command BO

MISC2-C

Misc 2

Command

 

N/A

   

Misc 3 Command BO

MISC3-C

Misc 3

Command

 

N/A

   

Misc 4 Command BO

MISC4-C

Misc 4

Command

 

N/A

   

Misc 5 Command BO

MISC5-C

Misc 5

Command

 

N/A

   

Misc 6 Command BO

MISC6-C

Misc 6

Command

 

N/A

   

Cooling Valve PAO

MISC-O

Miscellaneous

Output_PAO

 

N/A

   

Mixed Air Damper AO

MISC-O

Miscellaneous

Output

Eff Mixed Air Damper Cmd

MAD-%

Mixed Air Damper

Effective Command

Reheat Stage 1 BO

MISC1-C

Miscellaneous

Stage 1 Command

Eff Reheat Stage 1 Binary Cmd

MISC1-EC

Miscellaneous

Effective Stg Command

Reheat Stage 2 BO

MISC2-C

Miscellaneous

Stage 2 Command

Eff Reheat Stage 2 Binary Cmd

MISC2-EC

Miscellaneous

Effective Stg Command

Reheat Stage 3 BO

MISC3-C

Miscellaneous

Stage 3 Command

Eff Reheat Stage 3 Binary Cmd

MISC3-EC

Miscellaneous

Effective Stg Command

Reheat Stage 4 BO

MISC4-C

Miscellaneous

Stage 4 Command

Eff Reheat Stage 4 Binary Cmd

MISC4-EC

Miscellaneous

Effective Stg Command

Reheat Stage 5 BO

MISC5-C

Miscellaneous

Stage 5 Command

Eff Reheat Stage 5 Binary Cmd

MISC5-EC

Miscellaneous

Effective Stg Command

Reheat Stage 6 BO

MISC6-C

Miscellaneous

Stage 6 Command

Eff Reheat Stage 6 Binary Cmd

MISC6-EC

Miscellaneous

Effective Stg Command

Reheat Stage 7 BO

MISC7-C

Miscellaneous

Stage 7 Command

Eff Reheat Stage 7 Binary Cmd

MISC7-EC

Miscellaneous

Effective Stg Command

Reheat Stage 8 BO

MISC8-C

Miscellaneous

Stage 8 Command

Eff Reheat Stage 8 Binary Cmd

MISC8-EC

Miscellaneous

Effective Stg Command

Supply Fan BO

MISC-C

Miscellaneous

Command

 

N/A

   

Mixed Air Damper AO

MAD-O

Mixed Air Damper

Output

Eff Mixed Air Damper Cmd

MAD-%

Mixed Air Damper

Effective Command

HW Mixing Valve AO

MIX-O

Mixing Valve

Output

Eff Mixing Valve Cmd

MIX-%

Mixing Valve

Effective Command

Motor 1 Command BO

MOTOR1-C

Motor 1

Command

 

N/A

   

Motor 2 Command BO

MOTOR2-C

Motor 2

Command

 

N/A

   

Motor 3 Command BO

MOTOR3-C

Motor 3

Command

 

N/A

   

Motor 4 Command BO

MOTOR4-C

Motor 4

Command

 

N/A

   

Motor 5 Command BO

MOTOR5-C

Motor 5

Command

 

N/A

   

Motor 6 Command BO

MOTOR6-C

Motor 6

Command

 

N/A

   

OA Damper AO

OAD-O

Outdoor Air Damper

Output

Eff OA Damper Cmd

OAD-%

OA Damper

Effective Command

OA Damper BO

OAD-C

Outdoor Air Damper

Command

 

N/A

   

OA Damper2 BO

OAD2-C

OA Damper2

Command

 

N/A

   

Fan BO

SF-C

Parallel Supply Fan

Command

 

N/A

   

PCHWP 1 AO

PCHWP1-O

PCHWP1

Output

Eff PCHWP 1 Cmd

PCHWP1-%

PCHWP 1

Effective Command

PCHWP1 BO

PCHWP1-C

PCHWP1

Command

 

N/A

   

PCHWP 2 AO

PCHWP2-O

PCHWP2

Output

Eff PCHWP 2 Cmd

PCHWP2-%

PCHWP 2

Effective Command

PCHWP2 BO

PCHWP2-C

PCHWP2

Command

 

N/A

   

PCHWP 3 AO

PCHWP3-O

PCHWP3

Output

Eff PCHWP 3 Cmd

PCHWP3-%

PCHWP 3

Effective Command

PCHWP3 BO

PCHWP3-C

PCHWP3

Command

 

N/A

   

PCHWP 4 AO

PCHWP4-O

PCHWP4

Output

Eff PCHWP 4 Cmd

PCHWP4-%

PCHWP 4

Effective Command

PCHWP4 BO

PCHWP4-C

PCHWP4

Command

 

N/A

   

PCHWP 5 AO

PCHWP5-O

PCHWP5

Output

Eff PCHWP 5 Cmd

PCHWP5-%

PCHWP 5

Effective Command

PCHWP5 BO

PCHWP5-C

PCHWP5

Command

 

N/A

   

PCHWP 6 AO

PCHWP6-O

PCHWP6

Output

Eff PCHWP 6 Cmd

PCHWP6-%

PCHWP 6

Effective Command

PCHWP6 BO

PCHWP6-C

PCHWP6

Command

 

N/A

   

PCHWP 7 AO

PCHWP7-O

PCHWP7

Output

Eff PCHWP 7 Cmd

PCHWP7-%

PCHWP 7

Effective Command

PCHWP7 BO

PCHWP7-C

PCHWP7

Command

 

N/A

   

PCHWP 8 AO

PCHWP8-O

PCHWP8

Output

Eff PCHWP 8 Cmd

PCHWP8-%

PCHWP 8

Effective Command

PCHWP8 BO

PCHWP8-C

PCHWP8

Command

 

N/A

   

PHWP1 AO

PHWP1-O

PHWP1

Output

Eff PHWP1 Cmd

PHWP1-%

PHWP1

Effective Command

PHWP1 BO

PHWP1-C

PHWP1

Command

 

N/A

   

PHWP2 AO

PHWP2-O

PHWP2

Output

Eff PHWP2 Cmd

PHWP2-%

PHWP2

Effective Command

PHWP2 BO

PHWP2-C

PHWP2

Command

 

N/A

   

PHWP3 AO

PHWP3-O

PHWP3

Output

Eff PHWP3 Cmd

PHWP3-%

PHWP3

Effective Command

PHWP3 BO

PHWP3-C

PHWP3

Command

 

N/A

   

PHWP4 AO

PHWP4-O

PHWP4

Output

Eff PHWP4 Cmd

PHWP4-%

PHWP4

Effective Command

PHWP4 BO

PHWP4-C

PHWP4

Command

 

N/A

   

PHWP5 AO

PHWP5-O

PHWP5

Output

Eff PHWP5 Cmd

PHWP5-%

PHWP5

Effective Command

PHWP5 BO

PHWP5-C

PHWP5

Command

 

N/A

   

PHWP6 AO

PHWP6-O

PHWP6

Output

Eff PHWP6 Cmd

PHWP6-%

PHWP6

Effective Command

PHWP6 BO

PHWP6-C

PHWP6

Command

 

N/A

   

PHWP7 AO

PHWP7-O

PHWP7

Output

Eff PHWP7 Cmd

PHWP7-%

PHWP7

Effective Command

PHWP7 BO

PHWP7-C

PHWP7

Command

 

N/A

   

PHWP8 AO

PHWP8-O

PHWP8

Output

Eff PHWP8 Cmd

PHWP8-%

PHWP8

Effective Command

PHWP8 BO

PHWP8-C

PHWP8

Command

 

N/A

   

Preheat Valve AO

PH-O

Preheat

Output

Eff Preheat Valve Cmd

PH-%

Preheat Valve

Effective Command

Preheat Valve BO

PH-C

Preheat

Command

Eff Preheat Valve Binary Cmd

PH-EC

Preheat Valve

Effective Vlv Command

Preheat Valve PAO

PH-O

Preheat

Output_PAO

Eff Preheat Valve Cmd

PH-%

Preheat Valve

Effective Command

Preheat Valve 1 AO

PH1-O

Preheat 1

Output

Eff Preheat Valve 1 Cmd

PH1-%

Preheat Valve 1

Effective Command

Preheat Valve 2 AO

PH2-O

Preheat 2

Output

Eff Preheat Valve 2 Cmd

PH2-%

Preheat Valve 2

Effective Command

Preheat Enable BO

PH-EN

Preheat Enable

Command

 

N/A

   

Preheat Damper AO

PHFBD-O

Preheat Face & Bypass Damper

Output

Eff Preheat Damper Cmd

PHFBD-%

Preheat Damper

Effective Command

Preheat Damper PAO

PHFBD-O

Preheat Face & Bypass Damper

Output_PAO

Eff Preheat Damper Cmd

PHFBD-%

Preheat Damper

Effective Command

Preheat Circulation Pump BO

PHP-C

Preheat Pump

Command

 

N/A

   

Preheat Circulation Pump 1 BO

PHP1-C

Preheat Circulation Pump 1

Command

 

N/A

   

Preheat Circulation Pump 2 BO

PHP2-C

Preheat Circulation Pump 2

Command

 

N/A

   

Preheat Stage 1 BO

PH1-C

Preheat Stage

Stage 1 Command

Eff Preheat Stage 1 Binary Cmd

PH1-EC

Preheat Stage 1

Effective Stg Command

Preheat Stage 2 BO

PH2-C

Preheat Stage

Stage 2 Command

Eff Preheat Stage 2 Binary Cmd

PH2-EC

Preheat Stage 2

Effective Stg Command

Preheat Stage 3 BO

PH3-C

Preheat Stage

Stage 3 Command

Eff Preheat Stage 3 Binary Cmd

PH3-EC

Preheat Stage 3

Effective Stg Command

Preheat Stage 4 BO

PH4-C

Preheat Stage

Stage 4 Command

Eff Preheat Stage 4 Binary Cmd

PH4-EC

Preheat Stage 4

Effective Stg Command

Preheat Stage 5 BO

PH5-C

Preheat Stage

Stage 5 Command

Eff Preheat Stage 5 Binary Cmd

PH5-EC

Preheat Stage 5

Effective Stg Command

Preheat Stage 6 BO

PH6-C

Preheat Stage

Stage 6 Command

Eff Preheat Stage 6 Binary Cmd

PH6-EC

Preheat Stage 6

Effective Stg Command

Preheat Stage 7 BO

PH7-C

Preheat Stage

Stage 7 Command

Eff Preheat Stage 7 Binary Cmd

PH7-EC

Preheat Stage 7

Effective Stg Command

Preheat Stage 8 BO

PH8-C

Preheat Stage

Stage 8 Command

Eff Preheat Stage 8 Binary Cmd

PH8-EC

Preheat Stage 8

Effective Stg Command

Reheat Valve AO

RH-O

Reheat

Output

Eff Reheat Valve Cmd

RH-%

Reheat Valve

Effective Command

Reheat Valve PAO

RH-O

Reheat

Output_PAO

Eff Reheat Valve Cmd

RH-%

Reheat Valve

Effective Command

Reheat Enable BO

RF-EN

Reheat Enable

Command

 

N/A

   

Reheat Circulation Pump BO

RHP-C

Reheat Pump

Command

 

N/A

   

Reheat Circulation Pump 1 BO

RHP1-C

Reheat Circulation Pump 1

Command

 

N/A

   

Reheat Circulation Pump 2 BO

RHP2-C

Reheat Circulation Pump 2

Command

 

N/A

   

Relief Fan BO

RLF-C

Relief Fan

Command

 

N/A

   

Relief Fan BO

RLF-C

Relief Fan

Run/Stop

 

N/A

   

Relief Fan Speed AO

RLF-O

Relief Fan

Output

Eff Relief Fan Speed Cmd

RLF-%

Relief Fan Speed

Effective Command

VSD Bypass Drive BV

RLF-BYPASS

Relief Fan

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

RLF-RESET

Relief Fan

Reset Drive Fault

 

N/A

   

Relief Fan2 BO

RLF2-C

Relief Fan2

Command

 

N/A

   

Relief Fan2 BO

RLF2-C

Relief Fan2

Run/Stop

 

N/A

   

Relief Fan2 Speed AO

RLF2-O

Relief Fan2

Output

Eff Relief Fan2 Speed Cmd

RLF2-%

Relief Fan2 Speed

Effective Command

Return Air Damper AO

RAD-O

Return Air Damper

Output

Eff Return Air Damper Cmd

RAD-%

Return Air Damper

Effective Command

Return Fan BO

RF-C

Return Fan

Command

 

N/A

   

Return Fan BO

RF-C

Return Fan

Run/Stop

 

N/A

   

Return Fan Speed AO

RF-O

Return Fan

Output

Eff Return Fan Speed Cmd

RF-%

Return Fan Speed

Effective Command

VSD Bypass Drive BV

RF-BYPASS

Return Fan

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

RF-RESET

Return Fan

Reset Drive Fault

 

N/A

   

Return Fan2 BO

RF2-C

Return Fan2

Command

 

N/A

   

Return Fan2 BO

RF2-C

Return Fan2

Run/Stop

 

N/A

   

Return Fan2 Speed AO

RF2-O

Return Fan2

Output

Eff Return Fan2 Speed Cmd

RF2-%

Return Fan2 Speed

Effective Command

Reversing Valve 1 BO

REV1-C

Reversing Valve 1

Binary Output

 

N/A

   

Reversing Valve 2 BO

REV2-C

Reversing Valve 2

Binary Output

 

N/A

   

Sand Filter Command BO

SANDFILT-C

Sand Filter

Command

 

N/A

   

Drain Valve BO

HDV-C

Scrubber Drain

Command

 

N/A

   

Fill Valve BO

HFV-C

Scrubber Fill

Command

 

N/A

   

SCHWP1 AO

SCHWP1-O

Sec CHW Pump1

Output

Eff SCHWP1 Cmd

SCHWP1-%

SCHWP1

Effective Command

SCHWP1 BO

SCHWP1-C

Sec CHW Pump1

Command

Eff SCHWP1 Binary Cmd

SCHWP1-EC

SCHWP1

Effective Stg Command

VSD Bypass Drive BV

SCHWP1-BYPASS

Sec CHW Pump1

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

SCHWP1-RESET

Sec CHW Pump1

Reset Drive Fault

 

N/A

   

SCHWP2 AO

SCHWP2-O

Sec CHW Pump2

Output

Eff SCHWP2 Cmd

SCHWP2-%

SCHWP2

Effective Command

SCHWP2 BO

SCHWP2-C

Sec CHW Pump2

Command

Eff SCHWP2 Binary Cmd

SCHWP2-EC

SCHWP2

Effective Stg Command

VSD Bypass Drive BV

SCHWP2-BYPASS

Sec CHW Pump2

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

SCHWP2-RESET

Sec CHW Pump2

Reset Drive Fault

 

N/A

   

SCHWP3 AO

SCHWP3-O

Sec CHW Pump3

Output

Eff SCHWP3 Cmd

SCHWP3-%

SCHWP3

Effective Command

SCHWP3 BO

SCHWP3-C

Sec CHW Pump3

Command

Eff SCHWP3 Binary Cmd

SCHWP3-EC

SCHWP3

Effective Stg Command

VSD Bypass Drive BV

SCHWP3-BYPASS

Sec CHW Pump3

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

SCHWP3-RESET

Sec CHW Pump3

Reset Drive Fault

 

N/A

   

SCHWP4 AO

SCHWP4-O

Sec CHW Pump4

Output

Eff SCHWP4 Cmd

SCHWP4-%

SCHWP4

Effective Command

SCHWP4 BO

SCHWP4-C

Sec CHW Pump4

Command

Eff SCHWP4 Binary Cmd

SCHWP4-EC

SCHWP4

Effective Stg Command

VSD Bypass Drive BV

SCHWP4-BYPASS

Sec CHW Pump4

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

SCHWP4-RESET

Sec CHW Pump4

Reset Drive Fault

 

N/A

   

SCHWP5 AO

SCHWP5-O

Sec CHW Pump5

Output

Eff SCHWP5 Cmd

SCHWP5-%

SCHWP5

Effective Command

SCHWP5 BO

SCHWP5-C

Sec CHW Pump5

Command

Eff SCHWP5 Binary Cmd

SCHWP5-EC

SCHWP5

Effective Stg Command

VSD Bypass Drive BV

SCHWP5-BYPASS

Sec CHW Pump5

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

SCHWP5-RESET

Sec CHW Pump5

Reset Drive Fault

 

N/A

   

SCHWP6 AO

SCHWP6-O

Sec CHW Pump6

Output

Eff SCHWP6 Cmd

SCHWP6-%

SCHWP6

Effective Command

SCHWP6 BO

SCHWP6-C

Sec CHW Pump6

Command

Eff SCHWP6 Binary Cmd

SCHWP6-EC

SCHWP6

Effective Stg Command

VSD Bypass Drive BV

SCHWP6-BYPASS

Sec CHW Pump6

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

SCHWP6-RESET

Sec CHW Pump6

Reset Drive Fault

 

N/A

   

SCHWP7 AO

SCHWP7-O

Sec CHW Pump7

Output

Eff SCHWP7 Cmd

SCHWP7-%

SCHWP7

Effective Command

SCHWP7 BO

SCHWP7-C

Sec CHW Pump7

Command

Eff SCHWP7 Binary Cmd

SCHWP7-EC

SCHWP7

Effective Stg Command

VSD Bypass Drive BV

SCHWP7-BYPASS

Sec CHW Pump7

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

SCHWP7-RESET

Sec CHW Pump7

Reset Drive Fault

 

N/A

   

SCHWP8 AO

SCHWP8-O

Sec CHW Pump8

Output

Eff SCHWP8 Cmd

SCHWP8-%

SCHWP8

Effective Command

SCHWP8 BO

SCHWP8-C

Sec CHW Pump8

Command

Eff SCHWP8 Binary Cmd

SCHWP8-EC

SCHWP8

Effective Stg Command

VSD Bypass Drive BV

SCHWP8-BYPASS

Sec CHW Pump8

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

SCHWP8-RESET

Sec CHW Pump8

Reset Drive Fault

 

N/A

   

SHWP1 AO

SHWP1-O

Sec HW Pump1

Output

Eff SHWP1 Cmd

SHWP1-%

SHWP1

Effective Command

SHWP1 BO

SHWP1-C

Sec HW Pump1

Command

Eff SHWP1 Binary Cmd

SHWP1-EC

SHWP1

Effective Stg Command

VSD Bypass Drive BV

SHWP1-BYPASS

Sec HW Pump1

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

SHWP1-RESET

Sec HW Pump1

Reset Drive Fault

 

N/A

   

SHWP2 AO

SHWP2-O

Sec HW Pump2

Output

Eff SHWP2 Cmd

SHWP2-%

SHWP2

Effective Command

SHWP2 BO

SHWP2-C

Sec HW Pump2

Command

Eff SHWP2 Binary Cmd

SHWP2-EC

SHWP2

Effective Stg Command

VSD Bypass Drive BV

SHWP2-BYPASS

Sec HW Pump2

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

SHWP2-RESET

Sec HW Pump2

Reset Drive Fault

 

N/A

   

SHWP3 AO

SHWP3-O

Sec HW Pump3

Output

Eff SHWP3 Cmd

SHWP3-%

SHWP3

Effective Command

SHWP3 BO

SHWP3-C

Sec HW Pump3

Command

Eff SHWP3 Binary Cmd

SHWP3-EC

SHWP3

Effective Stg Command

VSD Bypass Drive BV

SHWP3-BYPASS

Sec HW Pump3

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

SHWP3-RESET

Sec HW Pump3

Reset Drive Fault

 

N/A

   

SHWP4 AO

SHWP4-O

Sec HW Pump4

Output

Eff SHWP4 Cmd

SHWP4-%

SHWP4

Effective Command

SHWP4 BO

SHWP4-C

Sec HW Pump4

Command

Eff SHWP4 Binary Cmd

SHWP4-EC

SHWP4

Effective Stg Command

VSD Bypass Drive BV

SHWP4-BYPASS

Sec HW Pump4

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

SHWP4-RESET

Sec HW Pump4

Reset Drive Fault

 

N/A

   

SHWP5 AO

SHWP5-O

Sec HW Pump5

Output

Eff SHWP5 Cmd

SHWP5-%

SHWP5

Effective Command

SHWP5 BO

SHWP5-C

Sec HW Pump5

Command

Eff SHWP5 Binary Cmd

SHWP5-EC

SHWP5

Effective Stg Command

VSD Bypass Drive BV

SHWP5-BYPASS

Sec HW Pump5

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

SHWP5-RESET

Sec HW Pump5

Reset Drive Fault

 

N/A

   

SHWP6 AO

SHWP6-O

Sec HW Pump6

Output

Eff SHWP6 Cmd

SHWP6-%

SHWP6

Effective Command

SHWP6 BO

SHWP6-C

Sec HW Pump6

Command

Eff SHWP6 Binary Cmd

SHWP6-EC

SHWP6

Effective Stg Command

VSD Bypass Drive BV

SHWP6-BYPASS

Sec HW Pump6

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

SHWP6-RESET

Sec HW Pump6

Reset Drive Fault

 

N/A

   

SHWP7 AO

SHWP7-O

Sec HW Pump7

Output

Eff SHWP7 Cmd

SHWP7-%

SHWP7

Effective Command

SHWP7 BO

SHWP7-C

Sec HW Pump7

Command

Eff SHWP7 Binary Cmd

SHWP7-EC

SHWP7

Effective Stg Command

VSD Bypass Drive BV

SHWP7-BYPASS

Sec HW Pump7

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

SHWP7-RESET

Sec HW Pump7

Reset Drive Fault

 

N/A

   

SHWP8 AO

SHWP8-O

Sec HW Pump8

Output

Eff SHWP8 Cmd

SHWP8-%

SHWP8

Effective Command

SHWP8 BO

SHWP8-C

Sec HW Pump8

Command

Eff SHWP8 Binary Cmd

SHWP8-EC

SHWP8

Effective Stg Command

VSD Bypass Drive BV

SHWP8-BYPASS

Sec HW Pump8

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

SHWP8-RESET

Sec HW Pump8

Reset Drive Fault

 

N/A

   

Sequenced Valves AO

HC-O

Sequenced Valves - Heating Cooling

Output

 

N/A

   

Fan BO

SF-C

Series Supply Fan

Command

 

N/A

   

Fan Speed AO

SF-O

Series Supply Fan

Output

 

N/A

   

Sideloop AO

SL-O

Sideloop

Output

Eff Sideloop Cmd

SL-%

Sideloop

Effective Command

Sideloop BO

SL-C

Sideloop

Command

Eff Sideloop Binary Cmd

SL-EC

Sideloop

Effective Vlv Command

Sideloop PAO

SL-O

Sideloop

Output_PAO

Eff Sideloop Cmd

SL-%

Sideloop

Effective Command

Sideloop Stage 1 BO

SL1-C

Sideloop

Stage 1 Command

Eff Sideloop Stage 1 Binary Cmd

SL1-EC

Sideloop Stage 1

Effective Stg Command

Sideloop Stage 2 BO

SL2-C

Sideloop

Stage 2 Command

Eff Sideloop Stage 2 Binary Cmd

SL2-EC

Sideloop Stage 2

Effective Stg Command

Sideloop Stage 3 BO

SL3-C

Sideloop

Stage 3 Command

Eff Sideloop Stage 3 Binary Cmd

SL3-EC

Sideloop Stage 3

Effective Stg Command

Sideloop Stage 4 BO

SL4-C

Sideloop

Stage 4 Command

Eff Sideloop Stage 4 Binary Cmd

SL4-EC

Sideloop Stage 4

Effective Stg Command

Sideloop Stage 5 BO

SL5-C

Sideloop

Stage 5 Command

Eff Sideloop Stage 5 Binary Cmd

SL5-EC

Sideloop Stage 5

Effective Stg Command

Sideloop Stage 6 BO

SL6-C

Sideloop

Stage 6 Command

Eff Sideloop Stage 6 Binary Cmd

SL6-EC

Sideloop Stage 6

Effective Stg Command

Sideloop Stage 7 BO

SL7-C

Sideloop

Stage 7 Command

Eff Sideloop Stage 7 Binary Cmd

SL7-EC

Sideloop Stage 7

Effective Stg Command

Sideloop Stage 8 BO

SL8-C

Sideloop

Stage 8 Command

Eff Sideloop Stage 8 Binary Cmd

SL8-EC

Sideloop Stage 8

Effective Stg Command

Steam Isolation Valve BO

STMISO-C

Steam Isolation Valve

Command

 

N/A

   

Supp Heating Stage 1 BO

SUPHTG1-C

Supplemental Heating

Stage 1 Command

Eff Supp Heating Stage 1 Binary Cmd

SUPHTG1-EC

Supp Heating Stage 1

Effective Stg Command

Supp Heating Valve AO

SUPHTG-O

Supplemental Heating

Output

Eff Supp Heating Valve Cmd

SUPHTG-%

Supplemental Heating

Effective Command

Supp Heating Valve BO

SUPHTG-C

Supplemental Heating

Command

Eff Supp Heating Valve Binary Cmd

SUPHTG-EC

Supp Heating Valve

Effective Vlv Command

Supp Heating Valve PAO

SUPHTG-O

Supplemental Heating

Output_PAO

Eff Supp Heating Valve Cmd

SUPHTG-%

Supplemental Heating

Effective Command

Supplemental Heating Enable BO

SUPHTG-EN

Supplemental Heating Enable

Command

 

N/A

   

Supplemental Heating Pump BO

SUPHTGP-C

Supplemental Heating Pump

Command

 

N/A

   

Supply Damper AO

DPR-O

Supply Air Damper

Output

Eff Damper Cmd

DPR-%

Damper

Effective Command

Supply Damper PAO

DPR-O

Supply Air Damper

Output_PAO

Eff Damper Cmd

DPR-%

Damper

Effective Command

Supply Damper PAO

DPR-O

Supply Air Damper

Output_PAO

_Integrated

Eff Damper Cmd

DPR-%

Damper

Effective Command

Supply Damper PAO - Minimum Pulse Width

PARAM-DPR-MINP

Supply Air Damper

MinPulse

 

N/A

   

Supply Damper PAO Stroke Time

PARAM-DPR-ST

Supply Air Damper

StrokeTime

 

N/A

   

Supply Fan BO

SF-C

Supply Fan

Command

 

N/A

   

Supply Fan BO

SF-C

Supply Fan

Run/Stop

 

N/A

   

Supply Fan Speed AO

SF-O

Supply Fan

Output

Eff Supply Fan Speed Cmd

SF-%

Supply Fan Speed

Effective Command

VSD Bypass Drive BV

SF-BYPASS

Supply Fan

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

SF-RESET

Supply Fan

Reset Drive Fault

 

N/A

   

Supply Fan2 BO

SF2-C

Supply Fan2

Command

 

N/A

   

Supply Fan2 BO

SF2-C

Supply Fan2

Run/Stop

 

N/A

   

Supply Fan2 Speed AO

SF2-O

Supply Fan2

Output

Eff Supply Fan2 Speed Cmd

SF2-%

Supply Fan2 Speed

Effective Command

TEF BO

TEF-C

TEF

Command

 

N/A

   

Tower Basin Heater BO

CTBH-EN

Tower Basin Heater

Command

 

N/A

   

Tower Basin MUV BO

CTMUV-C

Tower Basin MU Valve

Command

 

N/A

   

Twr Bypass Valve AO

CTV-O

Tower Bypass Valve

Output

 

N/A

   

Twr1 Basin Heater BO

CT1BH-EN

Tower1 Basin Heater

Command

 

N/A

   

Twr1 Basin MU BO

CT1MUV-C

Tower1 Basin MU Valve

Command

 

N/A

   

Twr1 Iso Valve BO

CT1ISOV-C

Tower1 Iso Valve

Command

 

N/A

   

Twr2 Basin Heater BO

CT2BH-EN

Tower2 Basin Heater

Command

 

N/A

   

Twr2 Basin MU BO

CT2MUV-C

Tower2 Basin MU Valve

Command

 

N/A

   

Twr2 Iso Valve BO

CT2ISOV-C

Tower2 Iso Valve

Command

 

N/A

   

Twr3 Basin Heater BO

CT3BH-EN

Tower3 Basin Heater

Command

 

N/A

   

Twr3 Basin MU BO

CT3MUV-C

Tower3 Basin MU Valve

Command

 

N/A

   

Twr3 Iso Valve BO

CT3ISOV-C

Tower3 Iso Valve

Command

 

N/A

   

Twr4 Basin Heater BO

CT4BH-EN

Tower4 Basin Heater

Command

 

N/A

   

Twr4 Basin MU BO

CT4MUV-C

Tower4 Basin MU Valve

Command

 

N/A

   

Twr4 Iso Valve BO

CT4ISOV-C

Tower4 Iso Valve

Command

 

N/A

   

Twr5 Basin Heater BO

CT5BH-EN

Tower5 Basin Heater

Command

 

N/A

   

Twr5 Basin MU BO

CT5MUV-C

Tower5 Basin MU Valve

Command

 

N/A

   

Twr5 Iso Valve BO

CT5ISOV-C

Tower5 Iso Valve

Command

 

N/A

   

Twr6 Basin Heater BO

CT6BH-EN

Tower6 Basin Heater

Command

 

N/A

   

Twr6 Basin MU BO

CT6MUV-C

Tower6 Basin MU Valve

Command

 

N/A

   

Twr6 Iso Valve BO

CT6ISOV-C

Tower6 Iso Valve

Command

 

N/A

   

Twr7 Basin Heater BO

CT7BH-EN

Tower7 Basin Heater

Command

 

N/A

   

Twr7 Basin MU BO

CT7MUV-C

Tower7 Basin MU Valve

Command

 

N/A

   

Twr7 Iso Valve BO

CT7ISOV-C

Tower7 Iso Valve

Command

 

N/A

   

Twr8 Basin Heater BO

CT8BH-EN

Tower8 Basin Heater

Command

 

N/A

   

Twr8 Basin MU BO

CT8MUV-C

Tower8 Basin MU Valve

Command

 

N/A

   

Twr8 Iso Valve BO

CT8ISOV-C

Tower8 Iso Valve

Command

 

N/A

   

TwrFan1 AO

CT1-O

TowerFan1

Output

Eff TwrFan1 Cmd

CT1-%

TwrFan1

Effective Command

TwrFan1 BO

CT1-C

TowerFan1

Command

Eff TwrFan1 Binary Cmd

CT1-EC

TwrFan1

Effective Stg Command

TwrFan1 Speed 1 BO

CT1L-C

TowerFan1

Command LO

Eff TwrFan1 Speed 1 Binary Cmd

CT1L-EC

TwrFan1 Speed 1

Effective Stg Command

TwrFan1 Speed 2 BO

CT1M-C

TowerFan1

Command MED

Eff TwrFan1 Speed 2 Binary Cmd

CT1M-EC

TwrFan1 Speed 2

Effective Stg Command

TwrFan1 Speed 3 BO

CT1H-C

TowerFan1

Command HI

Eff TwrFan1 Speed 3 Binary Cmd

CT1H-EC

TwrFan1 Speed 3

Effective Stg Command

VSD Bypass Drive BV

CT1-BYPASS

TowerFan1

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

CT1-RESET

TowerFan1

Reset Drive Fault

 

N/A

   

TwrFan1 IsoVlv BO

CT1ISOV-C

TowerFan1 Iso Valve

Command

 

N/A

   

TwrFan2 AO

CT2-O

TowerFan2

Output

Eff TwrFan2 Cmd

CT2-%

TwrFan2

Effective Command

TwrFan2 BO

CT2-C

TowerFan2

Command

Eff TwrFan2 Binary Cmd

CT2-EC

TwrFan2

Effective Stg Command

TwrFan2 Speed 1 BO

CT2L-C

TowerFan2

Command LO

Eff TwrFan2 Speed 2 Binary Cmd

CT2L-EC

TwrFan2 Speed 2

Effective Stg Command

TwrFan2 Speed 2 BO

CT2M-C

TowerFan2

Command MED

Eff TwrFan2 Speed 2 Binary Cmd

CT2M-EC

TwrFan2 Speed 2

Effective Stg Command

TwrFan2 Speed 3 BO

CT2H-C

TowerFan2

Command HI

Eff TwrFan2 Speed 3 Binary Cmd

CT2H-EC

TwrFan2 Speed 3

Effective Stg Command

VSD Bypass Drive BV

CT2-BYPASS

TowerFan2

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

CT2-RESET

TowerFan2

Reset Drive Fault

 

N/A

   

TwrFan2 IsoVlv BO

CT2ISOV-C

TowerFan2 Iso Valve

Command

 

N/A

   

TwrFan3 AO

CT3-O

TowerFan3

Output

Eff TwrFan3 Cmd

CT3-%

TwrFan3

Effective Command

TwrFan3 BO

CT3-C

TowerFan3

Command

Eff TwrFan3 Binary Cmd

CT3-EC

TwrFan3

Effective Stg Command

TwrFan3 Speed 1 BO

CT3L-C

TowerFan3

Command LO

Eff TwrFan3 Speed 3 Binary Cmd

CT3M-EC

TwrFan3 Speed 3

Effective Stg Command

TwrFan3 Speed 2 BO

CT3M-C

TowerFan3

Command MED

Eff TwrFan3 Speed 2 Binary Cmd

CT3L-EC

TwrFan3 Speed 2

Effective Stg Command

TwrFan3 Speed 3 BO

CT3H-C

TowerFan3

Command HI

Eff TwrFan3 Speed 3 Binary Cmd

CT3H-EC

TwrFan3 Speed 3

Effective Stg Command

VSD Bypass Drive BV

CT3-BYPASS

TowerFan3

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

CT3-RESET

TowerFan3

Reset Drive Fault

 

N/A

   

TwrFan3 IsoVlv BO

CT3ISOV-C

TowerFan3 Iso Valve

Command

 

N/A

   

TwrFan4 AO

CT4-O

TowerFan4

Output

Eff TwrFan4 Cmd

CT4-%

TwrFan4

Effective Command

TwrFan4 BO

CT4-C

TowerFan4

Command

Eff TwrFan4 Binary Cmd

CT4-EC

TwrFan4

Effective Stg Command

TwrFan4 Speed 1 BO

CT4L-C

TowerFan4

Command LO

Eff TwrFan4 Speed 4 Binary Cmd

CT4H-EC

TwrFan4 Speed 4

Effective Stg Command

TwrFan4 Speed 2 BO

CT4M-C

TowerFan4

Command MED

Eff TwrFan4 Speed 2 Binary Cmd

CT4L-EC

TwrFan4 Speed 2

Effective Stg Command

TwrFan4 Speed 3 BO

CT4H-C

TowerFan4

Command HI

Eff TwrFan4 Speed 3 Binary Cmd

CT4M-EC

TwrFan4 Speed 3

Effective Stg Command

VSD Bypass Drive BV

CT4-BYPASS

TowerFan4

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

CT4-RESET

TowerFan4

Reset Drive Fault

 

N/A

   

TwrFan4 IsoVlv BO

CT4ISOV-C

TowerFan4 Iso Valve

Command

 

N/A

   

TwrFan5 AO

CT5-O

TowerFan5

Output

Eff TwrFan5 Cmd

CT5-%

TwrFan5

Effective Command

TwrFan5 BO

CT5-C

TowerFan5

Command

Eff TwrFan5 Binary Cmd

CT5-EC

TwrFan5

Effective Stg Command

TwrFan5 Speed 1 BO

CT5L-C

TowerFan5

Command LO

Eff TwrFan5 Speed 5 Binary Cmd

CT5H-EC

TwrFan5 Speed 5

Effective Stg Command

TwrFan5 Speed 2 BO

CT5M-C

TowerFan5

Command MED

Eff TwrFan5 Speed 2 Binary Cmd

CT5L-EC

TwrFan5 Speed 2

Effective Stg Command

TwrFan5 Speed 3 BO

CT5H-C

TowerFan5

Command HI

Eff TwrFan5 Speed 3 Binary Cmd

CT5M-EC

TwrFan5 Speed 3

Effective Stg Command

VSD Bypass Drive BV

CT5-BYPASS

TowerFan5

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

CT5-RESET

TowerFan5

Reset Drive Fault

 

N/A

   

TwrFan5 IsoVlv BO

CT5ISOV-C

TowerFan5 Iso Valve

Command

 

N/A

   

TwrFan6 AO

CT6-O

TowerFan6

Output

Eff TwrFan6 Cmd

CT6-%

TwrFan6

Effective Command

TwrFan6 BO

CT6-C

TowerFan6

Command

Eff TwrFan6 Binary Cmd

CT6-EC

TwrFan6

Effective Stg Command

TwrFan6 Speed 1 BO

CT6L-C

TowerFan6

Command LO

Eff TwrFan6 Speed 6 Binary Cmd

CT6H-EC

TwrFan6 Speed 6

Effective Stg Command

TwrFan6 Speed 2 BO

CT6M-C

TowerFan6

Command MED

Eff TwrFan6 Speed 2 Binary Cmd

CT6L-EC

TwrFan6 Speed 2

Effective Stg Command

TwrFan6 Speed 3 BO

CT6H-C

TowerFan6

Command HI

Eff TwrFan6 Speed 3 Binary Cmd

CT6M-EC

TwrFan6 Speed 3

Effective Stg Command

VSD Bypass Drive BV

CT6-BYPASS

TowerFan6

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

CT6-RESET

TowerFan6

Reset Drive Fault

 

N/A

   

TwrFan6 IsoVlv BO

CT6ISOV-C

TowerFan6 Iso Valve

Command

 

N/A

   

TwrFan7 AO

CT7-O

TowerFan7

Output

Eff TwrFan7 Cmd

CT7-%

TwrFan7

Effective Command

TwrFan7 BO

CT7-C

TowerFan7

Command

Eff TwrFan7 Binary Cmd

CT7-EC

TwrFan7

Effective Stg Command

TwrFan7 Speed 1 BO

CT7L-C

TowerFan7

Command LO

Eff TwrFan7 Speed 7 Binary Cmd

CT7H-EC

TwrFan7 Speed 7

Effective Stg Command

TwrFan7 Speed 2 BO

CT7M-C

TowerFan7

Command MED

Eff TwrFan7 Speed 2 Binary Cmd

CT7L-EC

TwrFan7 Speed 2

Effective Stg Command

TwrFan7 Speed 3 BO

CT7H-C

TowerFan7

Command HI

Eff TwrFan7 Speed 3 Binary Cmd

CT7M-EC

TwrFan7 Speed 3

Effective Stg Command

VSD Bypass Drive BV

CT7-BYPASS

TowerFan7

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

CT7-RESET

TowerFan7

Reset Drive Fault

 

N/A

   

TwrFan7 IsoVlv BO

CT7ISOV-C

TowerFan7 Iso Valve

Command

 

N/A

   

TwrFan8 AO

CT8-O

TowerFan8

Output

Eff TwrFan8 Cmd

CT8-%

TwrFan8

Effective Command

TwrFan8 BO

CT8-C

TowerFan8

Command

Eff TwrFan8 Binary Cmd

CT8-EC

TwrFan8

Effective Stg Command

TwrFan8 Speed 1 BO

CT8L-C

TowerFan8

Command LO

Eff TwrFan8 Speed 8 Binary Cmd

CT8H-EC

TwrFan8 Speed 8

Effective Stg Command

TwrFan8 Speed 2 BO

CT8M-C

TowerFan8

Command MED

Eff TwrFan8 Speed 2 Binary Cmd

CT8L-EC

TwrFan8 Speed 2

Effective Stg Command

TwrFan8 Speed 3 BO

CT8H-C

TowerFan8

Command HI

Eff TwrFan8 Speed 3 Binary Cmd

CT8M-EC

TwrFan8 Speed 3

Effective Stg Command

VSD Bypass Drive BV

CT8-BYPASS

TowerFan8

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

CT8-RESET

TowerFan8

Reset Drive Fault

 

N/A

   

TwrFan8 IsoVlv BO

CT8ISOV-C

TowerFan8 Iso Valve

Command

 

N/A

   

Voltage Out 1 AO

VOLT1-O

Voltage 1

Output

 

N/A

   

Voltage Out 2 AO

VOLT2-O

Voltage 2

Output

 

N/A

   

Voltage Out 3 AO

VOLT3-O

Voltage 3

Output

 

N/A

   

Voltage Out 4 AO

VOLT4-O

Voltage 4

Output

 

N/A

   

Voltage Out 5 AO

VOLT5-O

Voltage 5

Output

 

N/A

   

Voltage Out 6 AO

VOLT6-O

Voltage 6

Output

 

N/A

   

Supply Fan BO

VSD1-C

VSD1

Run/Stop

 

N/A

   

Supply Fan Speed AO

VSD1-O

VSD1

Output

Eff Supply Fan Speed Cmd

SF-%

Supply Fan Speed

Effective Command

VSD Bypass Drive BV

VSD1-BYPASS

VSD1

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

VSD1-RESET

VSD1

Reset Drive Fault

 

N/A

   

Supply Fan BO

VSD2-C

VSD2

Run/Stop

 

N/A

   

Supply Fan Speed AO

VSD2-O

VSD2

Output

Eff Supply Fan Speed Cmd

SF-%

Supply Fan Speed

Effective Command

VSD Bypass Drive BV

VSD2-BYPASS

VSD2

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

VSD2-RESET

VSD2

Reset Drive Fault

 

N/A

   

Supply Fan BO

VSD3-C

VSD3

Run/Stop

 

N/A

   

Supply Fan Speed AO

VSD3-O

VSD3

Output

Eff Supply Fan Speed Cmd

SF-%

Supply Fan Speed

Effective Command

VSD Bypass Drive BV

VSD3-BYPASS

VSD3

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

VSD3-RESET

VSD3

Reset Drive Fault

 

N/A

   

Supply Fan BO

VSD4-C

VSD4

Run/Stop

 

N/A

   

Supply Fan Speed AO

VSD4-O

VSD4

Output

Eff Supply Fan Speed Cmd

SF-%

Supply Fan Speed

Effective Command

VSD Bypass Drive BV

VSD4-BYPASS

VSD4

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

VSD4-RESET

VSD4

Reset Drive Fault

 

N/A

   

Supply Fan BO

VSD5-C

VSD5

Run/Stop

 

N/A

   

Supply Fan Speed AO

VSD5-O

VSD5

Output

Eff Supply Fan Speed Cmd

SF-%

Supply Fan Speed

Effective Command

VSD Bypass Drive BV

VSD5-BYPASS

VSD5

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

VSD5-RESET

VSD5

Reset Drive Fault

 

N/A

   

Supply Fan BO

VSD6-C

VSD6

Run/Stop

 

N/A

   

Supply Fan Speed AO

VSD6-O

VSD6

Output

Eff Supply Fan Speed Cmd

SF-%

Supply Fan Speed

Effective Command

VSD Bypass Drive BV

VSD6-BYPASS

VSD6

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

VSD6-RESET

VSD6

Reset Drive Fault

 

N/A

   

Supply Fan BO

VSD7-C

VSD7

Run/Stop

 

N/A

   

Supply Fan Speed AO

VSD7-O

VSD7

Output

Eff Supply Fan Speed Cmd

SF-%

Supply Fan Speed

Effective Command

VSD Bypass Drive BV

VSD7-BYPASS

VSD7

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

VSD7-RESET

VSD7

Reset Drive Fault

 

N/A

   

Supply Fan BO

VSD8-C

VSD8

Run/Stop

 

N/A

   

Supply Fan Speed AO

VSD8-O

VSD8

Output

Eff Supply Fan Speed Cmd

SF-%

Supply Fan Speed

Effective Command

VSD Bypass Drive BV

VSD8-BYPASS

VSD8

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

VSD8-RESET

VSD8

Reset Drive Fault

 

N/A

   

Supply Fan BO

VSD9-C

VSD9

Run/Stop

 

N/A

   

Supply Fan Speed AO

VSD9-O

VSD9

Output

Eff Supply Fan Speed Cmd

SF-%

Supply Fan Speed

Effective Command

VSD Bypass Drive BV

VSD9-BYPASS

VSD9

Bypass Drive

 

N/A

   

VSD Reset Drive Fault BV

VSD9-RESET

VSD9

Reset Drive Fault

 

N/A

   

Fan Speed Status Display MSV

ZNF-%

Zone

Fan Speed Status

 

N/A

   

Occupancy Status Display MSV

OCC-MODE

Zone

Occ Status

 

N/A

   

Zone 1 Heating Pump BO

ZHLP1-C

Zone Loop Heating Pump 1

Command

 

N/A

   

Zone 2 Heating Pump BO

ZHLP2-C

Zone Loop Heating Pump 2

Command

 

N/A

   

Zone 3 Heating Pump BO

ZHLP3-C

Zone Loop Heating Pump 3

Command

 

N/A

   

Zone 4 Heating Pump BO

ZHLP4-C

Zone Loop Heating Pump 4

Command

 

N/A

   

Zone 5 Heating Pump BO

ZHLP5-C

Zone Loop Heating Pump 5

Command

 

N/A

   

Zone 6 Heating Pump BO

ZHLP6-C

Zone Loop Heating Pump 6

Command

 

N/A

   

Zone 7 Heating Pump BO

ZHLP7-C

Zone Loop Heating Pump 7

Command

 

N/A

   

Zone 8 Heating Pump BO

ZHLP8-C

Zone Loop Heating Pump 8

Command

 

N/A

   

Occupancy Status Display MSV

OCC-MODE1

Zone1

Occ Status

 

N/A

   

Zone 1 Damper AO

ZN1D-O

Zone1 Damper

Output

Eff Zone 1 Damper Cmd

ZN1D-%

Zone 1 Damper

Effective Command

Zone 1 Damper PAO

ZN1D-O

Zone1 Damper

Output_PAO

Eff Zone 1 Damper Cmd

ZN1D-%

Zone 1 Damper

Effective Command

Zone 1 Heating Stage 1 BO

ZN1HTG1-C

Zone1 Heating

Stage 1 Command

Eff Zone 1 Heating Stage 1 Binary Cmd

ZN1HTG1-EC

Zone 1 Heating Stage 1

Effective Stg Command

Zone 1 Heating Stage 2 BO

ZN1HTG2-C

Zone1 Heating

Stage 2 Command

Eff Zone 1 Heating Stage 2 Binary Cmd

ZN1HTG2-EC

Zone 1 Heating Stage 2

Effective Stg Command

Zone 1 Heating Stage 3 BO

ZN1HTG3-C

Zone1 Heating

Stage 3 Command

Eff Zone 1 Heating Stage 3 Binary Cmd

ZN1HTG3-EC

Zone 1 Heating Stage 3

Effective Stg Command

Zone 1 Heating Valve AO

ZN1HTG-O

Zone1 Heating

Output

Eff Zone 1 Heating Valve Cmd

ZN1HTG-%

Zone 1 Heating Valve

Effective Command

Zone 1 Heating Valve BO

ZN1HTG-C

Zone1 Heating

Command

Eff Zone 1 Heating Valve Binary Cmd

ZN1HTG-EC

Zone 1 Heating Valve

Effective Vlv Command

Zone 1 Heating Valve PAO

ZN1HTG-O

Zone1 Heating

Output_PAO

Eff Zone 1 Heating Valve Cmd

ZN1HTG-%

Zone 1 Heating Valve

Effective Command

Occupancy Status Display MSV

OCC-MODE2

Zone2

Occ Status

 

N/A

   

Zone 2 Damper AO

ZN2D-O

Zone2 Damper

Output

Eff Zone 2 Damper Cmd

ZN2D-%

Zone 2 Damper

Effective Command

Zone 2 Damper PAO

ZN2D-O

Zone2 Damper

Output_PAO

Eff Zone 2 Damper Cmd

ZN2D-%

Zone 2 Damper

Effective Command

Zone 2 Heating Stage 1 BO

ZN2HTG1-C

Zone2 Heating

Stage 1 Command

Eff Zone 2 Heating Stage 2 Binary Cmd

ZN2HTG1-EC

Zone 2 Heating Stage 2

Effective Stg Command

Zone 2 Heating Stage 2 BO

ZN2HTG2-C

Zone2 Heating

Stage 2 Command

Eff Zone 2 Heating Stage 2 Binary Cmd

ZN2HTG2-EC

Zone 2 Heating Stage 2

Effective Stg Command

Zone 2 Heating Stage 3 BO

ZN2HTG3-C

Zone2 Heating

Stage 3 Command

Eff Zone 2 Heating Stage 3 Binary Cmd

ZN2HTG3-EC

Zone 2 Heating Stage 3

Effective Stg Command

Zone 2 Heating Valve AO

ZN2HTG-O

Zone2 Heating

Output

Eff Zone 2 Heating Valve Cmd

ZN2HTG-%

Zone 2 Heating Valve

Effective Command

Zone 2 Heating Valve BO

ZN2HTG-C

Zone2 Heating

Command

Eff Zone 2 Heating Valve Binary Cmd

ZN2HTG-EC

Zone 2 Heating Valve

Effective Vlv Command

Zone 2 Heating Valve PAO

ZN2HTG-O

Zone2 Heating

Output_PAO

Eff Zone 2 Heating Valve Cmd

ZN2HTG-%

Zone 2 Heating Valve

Effective Command

Occupancy Status Display MSV

OCC-MODE3

Zone3

Occ Status

 

N/A

   

Zone 3 Damper AO

ZN3D-O

Zone3 Damper

Output

Eff Zone 3 Damper Cmd

ZN3D-%

Zone 3 Damper

Effective Command

Zone 3 Damper PAO

ZN3D-O

Zone3 Damper

Output_PAO

Eff Zone 3 Damper Cmd

ZN3D-%

Zone 3 Damper

Effective Command

Zone 3 Heating Stage 1 BO

ZN3HTG1-C

Zone3 Heating

Stage 1 Command

Eff Zone 3 Heating Stage 3 Binary Cmd

ZN3HTG2-EC

Zone 3 Heating Stage 3

Effective Stg Command

Zone 3 Heating Stage 2 BO

ZN3HTG2-C

Zone3 Heating

Stage 2 Command

Eff Zone 3 Heating Stage 2 Binary Cmd

ZN3HTG3-EC

Zone 3 Heating Stage 2

Effective Stg Command

Zone 3 Heating Stage 3 BO

ZN3HTG3-C

Zone3 Heating

Stage 3 Command

Eff Zone 3 Heating Stage 3 Binary Cmd

ZN3HTG3-EC

Zone 3 Heating Stage 3

Effective Stg Command

Zone 3 Heating Valve AO

ZN3HTG-O

Zone3 Heating

Output

Eff Zone 3 Heating Valve Cmd

ZN3HTG-%

Zone 3 Heating Valve

Effective Command

Zone 3 Heating Valve BO

ZN3HTG-C

Zone3 Heating

Command

Eff Zone 3 Heating Valve Binary Cmd

ZN3HTG-EC

Zone 3 Heating Valve

Effective Vlv Command

Zone 3 Heating Valve PAO

ZN3HTG-O

Zone3 Heating

Output_PAO

Eff Zone 3 Heating Valve Cmd

ZN3HTG-%

Zone 3 Heating Valve

Effective Command

Occupancy Status Display MSV

OCC-MODE4

Zone4

Occ Status

 

N/A

   

Zone 4 Damper AO

ZN4D-O

Zone4 Damper

Output

Eff Zone 4 Damper Cmd

ZN4D-%

Zone 4 Damper

Effective Command

Zone 4 Damper PAO

ZN4D-O

Zone4 Damper

Output_PAO

Eff Zone 4 Damper Cmd

ZN4D-%

Zone 4 Damper

Effective Command

Zone 4 Heating Stage 1 BO

ZN4HTG1-C

Zone4 Heating

Stage 1 Command

Eff Zone 4 Heating Stage 4 Binary Cmd

ZN4HTG3-EC

Zone 4 Heating Stage 4

Effective Stg Command

Zone 4 Heating Stage 2 BO

ZN4HTG2-C

Zone4 Heating

Stage 2 Command

Eff Zone 4 Heating Stage 2 Binary Cmd

ZN4HTG4-EC

Zone 4 Heating Stage 2

Effective Stg Command

Zone 4 Heating Stage 3 BO

ZN4HTG3-C

Zone4 Heating

Stage 3 Command

Eff Zone 4 Heating Stage 3 Binary Cmd

ZN4HTG2-EC

Zone 4 Heating Stage 3

Effective Stg Command

Zone 4 Heating Valve AO

ZN4HTG-O

Zone4 Heating

Output

Eff Zone 4 Heating Valve Cmd

ZN4HTG-%

Zone 4 Heating Valve

Effective Command

Zone 4 Heating Valve BO

ZN4HTG-C

Zone4 Heating

Command

Eff Zone 4 Heating Valve Binary Cmd

ZN4HTG-EC

Zone 4 Heating Valve

Effective Vlv Command

Zone 4 Heating Valve PAO

ZN4HTG-O

Zone4 Heating

Output_PAO

Eff Zone 4 Heating Valve Cmd

ZN4HTG-%

Zone 4 Heating Valve

Effective Command

Zone 5 Damper AO

ZN5D-O

Zone5 Damper

Output

Eff Zone 5 Damper Cmd

ZN5D-%

Zone 5 Damper

Effective Command

Zone 5 Damper PAO

ZN5D-O

Zone5 Damper

Output_PAO

Eff Zone 5 Damper Cmd

ZN5D-%

Zone 5 Damper

Effective Command

Zone 5 Heating Stage 1 BO

ZN5HTG1-C

Zone5 Heating

Stage 1 Command

Eff Zone 5 Heating Stage 5 Binary Cmd

ZN5HTG3-EC

Zone 5 Heating Stage 5

Effective Stg Command

Zone 5 Heating Stage 2 BO

ZN5HTG2-C

Zone5 Heating

Stage 2 Command

Eff Zone 5 Heating Stage 2 Binary Cmd

ZN5HTG5-EC

Zone 5 Heating Stage 2

Effective Stg Command

Zone 5 Heating Stage 3 BO

ZN5HTG3-C

Zone5 Heating

Stage 3 Command

Eff Zone 5 Heating Stage 3 Binary Cmd

ZN5HTG2-EC

Zone 5 Heating Stage 3

Effective Stg Command

Zone 5 Heating Valve AO

ZN5HTG-O

Zone5 Heating

Output

Eff Zone 5 Heating Valve Cmd

ZN5HTG-%

Zone 5 Heating Valve

Effective Command

Zone 5 Heating Valve BO

ZN5HTG-C

Zone5 Heating

Command

Eff Zone 5 Heating Valve Binary Cmd

ZN5HTG-EC

Zone 5 Heating Valve

Effective Vlv Command

Zone 5 Heating Valve PAO

ZN5HTG-O

Zone5 Heating

Output_PAO

Eff Zone 5 Heating Valve Cmd

ZN5HTG-%

Zone 5 Heating Valve

Effective Command

Zone 6 Damper AO

ZN6D-O

Zone6 Damper

Output

Eff Zone 6 Damper Cmd

ZN6D-%

Zone 6 Damper

Effective Command

Zone 6 Damper PAO

ZN6D-O

Zone6 Damper

Output_PAO

Eff Zone 6 Damper Cmd

ZN6D-%

Zone 6 Damper

Effective Command

Zone 6 Heating Stage 1 BO

ZN6HTG1-C

Zone6 Heating

Stage 1 Command

Eff Zone 6 Heating Stage 6 Binary Cmd

ZN6HTG3-EC

Zone 6 Heating Stage 6

Effective Stg Command

Zone 6 Heating Stage 2 BO

ZN6HTG2-C

Zone6 Heating

Stage 2 Command

Eff Zone 6 Heating Stage 2 Binary Cmd

ZN6HTG6-EC

Zone 6 Heating Stage 2

Effective Stg Command

Zone 6 Heating Stage 3 BO

ZN6HTG3-C

Zone6 Heating

Stage 3 Command

Eff Zone 6 Heating Stage 3 Binary Cmd

ZN6HTG2-EC

Zone 6 Heating Stage 3

Effective Stg Command

Zone 6 Heating Valve AO

ZN6HTG-O

Zone6 Heating

Output

Eff Zone 6 Heating Valve Cmd

ZN6HTG-%

Zone 6 Heating Valve

Effective Command

Zone 6 Heating Valve BO

ZN6HTG-C

Zone6 Heating

Command

Eff Zone 6 Heating Valve Binary Cmd

ZN6HTG-EC

Zone 6 Heating Valve

Effective Vlv Command

Zone 6 Heating Valve PAO

ZN6HTG-O

Zone6 Heating

Output_PAO

Eff Zone 6 Heating Valve Cmd

ZN6HTG-%

Zone 6 Heating Valve

Effective Command

Zone 7 Damper AO

ZN7D-O

Zone7 Damper

Output

Eff Zone 7 Damper Cmd

ZN7D-%

Zone 7 Damper

Effective Command

Zone 7 Damper PAO

ZN7D-O

Zone7 Damper

Output_PAO

Eff Zone 7 Damper Cmd

ZN7D-%

Zone 7 Damper

Effective Command

Zone 7 Heating Stage 1 BO

ZN7HTG1-C

Zone7 Heating

Stage 1 Command

Eff Zone 7 Heating Stage 7 Binary Cmd

ZN7HTG3-EC

Zone 7 Heating Stage 7

Effective Stg Command

Zone 7 Heating Stage 2 BO

ZN7HTG2-C

Zone7 Heating

Stage 2 Command

Eff Zone 7 Heating Stage 2 Binary Cmd

ZN7HTG7-EC

Zone 7 Heating Stage 2

Effective Stg Command

Zone 7 Heating Stage 3 BO

ZN7HTG3-C

Zone7 Heating

Stage 3 Command

Eff Zone 7 Heating Stage 3 Binary Cmd

ZN7HTG2-EC

Zone 7 Heating Stage 3

Effective Stg Command

Zone 7 Heating Valve AO

ZN7HTG-O

Zone7 Heating

Output

Eff Zone 7 Heating Valve Cmd

ZN7HTG-%

Zone 7 Heating Valve

Effective Command

Zone 7 Heating Valve BO

ZN7HTG-C

Zone7 Heating

Command

Eff Zone 7 Heating Valve Binary Cmd

ZN7HTG-EC

Zone 7 Heating Valve

Effective Vlv Command

Zone 7 Heating Valve PAO

ZN7HTG-O

Zone7 Heating

Output_PAO

Eff Zone 7 Heating Valve Cmd

ZN7HTG-%

Zone 7 Heating Valve

Effective Command

Zone 8 Damper AO

ZN8D-O

Zone8 Damper

Output

Eff Zone 8 Damper Cmd

ZN8D-%

Zone 8 Damper

Effective Command

Zone 8 Damper PAO

ZN8D-O

Zone8 Damper

Output_PAO

Eff Zone 8 Damper Cmd

ZN8D-%

Zone 8 Damper

Effective Command

Zone 8 Heating Stage 1 BO

ZN8HTG1-C

Zone8 Heating

Stage 1 Command

Eff Zone 8 Heating Stage 8 Binary Cmd

ZN8HTG3-EC

Zone 8 Heating Stage 8

Effective Stg Command

Zone 8 Heating Stage 2 BO

ZN8HTG2-C

Zone8 Heating

Stage 2 Command

Eff Zone 8 Heating Stage 2 Binary Cmd

ZN8HTG8-EC

Zone 8 Heating Stage 2

Effective Stg Command

Zone 8 Heating Stage 3 BO

ZN8HTG3-C

Zone8 Heating

Stage 3 Command

Eff Zone 8 Heating Stage 3 Binary Cmd

ZN8HTG2-EC

Zone 8 Heating Stage 3

Effective Stg Command

Zone 8 Heating Valve AO

ZN8HTG-O

Zone8 Heating

Output

Eff Zone 8 Heating Valve Cmd

ZN8HTG-%

Zone 8 Heating Valve

Effective Command

Zone 8 Heating Valve BO

ZN8HTG-C

Zone8 Heating

Command

Eff Zone 8 Heating Valve Binary Cmd

ZN8HTG-EC

Zone 8 Heating Valve

Effective Vlv Command

Zone 8 Heating Valve PAO

ZN8HTG-O

Zone8 Heating

Output_PAO

Eff Zone 8 Heating Valve Cmd

ZN8HTG-%

Zone 8 Heating Valve

Effective Command