Line Segment - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

See Configuring the Line Segment Block.

Table 1. Line Segment

Field

Description

Edit Use to edit the table data.
Name Use to enter a name for the block.
Object Identifier Indicates object BACnet ID and instance number.
Input and Outputs Table

Displays both an Inputs and an Outputs table for the selected module/block. These tables include the following data:

  • Name: Name of the input or output.
  • Standard Name: Johnson Controls standard name used for the input or output.
  • Default Value: Default values of the inputs and outputs.
  • Units: Units of measurement used for the inputs and outputs.
  • Display Precision: Display Precision value used for the inputs and outputs (for example, 10ths).
  • BACnet Exposed: Indicates whether the input or output parameter is exposed for BACnet systems.

Input Points

Lists the values expected of the Line Segment input in ascending order.

Output Points

Lists the values that the Line Segment maps to from the Input Points column.

Apply

Applies the changes.

Cancel

Discards the changes.

Close Closes the screen.

Opens the Help system.