Hidden Edge Label - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

See the Changing the Hidden Edge Label of a Connection section.

Table 1. Hidden Edge Label

Field

Description

Label

Use to type a label name to use to indicate the associated hidden connection line.

OK

Applies the changes and closes the dialog box.

Cancel

Closes the dialog box without applying the changes.