The New Module Selection screen appears in multiple instances, such as when you add a new item within the Control View, or when you open the Launch Wizard. Table 1 and Table 2 provide information on the differences between adding new module selections and input/output selections. See Creating Custom Logic (Adding Modules) and Using the Launch Wizard.
The following table applies to the New Module Selection dialog box for the following options:
- Launch Wizard
- Network Inputs
-
Setpoint/Miscellaneous Module Selection
-
State Generation Module Selection
-
Output Control Module Selection
- Network Outputs
|
Field |
Description |
|---|---|
| Filter |
Filters the content of the table. Type one or more letters appearing in the data you want to view. |
| Count | Specifies the number of modules to add to the system. |
| Name |
Lists the default name of the module. This name appears in the UI if you do not specify a User Name.
Note: To open the web help for a module, click the appropriate link in this field.
|
|
Palette |
Specifies the folder or category that the module is part of. |
|
Standard Name |
Displays a Johnson Controls standard name for the module. |
|
User Name |
Specify a name for the module.
Note: If this field is blank, the value in the Name column is used.
|
| Previous | Disabled for Classic View additions. |
| Next | Disabled for Classic View additions. |
| Finish | Applies changes and closes the dialog box. |
| Cancel | Discards changes and closes the dialog box. |
|
|
Opens the Help system. |
The following table applies to the New Module Selection dialog box for the following options:
- Inputs
-
Miscellaneous Inputs
- Outputs
-
Miscellaneous Outputs
|
Field |
Description |
|---|---|
| Filter |
Filters the content of the table. Type one or more letters appearing in the data you want to view. |
| Count | Specifies the number of points to add to the system. |
|
Application |
Lists the application types available for the points. |
|
Function |
Lists the functions available for the points. |
|
Data Type |
Lists the data types available for the points. |
|
Signal |
Lists the signals available for the points. |
|
User Name |
Specify a name for the module. |
| Previous | Disabled for Classic View additions. |
| Next | Disabled for Classic View additions. |
| Finish | Applies changes and closes the dialog box. |
|
Cancel |
Discards changes and closes the dialog box. |
|
|
Opens the Help system. |