Create State Selection Table - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

See Customizing State Selection Tables.

Table 1. Create State Selection Table

Field

Description

Name

Use to type a name for the module/table. We recommend leaving this field empty so that dynamic naming may be used.

Table Priority

Indicates the order in which the table appears in the State Tables dialog box.

Table Data Type (Port Type)

Use to select an Enumeration set to use, or indicates to use a Boolean data type.

OK

Creates the table and closes the dialog box.

Cancel

Closes the dialog box without applying the change.

Opens the Help system.