Create State Selection Column - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
See Customizing State Selection Tables.

Table 1. Create State Selection Column

Field

Description

Name

Use to type a name for the module/column. We recommend leaving this field empty so that dynamic naming may be used.

Column Index

Indicates the order in which the column appears in the table.

Column Data Type (Port Type)

Use to select an Enumeration set to use, or indicates to use a Boolean data type.

OK

Creates the column and closes the dialog box.

Cancel

Closes the dialog box without applying the change.

Opens the Help system.