System Types and Configurations - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

When selecting a system, you first choose the overall type of system and a specific configuration to create. For example, you may select VAV as the system type and Single Duct as the specific configuration to use. See the Selecting a System (Creating a New System) steps and the Applications section for details on the System Selection options: